Some customers often use LVDS LCD with low resolution on i.MX6 platform, such as 320x240, but by defualt , linux bsp doesn't support low frequency pixel clock for LVDS module input. Question: When we port LVDS LCD with 320x240 resolution to android4.2.2, we found pixel clock is not correct, it always output 38.9MHz, it is no probem for big resolution , for example 1024x768, but the clock we need for 320x240 LCD is 6.4MHz. According to the quesiton, Let us check IPU & LDB clock in i.MX6 datasheet at first : From above table, if ldb clock is from IPU, we will not get 6.4MHz pixel clock, so we will have to adjust its source clock: The following steps are procedure that ports LVDS LCD with 320x240 resolution to i.MX6Q. 1. Adding LVDS LCD timing structure to ldb.c static struct fb_videomode ldb_modedb[] = { { "LDB-XGA", 60, 320, 240, 155914, 38, 20, 15, 4, 30, 3, 0, FB_VMODE_NONINTERLACED, FB_MODE_IS_DETAILED, }, { "LDB-1080P60", 60, 1920, 1080, 7692, 100, 40, 30, 3, 10, 2, 0, FB_VMODE_NONINTERLACED, FB_MODE_IS_DETAILED,}, }; 2.Modifying clock source of ldb module Checking /arch/arm/mach-mx6/clock.c, we can find there are 3 ldb's clock source : &pll5_video_main_clk, &pll2_pfd_352M, &pll2_pfd_400M, static int _clk_ldb_di1_set_parent(struct clk *clk, struct clk *parent) { u32 reg, mux; int rev = mx6q_revision(); reg = __raw_readl(MXC_CCM_CS2CDR) & ~MXC_CCM_CS2CDR_LDB_DI1_CLK_SEL_MASK; mux = _get_mux6(parent, &pll5_video_main_clk, &pll2_pfd_352M, &pll2_pfd_400M, (rev == IMX_CHIP_REVISION_1_0) ? &pll3_pfd_540M : /* MX6Q TO1.0 */ &mmdc_ch1_axi_clk[0], /* MX6Q TO1.1 and MX6DL */ &pll3_usb_otg_main_clk, NULL); reg |= (mux << MXC_CCM_CS2CDR_LDB_DI1_CLK_SEL_OFFSET); __raw_writel(reg, MXC_CCM_CS2CDR); return 0; } By default, pll2_pfd_352M is configured as the clock source of ldb: clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M); clk_set_parent(&ldb_di1_clk, &pll2_pfd_352M); We should change the clock source to be pll5_video_main_clk clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk,); clk_set_parent(&ldb_di1_clk, &pll5_video_main_clk,); 3. Configuring initial clock in board-mx6q_sabresd.c static struct ipuv3_fb_platform_data sabresd_fb_data[] = { { /*fb0*/ .disp_dev = "ldb", .interface_pix_fmt = IPU_PIX_FMT_RGB666, .mode_str = "LDB-XGA", .default_bpp = 16, .int_clk = false, .late_init = false, } int_clk=false means LDB clock is from PLL2_PFD_352 or pll5_video_main_clk; int_clk=true mean LDB clock if from IPU. OK, after doing above steps, LVDS LCD with low resolution should normally work. Freescale TICS team Weidong.sun 2015-08-18
查看全文