It is one mandatory patch if you are in the case: The chip you are using is imx6sx TO1.3 and newer, and use the kobs-ng to flash your image to the Nand memory chip. If you are using MFG, you also need rebuild the kobs-ng, and update the binary into your MFG tool. The patch have been integrated into the default release yocto_4.1.15, but if you are using the older version release before yocto_4.1.15, please make sure you have integrated the modification when you need to use kobs-ng to flash the image to Nand memory chip. commit 5ecf08703da489a3bd317341f630870a3d07dab9 Author: Han Xu <han.xu@nxp.com> Date: Thu Jan 28 14:40:14 2016 -0600 MMT-105: change the i.mx6sx revision check change the i.mx6sx revision check since v1.3 uses v1.2 boot config as well. Signed-off-by: Han Xu <han.xu@nxp.com> (cherry picked from commit 1dac0c14d1e2016c2fa804f6628543d8d238c680) diff --git a/src/plat_boot_config.c b/src/plat_boot_config.c index 461675a..e1ef6f3 100644 --- a/src/plat_boot_config.c +++ b/src/plat_boot_config.c @@ -1,5 +1,5 @@ /* -* Copyright (C) 2010-2015 Freescale Semiconductor, Inc. All Rights Reserved. +* Copyright (C) 2010-2016 Freescale Semiconductor, Inc. All Rights Reserved. */ /* @@ -256,10 +256,12 @@ int discover_boot_rom_version(void) } fgets(line_buffer, sizeof(line_buffer), revision); if (!strncmp(line_buffer, "1.0", strlen("1.0")) || - !strncmp(line_buffer, "1.1", strlen("1.1"))) + !strncmp(line_buffer, "1.1", strlen("1.1"))) { plat_config_data = &mx6sx_boot_config; - if (!strncmp(line_buffer, "1.2", strlen("1.2"))) + /* all other revisions should use the latest boot config */ + } else { plat_config_data = &mx6sx_to_1_2_boot_config; + } } if (!strncmp(line_buffer, plat_imx6ul, strlen(plat_imx6ul))) How to apply it to older version quickly: Apply the patch and rebuild the kobs-ng in yocto_3.14_x environment: bitbake -c compile -v -f imx-kobs cd tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/imx-kobs/5.0-r0/imx-kobs-5.0 git apply yocto_3_14_x.patch bitbake -c compile -v -f imx-kobs you can find the new binary “kobs-ng” under “tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/imx-kobs/5.0-r0/build/src” Apply the patch and rebuild the kobs-ng in yocto_3.10_53 environment: . ./setup-environment build bitbake -c compile -v -f imx-kobs cd tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/imx-kobs/3.10.53-1.1.0-r0/imx-kobs-3.10.53-1.1.0 git apply yocto_3_10_53patch bitbake -c compile -v -f imx-kobs you can find t he new binary “kobs-ng” under tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/imx-kobs/3.10.53-1.1.0-r0/imx-kobs-3.10.53-1.1.0/src As one alternation method, you also can download the whole imx-kobs-5.4 package which yocto_4.1.15 is using to build. wget http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-kobs-5.4.tar.gz
View full article