i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341566 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342877 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342833 
View full article
L5.4.3_1.0.0 release is now available on IMX_SW landing page: BSP Updates and Releases -> Linux ->Linux L5.4.3_1.0.0. Documentation -> Linux -> Linux 5.4.3_1.0.0 Documentation Files available: # Name Description 1 imx-yocto-LF_L5.4.3_1.0.0.zip i.MX L5.4.3_1.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 LF_v5.4.y-1.0.0_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6Solox Linux Binary Demo Files 3 LF_v5.4.y-1.0.0_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 LF_v5.4.y-1.0.0_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 LF_v5.4.y-1.0.0_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  6 LF_v5.4.y-1.0.0_images_MX8MMEVK.zip i.MX 8M Mini EVK Linux Binary Demo Files  7 LF_v5.4.y-1.0.0_images_MX8MNEVK.zip i.MX 8M Nano EVK Linux Binary Demo Files  8 LF_v5.4.y-1.0.0_images_MX8MQEVK.zip i.MX 8M Quad EVK Linux Binary Demo files 9 LF_v5.4.y-1.0.0_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 LF_v5.4.y-1.0.0_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.10.1.tar.gz System Controller Firmware (SCFW) porting kit v1.2.10.1 for L5.4.3_1.0.0   Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 8M Nano EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board   What’s New/Features: Please consult the Release Notes.   Known Issues: For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-zeus ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-zeus      
View full article
[中文翻译版] 见附件   原文链接: i.MX Create Android SDCard Mirror 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343079 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343116 
View full article
[中文翻译版] 见附件   原文链接: Guide to flash an eMMC from SD Card on i.MX6Q SABRE-SD 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343344 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343372 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343273 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343518 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343761 
View full article
Instrumenting A Board To instrument a board, the connection between the power supply and the target device needs to be broken, usually via a series resistor that's placed on the board. Sometimes the inductor needs to be lifted if no series resistor was included on the rail by the board's designer. In the ideal case, through-hole connections were also provided on the board for the connection of these off-board sensors. Here are three close-up photos that show several boards that have been instrumented: In all three cases, the sensors stand in place via the two outer current carrying wires. The middle and right used insulated wires where as the one on the left used bare wires. In all three cases, the sensor's + connection needs to go towards the power supply and the - connection goes to the target device. The outer wires here are 24-26 gauge. (The relatively heavy gauge wire is used to keep the series resistance of inserting a smart sensor to a minimum.) The ground connection is the middle hole of the smart sensor. In the left and middle photos, a 30 gauge wire connects to the middle hole ground connection on the  board. In the right photo, the ground wire was more conveniently added to a big cap just below the bottom of edge of the photo. Here are wider angle view photos of two of the boards above: The sensors on the left are free-standing since the current carrying wires are stiff enough to hold them upright. Care must be taken since too much flexing will cause a wire to break. Too much bending can also cause a short to the board (and that's why insulated wires were used on these boards). The board on the right has the sensors laying parallel to the board. They are not affixed to the board, but a wire is wrapped around the bundle of ribbon cables out of view past the right edge of the photo. For boards without the through hole connections, the smart sensors need to be immobilized to keep from pulling the SMT pads off the board. If there is room on the board or sides of connectors or large components, the sensors may be attached down with foam double-sticky tape (see photo below, sensor affixed on top i.MX7ULP): For boards where there are no convenient unpopulated areas or there are too many sensors, some other means needs to be devised to immoblize the smart sensors. In the left photo below, two inductors per sensor have been flipped and the two sensors inserted to instrument the two rails. The solder pads on the inductors would easily be broken off by any movement of the smart sensors, so a cage with clamps to hold the ribbon cables was 3D printed. On the back side, there is room for the aggregator to be zip tied to the bottom plate, so the instrumented board can be moved as a single unit with minimal flexing of the ribbon cables.
View full article
When you do long test (days or weeks) test on i.MX board and your test fails, you often wants to know what has happen with a JTAG probe. The problem is when you have 50 boards running in parallel, you don't have the budget to have 50 JTAG debug probe. If you do a "hot plug" of your JTAG probe, you have roughly one chance out 2 to reset your board... so you'll have to wait another couple of hour to resee the problem. Anyway to have a reliable JTAG plug with no reset, it is really simple... cut the RESET line on your cable! then you'll still be able to "attach" to your i.MX. On the MEK board, with a 10-pin JTAG connector, you have the cut the cable line 10 of the ribbon cable: On the cable, cut the reset line like this: With my Lauterbach JTAG  probe, when I do a "hot plug" I never have a reset of my i.MX. BR Vincent
View full article
The Linux L4.14.98_1.0.0_GA; and SDK2.5 for 8QM/8QXP Post GA, SDK2.5.1 for 7ULP GA3 release are now available. Linux on IMX_SW web page, Overview -> BSP Updates and Releases -> Linux L4.14.98_2.0.0 SDK on https://mcuxpresso.nxp.com Files available: Linux:  # Name Description 1 imx-yocto-L4.14.98_2.0.0_ga.zip L4.14.98_2.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 L4.14.98_2.0.0_ga_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6Solox Linux Binary Demo Files 3 L4.14.98_2.0.0_ga_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 L4.14.98_2.0.0_ga_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 L4.14.98_2.0.0_ga_images_MX7DSABRESD.zip i.MX 7Dual SABRESD Linux Binary Demo Files  6 L4.14.98_2.0.0_ga_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  7 L4.14.98_2.0.0_ga_images_MX8MMEVK.zip i.MX 8MMini EVK Linux Binary Demo Files  8 L4.14.98_2.0.0_ga_images_MX8MQEVK.zip i.MX 8MQuad EVK Linux Binary Demo files 9 L4.14.98_2.0.0_ga_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 L4.14.98_2.0.0_ga_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.tar.gz System Controller Firmware (SCFW) porting kit of L4.14.98_2.0.0 12 imx-aacpcodec-4.4.5.tar.gz Linux AAC Plus Codec v4.4.5 13 VivanteVTK-v6.2.4.p4.1.7.8.tgz Vivante Tool Kit v6.2.4.p4.1.7.8   SDK: On https://mcuxpresso.nxp.com/, click the Select Development Board, EVK-MCIMX7ULP//MEK-MIMX8QM/MEK-MIMX-8QX to customize the SDK based on your configuration then download the SDK package.  Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD and SABRE-AI Boards MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board What’s New/Features: Please consult the Release Notes.   Known issues For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-sumo ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-sumo#
View full article
The following document contains a list of document, questions and discussions that are relevant in the community based on amount of views. If you are having a problem, doubt or getting started in i.MX processors, you should check the following links to see if your doubt is in there. Yocto Project Freescale Yocto Project main page‌ Yocto Training - HOME‌ i.MX Yocto Project: Frequently Asked Questions‌ Useful bitbake commands‌ Yocto Project Package Management - smart  How to add a new layer and a new recipe in Yocto  Setting up the Eclipse IDE for Yocto Application Development Guide to the .sdcard format  Yocto NFS & TFTP boot  YOCTO project clean  Yocto with a package manager (ex: apt-get)  Yocto Setting the Default Ethernet address and disable DHCP on boot.  i.MX x Building QT for i.MX6  i.MX6/7 DDR Stress Test Tool V3.00  i.MX6DQSDL DDR3 Script Aid  Installing Ubuntu Rootfs on NXP i.MX6 boards  iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP i.MX Design&Tool Lists  Simple GPIO Example - quandry  i.MX6 GStreamer-imx Plugins - Tutorial & Example Pipelines  Streaming USB Webcam over Network  Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53  Linux / Kernel Copying Files Between Windows and Linux using PuTTY  Building Linux Kernel  Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)  load kernel from SD card in U-boot  Changing the Kernel configuration for i.MX6 SABRE  Android  The Android Booting process  What is inside the init.rc and what is it used for.  Others How to use qtmultimedia(QML) with Gstreamer 1.0
View full article
The document descript how to use the win32diskimager to create bootable sdcard.  How to resize sdcard mirror rootfs partition. Ex: fsl-image-validation-imx-imx6qpdlsolox.sdcard
View full article