In FSL i.MX53 reference design, it is configured as: static struct mxc_audio_platform_data sgtl5000_data = { .ssi_num = 1, .src_port = 2, .ext_port = 5, .hp_irq = gpio_to_irq(HEADPHONE_DEC_B), .hp_status = headphone_det_status, .init = mxc_sgtl5000_init, .ext_ram_rx = 1, }; by default. If change the configuration to be : static struct mxc_audio_platform_data sgtl5000_data = { .ssi_num = 0, .src_port = 1, .ext_port = 5, .hp_irq = gpio_to_irq(HEADPHONE_DEC_B), .hp_status = headphone_det_status, .init = mxc_sgtl5000_init, .ext_ram_rx = 1, }; There will prompt "imx_ssi_irq mxc_ssi SISR 8003a3 SIER 180100 fifo_errs=XXXX" constantly, and audio is greatly distorted. The root cause of this issue is that SSI1/3 use SDMA, and also use IPMUX, but there is not the clock dependency between SDMA and IPMUX, so sometimes IPMUX clock is closed automatically. The attached patch may fix this issue. NOTE: If use SSI2 .ssi_num = 1, .src_port = 2, If use SSI1 .ssi_num = 0, .src_port = 1,
View full article