Customer is asking high-capacity external storage(for example >64GB) support on i.MX BSP, ext4 is ok for HC storage, but it can’t be supported by Windows.
Pls find NFTS and exFAT support status on Linux BSP below:
Updated test result on L5.4.70.2.3.0 and L6.1.22:
L5.4.70.2.3.0
1.You can enable ntfs support in kernel config as below, ntfs can be mounted normally, but you can only modify existing file content in disk, you can’t create/delete/rename file on disk.
> File systems > DOS/FAT/NT Filesystems
Log:
root@imx8mpevk:~# mount -t ntfs /dev/sda1 /mnt/fat/
[ 662.732869] ntfs: volume version 3.1.
root@imx8mpevk:~# cp ntfs-3g /mnt/fat/
cp: cannot create regular file '/mnt/fat/ntfs-3g': Permission denied
root@imx8mpevk:~# ls /mnt/fat/
111.png Image_org System Volume Information gpuinfo.sh
root@imx8mpevk:~# vi /mnt/fat/gpuinfo.sh
root@imx8mpevk:~# umount /mnt/fat/
root@imx8mpevk:~#
ntfs file system can be accessed via ntfs-3g in user space as below
//build:
wget https://tuxera.com/opensource/ntfs-3g_ntfsprogs-2017.3.23.tgz
tar zxvf ntfs-3g_ntfsprogs-2017.3.23.tgz
cd ntfs-3g_ntfsprogs-2017.3.23/
source ../../sdk/environment-setup-aarch64-poky-linux
./configure --host=aarch64-linux --build=aarch64-poky-linux --disable-shared --enable-static
make
ls /src/ntfs-3g
//put it into rootfs
cp ntfs-3g /bin
//test log:
root@imx8mpevk:/#
[ 1058.724471] usb 1-1: USB disconnect, device number 4
[ 1062.058613] usb 1-1: new high-speed USB device number 5 using xhci-hcd
[ 1062.214029] usb-storage 1-1:1.0: USB Mass Storage device detected
[ 1062.220986] scsi host0: usb-storage 1-1:1.0
[ 1063.235871] scsi 0:0:0:0: Direct-Access VendorCo ProductCode 2.00 PQ: 0 ANSI: 4
[ 1063.246185] sd 0:0:0:0: [sda] 15728640 512-byte logical blocks: (8.05 GB/7.50 GiB)
[ 1063.254023] sd 0:0:0:0: [sda] Write Protect is off
[ 1063.259164] sd 0:0:0:0: [sda] No Caching mode page found
[ 1063.264540] sd 0:0:0:0: [sda] Assuming drive cache: write through
[ 1063.296946] sda: sda1
[ 1063.300860] sd 0:0:0:0: [sda] Attached SCSI removable disk
root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/
root@imx8mpevk:/# ls /mnt/fat/
README System Volume Information gpu.sh gpuinfo.sh
root@imx8mpevk:/# cp /unit_tests/memtool /mnt/fat/
root@imx8mpevk:/# umount /mnt/fat/
root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/
root@imx8mpevk:/# ls /mnt/fat/
README System Volume Information gpu.sh gpuinfo.sh memtool
root@imx8mpevk:/#
3.exFAT is not supported on this BSP..
L6.1.22(you can check it on L5.15 and above, should be the same)
You can enable ntfs support in kernel config as below, full features can be supported.
> File systems > DOS/FAT/EXFAT/NT Filesystems
Pls use ‘-t ntfs3’ during mounting, otherwise it will be mounted as ‘read-only’
Log:
root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/
root@imx8ulpevk:~# ls /mnt/fat/
111.png Image_org 'System Volume Information'
root@imx8ulpevk:~#
root@imx8ulpevk:~# cp gpuinfo.sh /mnt/fat/
root@imx8ulpevk:~# umount /mnt/fat/
root@imx8ulpevk:~#
root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/
root@imx8ulpevk:~# ls /mnt/fat/
111.png Image_org 'System Volume Information' gpuinfo.sh
root@imx8ulpevk:~#
exFAT has been supported in L6.1.22.
> File systems > DOS/FAT/EXFAT/NT Filesystems
/dev/sda1 on /run/media/sda1 type exfat (rw,relatime,fmask=0022,dmask=0022,iocharset=utf8,errors=remount-ro)
root@imx8ulpevk:~# ls /run/media/sda1
'Certificate of Completion.pdf' carlife.MP4
Image_org example.tflite
L5.4.70_2.3.0 mx8mp_vpu.txt
NXP-5G.mp4 sd.mp4
'System Volume Information' vela.ini
android_p9.0.0_2.1.0-auto-ga_image_8qmek
root@imx8ulpevk:~# ls
Image_org gpuinfo.sh
root@imx8ulpevk:~# cp gpuinfo.sh /run/media/sda1/
root@imx8ulpevk:~# umount /run/media/sda1
root@imx8ulpevk:~#
記事全体を表示