i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the  i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. i.MX 8M Family DDR Tools Overview The i.MX 8M Family DDR Tool is a Windows-based software to help users to do LPDDR4/DDR4/DDR3L training, stress test and DDR initial code generation for u-boot SPL. This page contains the latest releases for the i.MX 8M Family DDR Tools and cover the following SoCs : i.MX 8M Quad and its derivatives i.MX 8M Quadlite and i.MX 8M Dual i.MX 8M Mini Quad and its derivatives i.MX 8M Mini Quadlite/Dual/DualLite/Solo/SoloLite  i.MX 8M Nano Quad and its derivatives i.MX 8M Nano Quadlite/Dual/DualLite/Solo/SoloLite  i.MX 8M Plus   NOTE: For the i.MX 8/8X Family of DDR tools please refer to the: i.MX 8/8X Family DDR Tools Release   The purpose of the i.MX 8M Family DDR Tools is to enable users to generate and test a custom DRAM initialization based on their device configuration (density, number of chip selects, etc.) and board layout (data bus bit swizzling, etc.).  This process equips the user to then proceed with the bring-up of a boot loader and an OS.  Once the OS is brought up, it is recommended to run an OS-based memory test (like Linux memtester) to further verify and test the DDR memory interface.     The i.MX 8M Family DDR Tools consist of: DDR Register Programming Aid (RPA) MSCALE DDR Tool   For more details regarding these DDR tools and their usage, refer to the i.MX 8M DDR Tools User Guide.   i.MX 8M Family DDR Tool    The i.MX 8M Family DDR stress test tool is a Windows-based software tool that is used as a mechanism to verify that the DDR initialization is operational for use with u-boot and OS bring-up. To install the DDR Stress Test, save and extract the zip file mscale_ddr_tool_vXXX_setup.exe.zip   (where 'xxx' is the current version number) and follow the on-screen installation instructions.     i.MX 8M Family DDR Tool Requirements   The tool requires access to the Windows registry, hence users must run it in administrator mode. When users design new i.MX 8M Family boards, please make sure to follow the rules outlined in the respective Hardware Developers Guide and the MSCALE_DDR_Tool_User_Guide, which can help users bring up DDR devices on their respective i.MX 8M boards.   i.MX 8M Family DDR Tool User Guide   The i.MX 8M DDR tool includes the document: MSCALE_DDR_Tool_User_Guide NOTE: Please read the MSCALE_DDR_Tool_User_Guide inside the package carefully before you use this tool.   i.MX8M DDR Tool Revision History   Rev Major Changes* (Features) Comments 3.31 Integration of the workaround for 8MQ ERR051273   3.30 Fix DBI enabled issue for all i.MX 8M series Automatically identify ROHM and PCA9450 PMICs on i.MX 8M Nano board Fix 4GB/8GB memory tester issues   3.20 Add support to i.MX 8M Plus   3.10 Fixe UART communication issues for some specific characters between the PC software and the target board. Fine-tune DDRPHY registers in generated C code.   3.00 Add support to i.MX8M-nano Add support to different PMIC or PMIC configuration Add support to stress test for all DDR frequency points RPA tools for Nano include support for DDR3L, DDR4, and LPDDR4.   Note that the DDR3L and LPDDR4 RPAs contain the name preliminary only to denote that these RPAs are based on internal NXP validation boards where the DDR4 RPA is based on the released EVK.   2.10 Change DDR4 capacity computing method   2.00 Add support to i.MX8M-mini   * Further details available in the release notes   Sample configuration in the .ds script for i.MX 8M debug UART2: ################step 0: configure debug uart port. Assumes use of UART IO Pads.   ##### ##### If using non-UART pads (i.e. using other pads to mux out the UART signals), ##### ##### then it is up to the user to overwrite the following IO register settings   ##### memory set 0x3033023C 32 0x00000000 #IOMUXC_SW_MUX_UART2_RXD memory set 0x30330240 32 0x00000000 #IOMUXC_SW_MUX_UART2_TXD memory set 0x303304A4 32 0x0000000E #IOMUXC_SW_PAD_UART2_RXD memory set 0x303304A8 32 0x0000000E #IOMUXC_SW_PAD_UART2_TXD memory set 0x303304FC 32 0x00000000 #IOMUXC_SW_MUX_UART2_SEL_RXD sysparam set debug_uart   1 #UART index from 0 ('0' = UART1, '1' = UART2, '2' = UART3, '3' = UART4)   Sample configuration in the front of the .ds script for i.MX 8M debug UART3  ################step 0: configure debug uart port. Assumes use of UART IO Pads.   ##### ##### If using non-UART pads (i.e. using other pads to mux out the UART signals), ##### ##### then it is up to the user to overwrite the following IO register settings   ##### memory set 0x30330244 32 0x00000000 #IOMUXC_SW_MUX_UART3_RXD memory set 0x30330248 32 0x00000000 #IOMUXC_SW_MUX_UART3_TXD memory set 0x303304AC 32 0x0000000E #IOMUXC_SW_PAD_UART3_RXD memory set 0x303304B0 32 0x0000000E #IOMUXC_SW_PAD_UART3_TXD memory set 0x30330504 32 0x00000002 #IOMUXC_SW_MUX_UART3_SEL_RXD sysparam set debug_uart   2 #UART index from 0 ('0' = UART1, '1' = UART2, '2' = UART3, '3' = UART4)   Sample configuration in the front of the .ds script for i.MX 8M Mini PMIC configuration: ##############step 0.5: configure I2C port IO pads according to your PCB design.   ##### ########### You can modify the following instructions to adapt to your board PMIC ####### memory set 0x30330214 32 0x00000010  #IOMUXC_SW_MUX_I2C1_SCL memory set 0x30330218 32 0x00000010  #IOMUXC_SW_MUX_I2C1_SDA memory set 0x3033047C 32 0x000000C6 #IOMUXC_SW_PAD_I2C1_SCL memory set 0x30330480 32 0x000000C6  #IOMUXC_SW_PAD_I2C1_SDA sysparam set pmic_cfg 0x004B #bit[7:0] = PMIC addr,bit[15:8]=I2C Bus. Bus index from 0 ('0' = I2C1, '1' = I2C2, '2' = I2C3, '3' = I2C4) sysparam set pmic_set 0x2F01 #bit[7:0] = Reg val, bit[15:8]=Reg addr. #REG(0x2F) = 0x01 sysparam set pmic_set 0x0C02   #REG(0x0C) = 0x02 sysparam set pmic_set 0x171E   #REG(0x17) = 0x1E sysparam set pmic_set 0x0C00   #REG(0x0C) = 0x00 sysparam set pmic_set 0x2F11    #REG(0x2F)=0x11     i.MX 8M Family DDR Register Programming Aid (RPA) The i.MX 8M DDR RPA (or simply RPA) is an Excel spreadsheet tool used to develop DDR initialization for a user’s specific DDR configuration (DDR device type, density, etc.). The RPA generates the DDR initialization(in a separate Excel worksheet tab):   DDR Stress Test Script: This format is used specifically with the DDR stress test by first copying the contents in this worksheet tab and then pasting it to a text file, naming the document with the “.ds” file extension. The user will select this file when executing the DDR stress test. The How to Use Excel worksheet tab provides instructions on using the RPA   i.MX 8M Family DDR Register Programming Aid (RPA): Current Versions To obtain the latest RPAs, please refer to the following links (note, existing RPAs have been removed from this main page and moved to the SoC specific links below): i.MX 8M Quad : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8M-m850D-DDR-Register-Programming-Aid-RPA/ta-p/1172441 i.MX 8M Mini : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443 i.MX 8M Nano: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MNano-m815S-DDR-Register-Programming-Aid-RPA/ta-p/1172444 i.MX 8M Plus: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352   Processor Mask Revisions Memory Supported Latest RPA Version * i.MX 8M Quad & Derivatives All LPDDR4 Rev 33 i.MX 8M Quad & Derivatives All DDR4 Rev 18 i.MX 8M Quad & Derivatives All DDR3L Rev 9 i.MX 8M Mini & Derivatives A0 LPDDR4 Rev 22 i.MX 8M Mini & Derivatives A0 DDR4 Rev 21 i.MX 8M Mini & Derivatives A0 DDR3L Rev 10 i.MX 8M Nano & Derivatives A0 LPDDR4 Rev 9 i.MX 8M Nano & Derivatives A0 DDR4 Rev 12 i.MX 8M Nano & Derivatives A0 DDR3L Rev 6 i.MX 8M Plus & Derivatives A1 LPDDR4 Rev 9 i.MX 8M Plus & Derivatives A1 DDR4 Rev 9 * For the details about the updates, please refer to the Revision History tab of the respective RPA.    To modify the DRAM Frequency for a custom setting refer to iMX 8M Mini Register Programming Aid DRAM PLL setting    Related Resources Links: iMX 8M Mini Register Programming Aid DRAM PLL setting  i.MX 8/8X Series DDR Tool Release  i.MX 6/7 DDR Stress test GUI Tool i.MX 8M Application Processor Related Resources i.MX8M (m850D) DDR Register Programming Aid (RPA)  i.MX8MMini (m845S) DDR Register Programming Aid (RPA)  i.MX8MNano (m815S) DDR Register Programming Aid (RPA) i.MX 8MPlus (m865S) DDR Register Programming Aids (RPA)   i.MX 8ULP DDR tools: i.MX Software and Development Tools | NXP Semiconductors Scroll down to “Other Resources --> Tools --> DDR Tools”  
View full article
Hello everyone, this document will explain on how to use the UUU (Universal Update Utility) tool to flash Linux to an i.MX device (i.MX 8MM).   Requirements:   MX 8M Mini EVK UUU tool documentation, available here Linux Binary Demo Files - i.MX 8MMini EVK UUU 1.2.135 binary Serial console emulator (tera term or putty)   UUU auto script For this example is used the L4.14.98_2.0.0_ga demo image for the i.MX 8MM, inside the demo image we will find the auto script, which by default flash the eMMC of the board, the structure of the script is as following   /***********************************************************************************/ uuu_version 1.2.39   # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk   # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk   # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -offset 0x57c00 SDPU: jump # }   # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -skipspl SDPV: jump # }   FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd mmc dev ${emmc_dev} FB: flash -raw2sparse all fsl-image-validation-imx-imx8mmevk.sdcard FB: flash bootloader imx-boot-imx8mmevk-sd.bin-flash_evk FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB: done /***********************************************************************************/    In short, when the board goes into serial downloader mode UUU downloads the bootloader to internal RAM, once done and uboot is running, through fastboot utility it will flash .sdcard file and uboot to the eMMC on the board.   More information about the protocol UUU use please refer to the UUU documentation (UUU.pdf) section 5 Supported protocol.   Running the tool In order to run the tool the binary of uuu needs to be downloaded, the binary files can be downloaded from the link above, uuu.exe is for Windows and uuu is for Linux. Once downloaded it can be placed inside the same file as the demo image, this so it is easy to run and cleaner on the shell commands.   Windows In windows OS the tool should be run using the Windows PowerShell in administrator mode, once open we will run the next commands: > .\uuu.exe uuu.auto   Linux >$ sudo ./uuu uuu.auto   The tool will start running and should be waiting for any i.MX device to be detected by host pc   Preparing the board For the board to be flashed it is needed to be in download mode, the switch configuration (i.MX 8MM EVK) is as following: SW1101  -  1010XXXXXX SW1102  -  XXXXXXXXX0   Connect a USB cable from the host pc which will run the tool to the USB OTG/TYPE C port, usually specified as download, on the board.   Connect a USB cable from the host to the OTG-to-UART for console output, usually specified as debug, on the board.   Open terminal emulator program with the following settings: Bits per second - 115200 Data bits - 8 Parity - None Stop bits - 1 Flow control - None   Power on the board, the download will start and the serial prompt will show the progress in uboot, wait until the tool show success.   Finally power off the board and change the switch configuration to boot from the eMMC, power on the board again and it should boot successfully!   Built in scripts One can use the built in scripts using the -b option to burn the bootloader  and the rootfs to the target flash, just type the command accordingly to the target flash device.    SD Write bootloader only: Windows: > .\uuu.exe -b sd <bootloader> Linux: $ sudo ./uuu -b sd <bootloader>   Replace <bootloader> for your .imx/.bin file, example using the i.MX 8MM for Windows and Linux respectively below. > .\uur.exe -b sd imx-boot-imx8mmevk-sd.bin-flash_evk $ sudo ./uuu -b sd imx-boot-imx8mmevk-sd.bin-flash_evk    Write whole Linux image Windows: > .\uuu.exe -b sd_all <bootloader> <rootfs>.sdcard Linux: $ sudo ./uuu -b sd_all <bootloader> <rootfs>.sdcard   Replace <bootloader> and <rootfs> for the name of your .imx/.bin and .sdcard files respectively, example using the i.MX 8MM below. > .\uuu.exe -b sd_all  imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard $ sudo ./uuu -b sd_all  imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard   eMMC Write bootloader only Windows: > .\uuu.exe -b emmc <bootloader> Linux: $ sudo ./uuu -b emmc <bootloader>   Example using i.MX 8MM > .\uuu.exe -b emmc imx-boot-imx8mmevk-sd.bin-flash_evk $ sudo ./uuu -b emmc imx-boot-imx8mmevk-sd.bin-flash_evk   Write whole Linux image Windows: > .\uuu.exe -b emmc_all <bootloader> <rootfs>.sdcard Linux: $ sudo ./uuu -b emmc_all <bootloader> <rootfs>.sdcard   Example using i.MX 8MM > .\uuu.exe -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard $ sudo ./uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard   Hope this will helpful for everyone who is starting to use this flashing tool.
View full article
  Just sharing some experiences during the development and studying.   Although, it appears some hardwares, it focuses on software to speed up your developing on your  hardware.     杂记共享一下在开发和学习过程中的经验。    虽然涉及一些硬件,但其本身关注软件,希望这些能加速您在自己硬件上的开发。 07/25/2024 iMX secondary boot collection https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-secondary-boot-collection/ta-p/1916915   07/25/2024 HSM Code-Signing Journey https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244 25JUL2024 - add pkcs11 proxy                         HSM Code-Signing Journey_25JUL2024.pdf                          HSM Code-Signing Journey_25JUL2024.txt   06/06/2024 HSM Code-Signing Journey https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244     02/07/2024 Device Tree Standalone Compile under Windows https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Device-Tree-Standalone-Compile-under-Windows/ta-p/1855271   02/07/2024 i.MX8X security overview and AHAB deep dive i.MX8X security overview and AHAB deep dive - NXP Community   11/23/2023 “Standalone” Compile Device Tree https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Standalone-Compile-Device-Tree/ta-p/1762373     10/26/2023 Linux Dynamic Debug https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Dynamic-Debug/ta-p/1746611   08/10/2023 u-boot environment preset for sdcard mirror u-boot environment preset for sdcard mirror - NXP Community   06/06/2023 all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek all(bootloader, device tree, Linux kernel, rootfs)... - NXP Community     09/26/2022 parseIVT - a script to help i.MX6 Code Signing parseIVT - a script to help i.MX6 Code Signing - NXP Community   Provide  run under windows   09/16/2022   create sdcard mirror under windows create sdcard mirror under windows - NXP Community     08/03/2022   i.MX8MM SDCARD Secondary Boot Demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011     02/16/2022 mx8_ddr_stress_test without UI   https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/mx8-ddr-stress-test-without-UI/ta-p/1414090   12/23/2021 i.MX8 i.MX8X Board Reset https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-i-MX8X-Board-Reset/ta-p/1391130       12/21/2021 regulator userspace-consumer https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/regulator-userspace-consumer/ta-p/1389948     11/24/2021 crypto af_alg blackkey demo crypto af_alg blackkey demo - NXP Community   09/28/2021 u-boot runtime modify Linux device tree(dtb) u-boot runtime modify Linux device tree(dtb) - NXP Community     08/17/2021 gpio-poweroff demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/gpio-poweroff-demo/ta-p/1324306         08/04/2021 How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709       07/14/2021 SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416     04/07/2021 i.MX8QXP eMMC Secondary Boot https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45       03/25/2021 sc_misc_board_ioctl to access the M4 partition from A core side sc_misc_board_ioctl to access the M4 partition fr... - NXP Community     03/17/2021 How to Changei.MX8X MEK+Base Board  Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8X-MEK-Base-Board-Linux-Debug-UART/ba-p/1246779#M43     03/16/2021 How to Change i.MX8MM evk Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938#M40       05/06/2020 Linux fw_printenv fw_setenv to access U-Boot's environment variables Linux fw_printenv fw_setenv to access U-Boot's env... - NXP Community     03/30/2020 i.MX6 DDR calibration/stress for Mass Production https://community.nxp.com/docs/DOC-346065     03/25/2020 parseIVT - a script to help i.MX6 Code Signing https://community.nxp.com/docs/DOC-345998     02/17/2020 Start your machine learning journey from tensorflow playground Start your machine learning journey from tensorflow playground      01/15/2020 How to add  iMX8QXP PAD(GPIO) Wakeup How to add iMX8QXP PAD(GPIO) Wakeup    01/09/2020 Understand iMX8QX Hardware Partitioning By Making M4 Hello world Running Correctly https://community.nxp.com/docs/DOC-345359   09/29/2019 Docker On i.MX6UL With Ubuntu16.04 https://community.nxp.com/docs/DOC-344462   09/25/2019 Docker On i.MX8MM With Ubuntu https://community.nxp.com/docs/DOC-344473 Docker On i.MX8QXP With Ubuntu https://community.nxp.com/docs/DOC-344474     08/28/2019 eMMC5.0 vs eMMC5.1 https://community.nxp.com/docs/DOC-344265     05/24/2019 How to upgrade  Linux Kernel and dtb on eMMC without UUU How to upgrade Linux Kernel and dtb on eMMC without UUU     04/12/2019 eMMC RPMB Enhance and GP https://community.nxp.com/docs/DOC-343116   04/04/2019 How to Dump a GPT SDCard Mirror(Android O SDCard Mirror) https://community.nxp.com/docs/DOC-343079   04/04/2019 i.MX Create Android SDCard Mirror https://community.nxp.com/docs/DOC-343078   04/02/2019: i.MX Linux Binary_Demo Files Tips  https://community.nxp.com/docs/DOC-343075   04/02/2019:       Update Set fast boot        eMMC_RPMB_Enhance_and_GP.pdf   02/28/2019: imx_builder --- standalone build without Yocto https://community.nxp.com/docs/DOC-342702   08/10/2018: i.MX6SX M4 MPU Settings For RPMSG update    Update slide CMA Arrangement Consideration i.MX6SX_M4_MPU_Settings_For_RPMSG_08102018.pdf   07/26/2018 Understand ML With Simplest Code https://community.nxp.com/docs/DOC-341099     04/23/2018:     i.MX8M Standalone Build     i.MX8M Standalone Build.pdf     04/13/2018:      i.MX6SX M4 MPU Settings For RPMSG  update            Add slide CMA Arrangement  Consideration     i.MX6SX_M4_MPU_Settings_For_RPMSG_04132018.pdf   09/05/2017:       Update eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 09/01/2017:       eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 08/30/2017:     Dual LVDS for High Resolution Display(For i.MX6DQ/DLS)     Dual LVDS for High Resolution Display.pdf 08/27/2017:  L3.14.28 Ottbox Porting Notes:         L3.14.28_Ottbox_Porting_Notes-20150805-2.pdf MFGTool Uboot Share With the Normal Run One:        MFGTool_Uboot_share_with_NormalRun_sourceCode.pdf Mass Production with programmer        Mass_Production_with_NAND_programmer.pdf        Mass_Production_with_emmc_programmer.pdf AndroidSDCARDMirrorCreator https://community.nxp.com/docs/DOC-329596 L3.10.53 PianoPI Porting Note        L3.10.53_PianoPI_PortingNote_151102.pdf Audio Codec WM8960 Porting L3.10.53 PianoPI        AudioCodec_WM8960_Porting_L3.10.53_PianoPI_151012.pdf TouchScreen PianoPI Porting Note         TouchScreen_PianoPI_PortingNote_151103.pdf Accessing GPIO From UserSpace        Accessing_GPIO_From_UserSpace.pdf        https://community.nxp.com/docs/DOC-343344 FreeRTOS for i.MX6SX        FreeRTOS for i.MX6SX.pdf i.MX6SX M4 fastup        i.MX6SX M4 fastup.pdf i.MX6 SDCARD Secondary Boot Demo        i.MX6_SDCARD_Secondary_Boot_Demo.pdf i.MX6SX M4 MPU Settings For RPMSG        i.MX6SX_M4_MPU_Settings_For_RPMSG_10082016.pdf Security        Security03172017.pdf    NOT related to i.MX, only a short memo
View full article
Design Check Lists: HW Design Checking List for i.MX6DQSDL HW Design Checking List for i.Mx53 Hardware Design Checklist for i.MX28 HW_Design_Checking_List_for_i.MX6SoloX i.MX6UL Hardware design checklist   DDR Design Tool: I.MX53 DDR3 Script Aid imx53 DDR stress tester V0.042 i.Mx6DQSDL DDR3 Script Aid MX6DQP DDR3 Script Aid i.Mx6DQSDL LPDDR2 Script Aid i.Mx6SL LPDDR2 Script Aid i.MX6SX DDR3 Script Aid I.MX6UL DDR3 Script Aid i.MX6UL_LPDDR2_Script_Aid i.MX6ULL_DDR3_Script_Aid  i.MX6ULL_LPDDR2_Script_Aid  MX6SLL_LPDDR2_Script_Aid  MX6SLL_LPDDR3_Script_Aid  i.MX6 DDR Stress Test Tool V1.0.3 i.MX6/7 DDR Stress Test Tool V3.00 i.MX8MSCALE DDR Tool Release  i.MX8M DDR3L register programming aid  i.MX 8/8X Family DDR Tools Release   Application Notes: MX_Design_Validation_Guide I.MX6 series USB Certification Guides
View full article
Sometimes it is helpful/faster to build a i.MX8MM boot binary outside of the Yocto environment. There are instructions on how to accomplish this on different places, this document tries to provide an example for the i.MX8M Mini LPDDR4 EVK, whenever possible pointing how to build for other boards. For the 8MM SoC a boot image is generated by imx-mkimage tool and requires: - u-boot - ARM trusted firmware image - ddr training firmware 1. Download and Build u-boot: mkdir imx-boot-bin cdimx-boot-bin git clone https://source.codeaurora.org/external/imx/uboot-imx.git cd uboot-imx/ git checkout -b imx_v2019.04_4.19.35_1.1.0 origin/imx_v2019.04_4.19.35_1.1.0 (Optional) Here you can "git log -1" to check that the commit matches SRCREV on the recipe. Next, use the BSP SDK script to setup the cross compilation environment, instructions on how to build it are here. source /opt/fsl-imx-wayland/4.19-warrior/environment-setup-aarch64-poky-linux export ARCH=arm Build make clean Supported boards have configuration files on "configs". Using the LPDDR4 EVK here: make imx8mm_evk_defconfig make 2.   Download and build the ARM Trusted Firmware cd .. git clone https://source.codeaurora.org/external/imx/imx-atf.git cd imx-atf/ git checkout -b imx_4.19.35_1.1.0 origin/imx_4.19.35_1.1.0 (Optional) Again, you can "git log -1" to check that the commit matches SRCREV on the recipe. https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/meta-bsp/recipes-bsp/imx-atf/imx-atf_2.0.bb?h=warrior-4.19.35-1.1.0 Build: make PLAT=imx8mm bl31 If you run into this error: aarch64-poky-linux-ld.bfd: unrecognized option '-Wl,-O1' aarch64-poky-linux-ld.bfd: use the --help option for usage information make: *** [Makefile:712: build/imx8mm/release/bl31/bl31.elf] Error 1 try:  unset LDFLAGS make PLAT=imx8mm bl31 3. Download the LPDDR4 training binaries It is on firmware-imx, recipe is here: https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/meta-bsp/recipes-bsp/firmware-imx?h=warrior-4.19.35-1.1.0 cd .. mkdir firmware-imx cd firmware-imx wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.5.bin chmod a+x firmware-imx-8.5.bin ./firmware-imx-8.5.bin 4. Download imx-mkimage and build the boot image cd .. git clone https://source.codeaurora.org/external/imx/imx-mkimage.git cd imx-mkimage/ git checkout -b imx_4.19.35_1.1.0 origin/imx_4.19.35_1.1.0 (Optional) "git log -1" matches SRCREV on: https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/meta-bsp/recipes-bsp/imx-mkimage/imx-mkimage_git.inc?h=warrior-4.19.35-1.1.0 Now, you can check the build targets and required binaries at iMX8M/soc.mak For the flash_evk for the imx8mm we will need binaries: u-boot: u-boot-spl.bin, u-boot-nodtb.bin, fsl-imx8mm-evk.dtb  ARM trusted firmware: bl31.bin LPDDR4 files: lpddr4_pmu_train_1d_imem.bin lpddr4_pmu_train_1d_dmem.bin lpddr4_pmu_train_2d_imem.bin lpddr4_pmu_train_2d_dmem.bin mkimage for mkimage_uboot Copy all these to imx-mkimage/iMX8M/ cp ../uboot-imx/spl/u-boot-spl.bin iMX8M/ cp ../uboot-imx/u-boot-nodtb.bin iMX8M/ cp ../uboot-imx/arch/arm/dts/fsl-imx8mm-evk.dtb iMX8M/ cp ../imx-atf/build/imx8mm/release/bl31.bin iMX8M/ cp ../firmware-imx/firmware-imx-8.5/firmware/ddr/synopsys/lpddr4_pmu_train_* iMX8M/ cp ../uboot-imx/tools/mkimage iMX8M/mkimage_uboot Build: make SOC=iMX8MM flash_evk Output binary is on ./iMX8M/flash.bin 5. Program on the SD Card: sudo dd if=iMX8M/flash.bin of=/dev/<path to your sd> bs=1024 seek=33
View full article
This document is a user guide for the GStreamer version 1.0 based accelerated solution included in all the i.MX 8 family SoCs supported by NXP BSP L5.4.24_1.1.0. Some instructions assume a host machine running a Linux distribution, such as Ubuntu, connected to i.MX 8 device. These commands were tested using Ubuntu 18.04 LTD, and while Ubuntu is not required on the host machine, other distributions have not been tested. These instructions are targeted for use with the following hardware: • i.MX 8MQ EVK • i.MX 8MN EVK • i.MX 8MN EVK • i.MX 8QXP MEK B0 • i.MX 8QM MEK B0   Release History v1.0 - Mar 2020 - Initial release. v2.0 - Sep 2020: Added the following content: - Mux/Demux Examples - Audio Examples - Image Examples - Transcode Examples - Streaming Examples - Multi-Display Examples - Scaling and Rotation Examples - Zero-copy Examples - Debug Examples Maintainers: . Marco Franchi . Pedro Jardim
View full article
Application Note AN13872  Enabling SWUpdate on i.MX 6ULL, i.MX 8M Mini, and i.MX 93 is available on www.nxp.com    SWUpdate: Embedded Systems become more and more complex. Software for Embedded Systems have new features and fixes can be updated in a reliable way. Most of time, we need OTA(Over-The-Air) to upgrade the system. Like Android has its own update system. Linux also need an update system. SWUpdate project is thought to help to update an embedded system from a storage media or from network. However, it should be mainly considered as a framework, where further protocols or installers (in SWUpdate they are called handlers) can be easily added to the application. Mongoose daemon mode: Mongoose is a daemon mode of SWUpdate that provides a web server, web interface and web application. Mongoose is running on the target board(i.MX8MM EVK/i.MX8QXP MEK).Using Web browser to access it.   Suricatta daemon mode: Suricatta regularly polls a remote server for updates, downloads, and installs them. Thereafter, it reboots the system and reports the update status to the server. The screenshot is SWUpdate scuricatta working with hawkbit server.          
View full article
  This is a detailed programming aid for the registers associated with i.MX 8M Plus DDR initialization. LPDDR4 DDR4  For more details, refer to the main mScale DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467 Please note that this page is only intended to store the RPA spreadsheets. For questions, please create a new community thread.  
View full article
Descriptions on the issue: running “uuu uuu-android-mx8mq-evk-emmc.lst” No any problem, downloading images is OK. running “uuu_imx_android_flash.bat -f imx8mq -a -e” Below lines will be showed on windows console: flash the file of u-boot-imx8mq.imx to the partition of bootloader0 <waiting for any devices>             Then downloading operation stopped. ------------------------------------------------------------------------                 In order to help uses save development time, I tested above 2 commands for downloading images on windows 7 64bit and windows 10 64bit respectively.                 Below is detailed steps for the operation: Hardware Preparations (1) Switch SW802 on i.MX8MQ EMEK, set 1-4 off, 2-3 on i.MX8MQ is at usb serial download mode. (2) Connecting J1701 to PC USB by a USB OTG cable. (3) Connecting J901(usb type c) to PC USB by a USB 3.0 cable. (4) Plugging 12V@3.5A adapter into Power Jack (J902) (5) Power on I.MX8MQ board via SW701 Switch Software Preparations (1) Related windows drivers for i.MX8MQ MEK                 Windows 7 64bit or windows 10 64bit will find new devices and begin to search and install corresponding drivers, like below:                 Probably windows 10 64bit can’t automatically install CP2105 driver from official website of manufacture: https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers                 Then installed it manually. (2) Power off i.MX8MQ MEK (3) Installing winusb driver by zadig                 According to method described in uuu.pdf, download zadig tool from https://zadig.akeo.ie/, and install it to windows 7 64bit . [Note] windows 10 64bit doesn’t need to install winusb driver. Press “Install WCID Driver” Button (4) Downloading Android SDK Manager Download SDK Manager from : http://visualgdb.com/android/install_redir?item=SDK After downloading it, decompress it, and run SDK Manager application: Press OK. Then press “Close” Close SDK Manager Installation Guide . Find the directory of SDK Manager installation, and enter into “platform-tools”, like below: D:\i.MX8-Projects\IMX8MQ-MEK-windows-drivers\android-sdk_r24.4.1-windows\android-sdk-windows\platform-tools Copy items in blue rectangle to C:\windows\system Copy items in red rectangle to C:\windows\system32     Beginning to download android images to I.MX8MQ MEK via UUU Tool (1) Downloading android DEMO images for i.MX8MQ MEK https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/evaluation-kit-for-the-i.mx-8m-applications-processor:MCIMX8M-EVK?tab=Design_Tools_Tab After downloading it, decompress it to a directory.  Like below: (2) Downloading UUU Tool https://github.com/NXPmicro/mfgtools/releases After downloading uuu.exe,  copy it to the directory of android 9.0 demo image , see above. (3) Run command “uuu_imx_android_flash.bat -f imx8mq -a -e” ----Power on i.MX8MQ MEK. ----open a command line window ---open Hyper terminal ( set it 115200 bps) ---run “uuu_imx_android_flash.bat -f imx8mq -a -e”           For windows 10 64bit, downloading images will be done without any errors.    But for windows 7 64bit, downloading images will stop at “ waiting for any devices”.    It means Android ADB driver will be needed. Follow the steps below to solve the problem. Right button, click “update driver” Close it.           Then downloading operations will be automatically continued. OK, done. NXP TIC team Weidong Sun 02-25-2019
View full article
         This document will describe how to add open JDK to i.MX yocto BSP. It will take two versions of Linux BSP as an example, one is the lower version of L4.1.15-2.0.0, the other is the latest version of L4.19.35-1.1.0. Adding openjdk-8 to L4.1.15-2.0.0(Ubuntu 16.04 LTS platform) Before adding an open JDK, you must download L4.1.15-2.0.0 BSP according to the i.MX_Yocto_Project_User's_Guide.pdf, and ensure that it can pass the compilation normally, that is to say, there is no error in the compilation. In this example, BSP is compiled using the following command. # DISTRO=fsl-imx-wayland MACHINE=imx6sxsabresd source fsl-setup-release.sh -b build-wayland # bitbake fsl-image-qt5          Then follow the steps below to add openjdk to the yocto layer:   Fetching openjdk-8 from Yocto website # cd ~/imx-release-bsp # cd sources # git clone git://git.yoctoproject.org/meta-java # cd meta-java # git checkout -b krogoth origin/krogoth  [Comment]    Yocto’s version is described in i.MX_Yocto_Project_User's_Guide.pdf 2. Modifying related configurations (1) build-wayland/conf/local.conf Add following lines to the file: # Possible provider: cacao-initial-native and jamvm-initial-native PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native" # Possible provider: cacao-native and jamvm-native PREFERRED_PROVIDER_virtual/java-native = "cacao-native" # Optional since there is only one provider for now PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native" IMAGE_INSTALL_append = " openjdk-8" Save it and exit (2)build-wayland/conf/bblayers.conf Add java layer to the file, like below: BBLAYERS = " \   ${BSPDIR}/sources/poky/meta \   ${BSPDIR}/sources/poky/meta-poky \   \   ${BSPDIR}/sources/meta-openembedded/meta-oe \   ${BSPDIR}/sources/meta-openembedded/meta-multimedia \   \   ${BSPDIR}/sources/meta-fsl-arm \   ${BSPDIR}/sources/meta-fsl-arm-extra \   ${BSPDIR}/sources/meta-fsl-demos \   ${BSPDIR}/sources/meta-java \ "…… Save it and exit. 3. Build openjdk-8 # cd ~/imx-release-bsp # source setup-environment build-wayland #bitbake openjdk-8 -c fetchall          Fetch all packages related to openjdk-8. [error handling]          During downloading packages, you may encounter errors like the following. (1)Fetch fastjar-0.98.tar.gz errors          The error is caused by invalid web address, we can download it from another link, see below: http://savannah.c3sl.ufpr.br/fastjar/fastjar-0.98.tar.gz copy the link to firefox in Ubuntu platform, and it will be downloaded into ~/Downloads # cd ~/imx-release-bsp/downloads # cp ~/Downloads/ fastjar-0.98.tar.gz ./ # touch fastjar-0.98.tar.gz.done   (2)Fetch “classpath-0.93.tar.gz” error          Download it from : http://mirror.nbtelecom.com.br/gnu/classpath/classpath-0.93.tar.gz And copy it to ~/imx-release-bsp/downloads, and create a file named classpath-0.93.tar.gz.done in the directory. # cd ~/imx-release-bsp/downloads # cp ~/Downloads/ classpath-0.93.tar.gz ./ # touch classpath-0.93.tar.gz.done (3) 8 files with tar.bz2 (hotspot-Java jvm)          These similar errors are very likely to be encountered.          These errors are caused by the bad network environment. You can download these packages manually. These are Java virtual machine source packages, i.e. hotspot JVM [Solution] # mkdir ~/temp # cd temp # wget http://www.multitech.net/mlinux/sources/56b133772ec1.tar.bz2 # wget http://www.multitech.net/mlinux/sources/ac29c9c1193a.tar.bz2 # wget http://www.multitech.net/mlinux/sources/1f032000ff4b.tar.bz2 # wget http://www.multitech.net/mlinux/sources/81f2d81a48d7.tar.bz2 # wget http://www.multitech.net/mlinux/sources/0549bf2f507d.tar.bz2 # wget http://www.multitech.net/mlinux/sources/0948e61a3722.tar.bz2 # wget http://www.multitech.net/mlinux/sources/48c99b423839.tar.bz2 # wget http://www.multitech.net/mlinux/sources/bf0932d3e0f8.tar.bz2          Then create .tar.bz2.done files for each package via touch command   # touch 56b133772ec1.tar.bz2.done # touch ac29c9c1193a.tar.bz2.done # touch 1f032000ff4b.tar.bz2.done # touch 81f2d81a48d7.tar.bz2.done # touch 0549bf2f507d.tar.bz2.done # touch 0948e61a3722.tar.bz2.done # touch 48c99b423839.tar.bz2.done # touch bf0932d3e0f8.tar.bz2.done          Like below:          Then copy these files to ~/ fsl-release-bsp/downloads/ # bitbake openjdk-8 -c compile          After openjdk compilation, you will be prompted as follows:          At last , install openjdk-8 to images # bitbake fsl-image-qt5          Done: [Additional description]          The above method of adding openjdk-8 is the steps after BSP compilation. Users can also add openjdk-8 before BSP compilation, and then compile it with BSP          According to steps in i.MX_Yocto_Project_User's_Guide.pdf, After running the following two commands, users can modify bblayers.conf and local.conf directly.          For example, steps below have been validated: … … # repo sync # cd ~/fsl-release-bsp # DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 # gedit ./conf/bblayers.conf          Add the same contents as above. # gedit ./conf/local.conf          Add the same contents as above. # bitbake fsl-image-gui          During compilation, users may encounter some errors, which can be handled by referring to the methods described above Adding openjdk-8 to L4.19.35-1.1.0(Ubuntu 18.04 LTS Platform) In fact, the steps to add openjdk-8 to l4.19.35 are the same as those described above, and the following steps have been verified. Before adding openjdk-8, i.mx8qxp full image has been compiled with 2 commands below, so we only need to add openjdk-8 here. # DISTRO=fsl-imx-xwayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-xwayland # bitbake imx-image-full # cd sources # git clone git://git.yoctoproject.org/meta-java # cd meta-java # git checkout -b warrior origin/warrior          Release L4.19.35_1.1.0 is released for Yocto Project 2.7 (Warrior). # cd ~/imx-release-bsp-l4.19.35 # source setup-environment build-xwayland-imx8qxpmek # gedit ./conf/bblayers.conf          Add meta-java to it.          ……            ${BSPDIR}/sources/meta-java \          ……          Save and exit. # gedit ./conf/local.conf          Add these lines to it.          # Possible provider: cacao-initial-native and jamvm-initial-native PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native" # Possible provider: cacao-native and jamvm-native PREFERRED_PROVIDER_virtual/java-native = "cacao-native" # Optional since there is only one provider for now PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native" IMAGE_INSTALL_append = " openjdk-8" Save and exit.   # cd ~/imx-release-bsp-l4.19.35/build-xwayland-imx8qxpmek # bitbake openjdk-8 -c fetch # bitbake openjdk-8 -c compile [Errors] [Solution] # gedit ./ tmp/work/x86_64-linux/openjdk-8-native/172b11-r0/jdk8u-33d274a7dda0/hotspot/make/linux/Makefile Comment the following lines: ----------------------------------------- check_os_version: #ifeq ($(DISABLE_HOTSPOT_OS_VERSION_CHECK)$(EMPTY_IF_NOT_SUPPORTED),) #       $(QUIETLY) >&2 echo "*** This OS is not supported:" `uname -a`; exit 1; #endif -----------------------------------------          Then continue # cd ~/imx-release-bsp-l4.19.35/build-xwayland-imx8qxpmek # bitbake openjdk-8 -c compile [comment]          Probably similar errors will be encountered during compiling other packages, we can use the same way like above to solve it, see bellow, please! Done:          At last, install openjdk-8 to images. # bitbake imx-image-full          Installation is done. NXP TIC Team  Weidong Sun 12/31/2019
View full article
    Xenomai is real-time framework, which can run seamlessly side-by-side Linux as a co-kernel system, or natively over mainline Linux kernels (with or without PREEMPT-RT patch). The dual kernel nicknamed Cobalt, is a significant rework of the Xenomai 2.x system. Cobalt implements the RTDM specification for interfacing with real-time device drivers. The native linux version, an enhanced implementation of the experimental Xenomai/SOLO work, is called Mercury. In this environment, only a standalone implementation of the RTDM specification in a kernel module is required, for interfacing the RTDM-compliant device drivers with the native kernel. You can get more detailed information from Home · Wiki · xenomai / xenomai · GitLab       I have ported xenomai 3.1 to i.MX Yocto 4.19.35-1.1.0, and currently support ARM64 and test on i.MX8MQ EVK board. I did over night test( 5 real-time threads + GPU SDK test case) and stress test by tool stress-ng on i.MX8MQ EVK board. It looks lile pretty good. Current version (20200730) also support i.MX8MM EVK.     You need git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-4.19.35-1.1.0-20200818 (which inlcudes all patches and bb file) and add the following variable in conf/local.conf before build xenomai by command bitbake xenomai.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. The following is test result by the command (/usr/xenomai/demo/cyclictest -p 99 -t 5 -m -n -i 1000  -l 100000😞 //Over normal Linux kernel without GPU SDK test case T: 0 ( 4220) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 9 Max: 23 T: 1 ( 4221) P:99 I:1500 C: 66672 Min: 7 Act: 10 Avg: 10 Max: 20 T: 2 ( 4222) P:99 I:2000 C: 50001 Min: 7 Act: 12 Avg: 10 Max: 81 T: 3 ( 4223) P:99 I:2500 C: 39998 Min: 7 Act: 11 Avg: 10 Max: 29 T: 4 ( 4224) P:99 I:3000 C: 33330 Min: 7 Act: 13 Avg: 10 Max: 26 //Over normal Linux kernel with GPU SDK test case T: 0 ( 4177) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 11 Max: 51 T: 1 ( 4178) P:99 I:1500 C: 66673 Min: 7 Act: 12 Avg: 10 Max: 35 T: 2 ( 4179) P:99 I:2000 C: 50002 Min: 7 Act: 12 Avg: 11 Max: 38 T: 3 ( 4180) P:99 I:2500 C: 39999 Min: 7 Act: 12 Avg: 11 Max: 42 T: 4 ( 4181) P:99 I:3000 C: 33330 Min: 7 Act: 12 Avg: 11 Max: 36   //Cobalt with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M --timeout 600s --metrics-brief T: 0 ( 4259) P:50 I:1000 C:3508590 Min:      0 Act:    0 Avg:    0 Max:      42 T: 1 ( 4260) P:50 I:1500 C:2338831 Min:      0 Act:    1 Avg:    0 Max:      36 T: 2 ( 4261) P:50 I:2000 C:1754123 Min:      0 Act:    1 Avg:    1 Max:      42 T: 3 ( 4262) P:50 I:2500 C:1403298 Min:      0 Act:    1 Avg:    1 Max:      45 T: 4 ( 4263) P:50 I:3000 C:1169415 Min:      0 Act:    1 Avg:    1 Max:      22   //Cobalt without GPU SDK test case T: 0 ( 4230) P:50 I:1000 C: 100000 Min: 0 Act: 0 Avg: 0 Max: 4 T: 1 ( 4231) P:50 I:1500 C:   66676 Min: 0 Act: 1 Avg: 0 Max: 4 T: 2 ( 4232) P:50 I:2000 C:   50007 Min: 0 Act: 1 Avg: 0 Max: 8 T: 3 ( 4233) P:50 I:2500 C:   40005 Min: 0 Act: 1 Avg: 0 Max: 3 T: 4 ( 4234) P:50 I:3000 C:   33338 Min: 0 Act: 1 Avg: 0 Max: 5 //Cobalt with GPU SDK test case T: 0 ( 4184) P:99 I:1000 C:37722968 Min: 0 Act: 1 Avg: 0 Max: 24 T: 1 ( 4185) P:99 I:1500 C:25148645 Min: 0 Act: 1 Avg: 0 Max: 33 T: 2 ( 4186) P:99 I:2000 C:18861483 Min: 0 Act: 1 Avg: 0 Max: 22 T: 3 ( 4187) P:99 I:2500 C:15089187 Min: 0 Act: 1 Avg: 0 Max: 23 T: 4 ( 4188) P:99 I:3000 C:12574322 Min: 0 Act: 1 Avg: 0 Max: 29 //Mercury without GPU SDK test case T: 0 ( 4287) P:99 I:1000 C:1000000 Min: 6 Act: 7 Avg: 7 Max: 20 T: 1 ( 4288) P:99 I:1500 C:  666667 Min: 6 Act: 9 Avg: 7 Max: 17 T: 2 ( 4289) P:99 I:2000 C:  499994 Min: 6 Act: 8 Avg: 7 Max: 24 T: 3 ( 4290) P:99 I:2500 C:  399991 Min: 6 Act: 9 Avg: 7 Max: 19 T: 4 ( 4291) P:99 I:3000 C:  333322 Min: 6 Act: 8 Avg: 7 Max: 21 //Mercury with GPU SDK test case T: 0 ( 4222) P:99 I:1000 C:1236790 Min: 6 Act: 7 Avg: 7 Max: 55 T: 1 ( 4223) P:99 I:1500 C:  824518 Min: 6 Act: 7 Avg: 7 Max: 44 T: 2 ( 4224) P:99 I:2000 C:  618382 Min: 6 Act: 8 Avg: 8 Max: 88 T: 3 ( 4225) P:99 I:2500 C:  494701 Min: 6 Act: 7 Avg: 8 Max: 49 T: 4 ( 4226) P:99 I:3000 C:  412247 Min: 6 Act: 7 Avg: 8 Max: 53 //////////////////////////////////////// Update for Yocto L5.4.47 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.47 2.2.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP). You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git,  and git checkout xenomai-5.4.47-2.2.0. You need to add the following variable in conf/local.conf before build xenomai by command bitbake imx-image-multimedia.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.4.70 2.3.0  /////////////////////////////////////////////////////////// New release  for Yocto release L5.4.70 2.3.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP) and i.MX8QM/QXP. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.0. Updating: 1, Support i.MX8QM and i.MX8QXP 2, Fix altency's the issue which uses legacy API to get time   //////////////////////////////////////// update for Yocto L5.4.70 2.3.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-5.4.70-2.3.2. Updating: 1, Enable Xenomai RTDM driver in Linux Kernel 2, Currently CAN, UART, GPIO,  SPI and Ethernet (in debug for RTNet)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf to enable relative device in Xenomai domain, for example rt-imx8mp-flexcan.   //////////////////////////////////////// Update for Yocto L5.4.70 2.3.4  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.4. You need to git clone  https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.4. Updating: 1, Enable RTNet FEC driver 2, Currently CAN, UART, GPIO,  SPI and Ethernet ( FEC Controller)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf and KERNEL_DEVICETREE += " freescale/imx8mm-rt-ddr4-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mmddr4evk.conf to enable rt_fec device in Xenomai domain. Verifying the network connection by RTnet Ping Between i.MX8M Mini EVK and i.MX8M Plus EVK a, Setup test environment 1, Connect ENET1 of  i.MX8M Plus EVK (used as a master) and  ENET of i.MX8M Mini EVK (used as a slave) of  to a switch or hub 2, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Plus EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.101" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -65,7 +65,7 @@ TDMA_MODE="master" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 3, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Mini EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.102" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -59,13 +59,13 @@ STAGE_2_CMDS="" # TDMA mode of the station ("master" or "slave") # Start backup masters in slave mode, it will then be switched to master # mode automatically during startup. -TDMA_MODE="master" +TDMA_MODE="slave" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 4, rename imx8mm-rt-ddr4-evk.dtb to imx8mm-ddr4-evk.dtb in /run/media/mmcblk1p1,  rename imx8mp-rt-evk.dtb to imx8mp-evk.dtb in /run/media/mmcblk1p1, and reboot board. 5, Run the below command on i.MX8M Mini EVK board. cd /usr/xenomai/sbin/ ./rtnet start & 5, Run the below command on i.MX8M Plus EVK board. cd /usr/xenomai/sbin/ ./rtnet start & When you see the log (rt_fec_main 30be0000.ethernet (unnamed net_device) (uninitialized): Link is Up - 100Mbps/Full - flow control rx/tx) and you can run command "./rtroute" to check route table if the slave IP (192.168.100.102) is in route.. b, Verify the network connection using the command below: ./rtping -s 1024 192.168.100.102 //////////////////////////////////////// Update for Yocto L5.10.52 2.1.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.52 2.1.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.52-2.1.0. Updating: 1, Upgrade Xenomai to v3.2 2, Enable Dovetail instead of ipipe. Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch.  Latency testing of Xenomai3.2+Dovetail with isolating CPU 2,3 ( Xenomai 3.2 on 8MM DDR4 EVK with GPU test case (GLES2/S08_EnvironmentMappingRefraction_Wayland) + iperf3 + 2 ping 65000 size + stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief )😞 The following is test result by the command (/usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000) root@imx8mmddr4evk:~# /usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000 # /dev/cpu_dma_latency set to 0us policy: fifo: loadavg: 5.96 6.04 6.03 7/155 1349 T: 0 ( 615) P:50 I:1000 C:63448632 Min: 0 Act: 0 Avg: 0 Max: 55 T: 1 ( 616) P:50 I:1500 C:42299087 Min: 0 Act: 0 Avg: 1 Max: 43 T: 2 ( 617) P:50 I:2000 C:31724315 Min: 0 Act: 0 Avg: 1 Max: 51 T: 3 ( 618) P:50 I:2500 C:25379452 Min: 0 Act: 0 Avg: 1 Max: 53 T: 4 ( 619) P:50 I:3000 C:21149543 Min: 0 Act: 0 Avg: 1 Max: 47 //////////////////////////////////////// Update for Yocto L5.10.72 2.2.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.72 2.2.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.72-2.2.2. Updating: 1, Upgrade Xenomai to v3.2.1 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.15.71 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.15.71 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.15.71-2.2.0. Updating: 1, Upgrade Xenomai to v3.2.2 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai"   //////////////////////////////////////// Update for Yocto L6.1.55 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L6.1.55 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git recipes-rtlinux-xenomai -b Linux-6.1.x Updating: 1, Upgrade Xenomai to v3.2.4 and support i.MX93 2, Enable EVL (aka Xenomai 4) for i.MX93 and legacy i.MX(6/7D/8X/8M) Copy recipes-rtlinux-xenomai to <Yocto folder>/sources/meta-imx/meta-bsp/, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "evl" IMAGE_INSTALL:append += " libevl"  
View full article
The Register Programming Aid (RPA) provides a default DRAM PLL setting (DRAM frequency) based on the default setting supported in u-boot.  It is highly recommended to use the default DRAM frequency settings in the RPA for ease of use and to align with u-boot.  Otherwise, in addition to updating the RPA for the new DRAM frequency, the u-boot SPL code itself will need to be manually updated with the new DRAM PLL setting.   Should the user wish to change the DRAM frequency, the following steps are required:   First, the user needs to update the RPA Register Configuration worksheet tab Device Information table “Clock Cycle Freq (MHz)“ setting to the desired DRAM frequency       2. Next, in the RPA DDR stress test file worksheet tab search for “memory set 0x30360054”.  The address “0x30360054” is for the DRAM PLL register address and its setting needs to be updated to the desired frequency.        Note that there is another place where the DRAM frequency is also updated “freq0 set 0x30360054” but it is automatically updated based on the setting above.    Below is a table of various frequencies to choose from.  For frequencies not listed in the table below, it is up to the user to calculate a new register setting based on the formula:     (24MHz x m)/(p x 2^s)   Where “m” represents the PLL_MAIN_DIV, “p” represents the PLL_PRE_DIV, and “s” represents the PLL_POST_DIV.  NOTE:  The DRAM frequency is double the DRAM PLL frequency DRAM_freq = DRAM_PLL x 2   The DRAM PLL register and bit settings are shown below:          The following table provides examples of the various settings to create the desired frequency:       For example, in the i.MX 8M Mini LPDDR4 RPA where the default DRAM frequency is 1500MHz, let’s assume that the user instead wants 1200MHz.    First, the user changes the RPA Register Configuration worksheet tab Device Information table “Clock Cycle Freq (MHz)“ setting to 1200.   Next, in the RPA DDR stress test file worksheet tab search for “memory set 0x30360054” and replace “0xFA080” (original setting from DRAM frequency 1500MHz) with “0x000C8022” (updated for DRAM frequency 1200MHz).  Note that for a DRAM frequency of 1200MHz, the DRAM PLL is configured for 600MHz, as the DRAM frequency is double the DRAM_PLL.   The steps outlined above are sufficient in order to create a DDR script for use with the DDR stress test tool to run the calibration and execute the DDR stress test.  However, to deploy the generated code in SPL, more steps are needed as the u-boot SPL DDR driver does not automatically change the DRAM PLL according to the generated code. Hence the user will need to manually modify related code in u-boot.  It is highly recommended to work with a software engineer familiar with u-boot when making the following modifications.    3. Modify DRAM PLL configuration in uboot-imx/drivers/ddr/imx8m.c, specifically the code highlighted below (function call dram_pll_init).  Note that the files and file paths in u-boot change frequently, so if this particular file (or file path) does not exist in the current u-boot, simply search for dram_pll_init or ddr_init.   void ddr_init(struct dram_timing_info *dram_timing) { ……    debug("DDRINFO: cfg clk\n");      if (is_imx8mq())           dram_pll_init(DRAM_PLL_OUT_800M);      else          dram_pll_init(DRAM_PLL_OUT_750M); ……  }   In the above code, the user should update the macro “DRAM_PLL_OUT_750M” with the new DRAM PLL value.  Note that the default DRAM_PLL_OUT_750M results in the DRAM frequency of 1500MHz, where the DRAM frequency is double the DRAM PLL (as previously stated above).   For example, if the user desires to run the DRAM at 1200MHz, they would change the above to: dram_pll_init(DRAM_PLL_OUT_600M);   Note that DRAM_PLL_OUT_600M is a supported macro in the dram_pll_init() API.  If the desired DRAM PLL configuration does not exist in dram_pll_init(), you will need to add support in uboot-imx/arch/arm/mach-imx/imx8m.c  (as stated above, if this file path does not exist in the current u-boot simply search for dram_pll_init):   void dram_pll_init(enum dram_pll_out_val pll_val) { …… }   Related Links i.MX8 MSCALE SERIES DDR Tool Release (V3.10) 
View full article
In some cases, i.MX board connect to different module. It has very tiny changes, such as just one gpio different driver strength. We can build an entire new software to handle this requirement. Here we introduce another way, using u-boot to modify the device tree(dtb) at runtime.   Here is u-boot fdt command for  How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709   run loadfdt fdt addr ${fdt_addr_r} fdt print /soc/bus/pinctrl/uart3grp fdt rm /soc/bus/pinctrl/uart3grp fdt print serial2 fdt set serial2 status disabled fdt print serial2 fdt print gpio4 fdt resize fdt mknode gpio4 gpio_hog_demo fdt set gpio4/gpio_hog_demo gpio-hog fdt set gpio4/gpio_hog_demo gpios <7 0> fdt set gpio4/gpio_hog_demo output-high fdt print gpio4 run mmcargs run loadimage booti ${loadaddr} - ${fdt_addr_r} root@imx8mmevk:~# cat /sys/kernel/debug/gpio gpiochip0: GPIOs 0-31, parent: platform/30200000.gpio, 30200000.gpio: gpio-5 ( |PCIe DIS ) out hi gpio-13 ( |ir-receiver ) in hi IRQ ACTIVE LOW gpio-15 ( |cd ) in hi IRQ ACTIVE LOW gpiochip1: GPIOs 32-63, parent: platform/30210000.gpio, 30210000.gpio: gpio-38 ( |? ) out hi gpio-42 ( |reset ) out lo ACTIVE LOW gpio-51 ( |regulator-usdhc2 ) out lo gpiochip2: GPIOs 64-95, parent: platform/30220000.gpio, 30220000.gpio: gpio-80 ( |status ) out hi gpiochip3: GPIOs 96-127, parent: platform/30230000.gpio, 30230000.gpio: gpio-117 ( |PCIe reset ) out hi gpiochip4: GPIOs 128-159, parent: platform/30240000.gpio, 30240000.gpio: gpio-135 ( |gpio_hog_demo ) out hi gpio-141 ( |spi1 CS0 ) out hi ACTIVE LOW gpio-149 ( |wlf,mute ) out hi ACTIVE LOW root@imx8mmevk:~# [ 33.758914] VSD_3V3: disabling dtc_utils-v1.6.1-win-x86_64.zip by msys2   
View full article
This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera options on the i.MX 8 boards. Plus, this document describes some Advanced camera use cases too, such as multiples cameras output using imxcompositor_g2d plugin, GStreamer zero-copy pipelines and V4L2 API extra-controls examples.
View full article
NXP i.MX 8 series of application processors support running ArmV8a 64-bit and ArmV7a 32-bit user space programs.  A Hello World program that prints the size of a long int is cross-compiled as 32-bit and as 64-bit from an Ubuntu host and then each is copied to MCIMX8MQ-EVK and run. Resources: Ubuntu 18.04 LTS Host i.MX 8M Evaluation Kit|NXP  MCIMX8MQ-EVK Linux Binary Demo Files - i.MX 8MQuad EVK L4.9.88_2.0.0_GA release Source Code: Create a file with contents below using your favorite editor, example name hello-sizeInt.c. #include <stdio.h> int main (int argc, char **argv) { printf ("Hello World, size of long int: %zd\n", sizeof (long int)); return 0; }‍‍‍‍‍‍‍ Ubuntu host packages: $ sudo apt-get install -y gcc-arm-linux-gnueabihf $ sudo apt-get install -y gcc-aarch64-linux-gnu‍‍‍‍ Line 1 installs the ArmV7a cross-compile tools: arm-linux-gnueabihf-gcc is used to cross compile on Ubuntu host Line 2 install the ArmV8a cross-compile tools: aarch64-linux-gnu-gcc is used to cross compile on Ubuntu host Create Linux User Space Applications Build each application and use the static option to gcc to include run time libraries. Build ArmV7a 32-bit application: $ arm-linux-gnueabihf-gcc -static hello-sizeInt.c -o hello-armv7a‍-static‍‍ Build ArmV8a 64-bit application: $ aarch64-linux-gnu-gcc -static  hello-sizeInt.c -o hello-armv8a‍-static‍‍ Copy Hello applications from Ubuntu host and run on MCIMX8MQ-EVK Using a SDCARD written with images from L4.9.88_2.0.0 Linux release (see resources for image link), power on EVK with Ethernet connected to network and Serial Console port which was connected to a windows 10 PC. Launched a terminal client (TeraTerm) to access console port. Login credentials: root and no password needed. Since Ethernet was connected a DHCP IP address was acquired, 192.168.1.241 on the EVK.  On the Ubuntu host, secure copy the hello applications to EVK: $ scp hello-armv7a-static root@192.168.1.241:~/ hello-armv7a-static                           100%  389KB   4.0MB/s   00:00    $ scp hello-armv8a-static root@192.168.1.241:~/ hello-armv8a-static                           100%  605KB   4.7MB/s   00:00 ‍‍‍‍‍‍‍‍‍‍ Run: root@imx8mqevk:~# ./hello-armv8a-static Hello World, sizeof long int: 8 root@imx8mqevk:~# ./hello-armv7a-static Hello World, sizeof long int: 4‍‍‍‍‍‍‍‍
View full article
  Test environment   i.MX8MP EVK LVDS0 LVDS-HDMI  bridge(it6263) Uboot2022, Uboot2023 Background   Some customers need show logo using LVDS panel. Current BSP doesn't support LVDS driver in Uboot. This patch provides i.MX8MPlus LVDS driver support in Uboot. If you want to connect it to LVDS panel , you need port your lvds panel driver like  simple-panel.c   Update [2022.9.19] Verify on L5.15.32_2.0.0  0001-L5.15.32-Add-i.MX8MP-LVDS-driver-in-uboot 'probe device is failed, ret -2, probe video device failed, ret -19' is caused by below code. It has been merged in attachment. // /* Only handle devices that have a valid ofnode */ // if (dev_has_ofnode(dev) && !(dev->driver->flags & DM_FLAG_IGNORE_DEFAULT_CLKS)) { // /* // * Process 'assigned-{clocks/clock-parents/clock-rates}' // * properties // */ // ret = clk_set_defaults(dev, CLK_DEFAULTS_PRE); // if (ret) // goto fail; // }   [2023.3.14] Verify on L5.15.71 0001-L5.15.71-Add-i.MX8MP-LVDS-support-in-uboot   [2023.9.12] For some panel with low DE, you need uncomment CTRL_INV_DE line and set this bit to 1. #include <linux/string.h> @@ -110,9 +111,8 @@ static void lcdifv3_set_mode(struct lcdifv3_priv *priv, writel(CTRL_INV_HS, (ulong)(priv->reg_base + LCDIFV3_CTRL_SET)); /* SEC MIPI DSI specific */ - writel(CTRL_INV_PXCK, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); - writel(CTRL_INV_DE, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); - + //writel(CTRL_INV_PXCK, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); + //writel(CTRL_INV_DE, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); }       [2024.5.15] If you are uing simple-panel.c, need use below patch to set display timing from panel to lcdif controller. diff --git a/drivers/video/simple_panel.c b/drivers/video/simple_panel.c index f9281d5e83..692c96dcaa 100644 --- a/drivers/video/simple_panel.c +++ b/drivers/video/simple_panel.c @@ -18,12 +18,27 @@ struct simple_panel_priv { struct gpio_desc enable; }; +/* define your panel timing here and + * copy it in simple_panel_get_display_timing */ +static const struct display_timing boe_ev121wxm_n10_1850_timing = { + .pixelclock.typ = 71143000, + .hactive.typ = 1280, + .hfront_porch.typ = 32, + .hback_porch.typ = 80, + .hsync_len.typ = 48, + .vactive.typ = 800, + .vfront_porch.typ = 6, + .vback_porch.typ = 14, + .vsync_len.typ = 3, +}; + @@ -100,10 +121,18 @@ static int simple_panel_probe(struct udevice *dev) return 0; } +static int simple_panel_get_display_timing(struct udevice *dev, + struct display_timing *timings) +{ + memcpy(timings, &boe_ev121wxm_n10_1850_timing, sizeof(*timings)); + + return 0; +} static const struct panel_ops simple_panel_ops = { .enable_backlight = simple_panel_enable_backlight, .set_backlight = simple_panel_set_backlight, + .get_display_timing = simple_panel_get_display_timing, }; static const struct udevice_id simple_panel_ids[] = { @@ -115,6 +144,7 @@ static const struct udevice_id simple_panel_ids[] = { { .compatible = "lg,lb070wv8" }, { .compatible = "sharp,lq123p1jx31" }, { .compatible = "boe,nv101wxmn51" }, + { .compatible = "boe,ev121wxm-n10-1850" }, { } };   [2024.7.23] Update patch for L6.6.23(Uboot2023)
View full article
Tested on Android 10 (android_Q10.0.0_1.0.0) After your the first BSP build the kernel sources are at: ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/ For the i.MX8M Mini, You can check the defconfig files being used on: ${MY_ANDROID}/device/fsl/imx8m/evk_8mm/UbootKernelBoardConfig.mk # imx8mm kernel defconfig TARGET_KERNEL_DEFCONFIG := android_defconfig TARGET_KERNEL_ADDITION_DEFCONF := android_addition_defconfig You could change one of them to add the desired configuration. - android_defconfig - is ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/arch/arm64/configs/android_defconfig - android_addition_defconfig - is on the same folder ${MY_ANDROID}/device/fsl/imx8m/evk_8mm/ "merge_config.sh" is called to generate the final defconfig file prior to building the kernel Check out: https://source.android.com/devices/architecture/kernel/config For example, I want to add DEVMEM support on my build: 1. Change the defconfig I add the line below to android_addition_defconfig CONFIG_DEVMEM=y (Or could have added it android_defconfig) 2. Build the kernel ./imx-make.sh kernel -c -j8 3. Verify your change After compiling, you can confirm your change by reading: ${MY_ANDROID}/out/target/product/evk_8mm/obj/KERNEL_OBJ/.config Then rebuild boot.img and reprogram the target.
View full article
The D-PHY PLL (in the red circle in the picture below) is the PLL that drives the MIPI Clock lane. It must be set in accordance with the video to be sent to the display.   Calculating the video bandwidth The video bandwidth is calculated with the following equation: Pixels per second = Horizontal res. x Vertical res. x Frame rate x Bits per pixel Taking as example the 1080p60 OLED display RM67191: Pixels per second = 1920 x 1080 x 60 x 24 Pixels per second = 2985984000 = 2,98Gpixels/sec Pixel clock calculation The Display pixel clock can be obtained on the display driver. In this example for RM67191, the pixel clock is 132Mpixel/sec, see file: panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Line 530: .pixelclock = { 66000000, 132000000, 132000000 }, Or the number can be obtained with the following equation: pixel clock = (hactive + hfront_porch + hsync_len + hback_porch) x (vactive + vfront_porch + vsync_len + vback_porch) x frame rate pixel clock = (1080 + 20 + 2 +34) × (1920 + 10 + 2 + 4) x 60 pixel clock = 132000000 (rounded up) Bit clock calculation (clock lane) The mipi-dphy bit_clk is the output clock and is calculated on file sec-dsim.c (line 1283): sec-dsim.c\bridge\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Bit clock can be calculated with the following equation: bit_clk = Pixel clock * Bits per pixel / Number of lanes In the case of 1980p60 (Raydium display), It is:   bit_clk = pixel clock * bits per pixel / number of lanes bit_clk = 132000000 * 24 / 4 bit_clk = 792000000 Other important timing parameters like 'p', 'm', 's' are obtained on the table in the following header file: sec_mipi_dphy_ln14lpp.h\imx\drm\gpu\drivers - linux-imx - i.MX Linux kernel 
View full article
Host Environment: ubuntu 16.04 LTS Linux BSP For i.MX : version 4.9.88 The document has 5 main contents: 1. Compiling core-image-base in Yocto BSP --Copy u-boot source code to a new directory --Copy linux kernel source code to a new directory 2. Exporting 4.9.88 toolchain from Freescale Yocto BSP (1) Using MACHINE=imx7dsabresd to export the toolchain (2) Using MACHINE=imx6qsabresd to export the toolchain. Actually above 2 are the same toolchain after exporting. Here , only show any one of boards(not ARM64) can be used for MACHINE. So users only need to export it for one time, select (1) or (2) to export toolchain. (3) Using MACHINE=imx8mqevk to export ARM64 toolchain 3. Compling u-boot & linux kernel under Stanalone iMX7DSabreSD --Compiling  u-boot for imx7dsabresd --Compiling kernel and dtb for imx7dsabresd iMX8MQEVK --Compiling u-boot for imx8mqevk --Compiling kernel and dtb for imx8mqevk 4. Compiling OS Firmware for i.MX7DSabreSD board --u-boot for mfg tools --kernel and dtb for mfg tools 5. Copy OS Firmware to the related path of MFG tools --------------------------------------------------------------------------------------------------------------------------- [Content of Document] 1. Compiling core-image-base in Yocto BSP          After repo syn is done according to “i.MX_Yocto_Project_User's_Guide.pdf”, Use the command to compile linux BSP, u-boot & kernel source code will be released. # DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source fsl-setup-release.sh -b build-fb # bitbake core-image-base          After compiling is done, u-boot & linux kernel source code is in the path below: u-boot: ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git linux: ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/git          We can create a new directory for uboot and linux kernel source code. Here I created a directory named disk2. # cd ~/ # mkdir disk2 # cd disk2 # mkdir u-boot-2017-03 # mkdir linux-imx-4.9.88 --Copy u-boot source code to a new directory # cd ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git # cp –r ./* ~/disk2/u-boot-2017-03 --Copy linux kernel source code to a new directory # cd ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/git # cp –r ./* ~/disk2/ linux-imx-4.9.88 2. Exporting 4.9.88 toolchain from Freescale Yocto BSP (1) Using MACHINE=imx7dsabresd to export the toolchain Step1: # cd ~/imx-yocto-bsp/ # DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source fsl-setup-release.sh -b build-minimal … … Do you accept the EULA you just read? (y/n)  y EULA has been accepted. Welcome to Freescale Community BSP The Yocto Project has extensive documentation about OE including a reference manual which can be found at:     http://yoctoproject.org/documentation For more information about OpenEmbedded see their website:     http://www.openembedded.org/ You can now run 'bitbake <target>' Common targets are:     core-image-minimal     meta-toolchain     meta-toolchain-sdk     adt-installer     meta-ide-support Your build environment has been configured with:     MACHINE=imx7dsabresd     SDKMACHINE=i686     DISTRO=fsl-imx-fb     EULA= BSPDIR= BUILD_DIR=. meta-freescale directory found Here “build-minimal” is a directory for compiling source code, users can also set it other name. In ~/imx-yocto-bsp/build-minimal, Begin to export toolchain with the command. Step2: # DISTRO=fsl-imx-fb MACHINE=imx7dsabresd bitbake core-image-minimal -c populate_sdk [Comment-1] About DISTRO and MACHINE on above 2 commands MACHINE can be set the values below. imx6qpsabreauto imx6qpsabresd imx6ulevk imx6ull14x14evk imx6ull9x9evk imx6dlsabreauto imx6dlsabresd imx6qsabreauto imx6qsabresd imx6slevk imx6solosabreauto imx6solosabresd imx6sxsabresd imx6sxsabreauto imx6sllevk imx7dsabresd imx7ulpevk imx8mqevk   So MACHINE’s value is the name each Evaluation Borad. DISTRO can be set the values below: fsl-imx-x11 - X11 graphics are not supported on i.MX 8. fsl-imx-wayland - Wayland weston graphics. fsl-imx-xwayland - Wayland graphics and X11. X11 applications using EGL are not supported. fsl-imx-fb - Frame Buffer graphics - no X11 or Wayland. Frame Buffer is not supported on i.MX 8 bitbake rootfs type       core-image-minimal       core-image-base       core-image-sato       fsl-image-machine-test       fsl-image-validation-imx       fsl-image-qt5-validation-imx Below is the detailed description for above rootfs type: [Comment-2] Descriptions on difference of toolchain between i.MX6/7 and i.MX8MQ          i.MX6 and i.MX7 are both 32bit ARM processor, they use the same toolchain.          i.MX8MQ is 64bit ARM processor, so it’s toolchain is different from that of i.MX6/7. Setp 3:          After above compiling is done, enter into ~/imx-yocto-bsp/build-minimal/tmp/deploy/sdk # cd ~/imx-yocto-bsp/build-minimal/tmp/deploy/sdk # ls Run .sh file: Then continue operations according to guidance: Done: OK, Let us check /opt/fsl-imx-fb/ directory: # ls /opt/fsl-imx-fb/4.9.88-2.0.0/          Because we used MACHINE=imx7dsabresd, environment was named “cortex-A7”, compiler’s version is still 4.9.88. (2) Using MACHINE=imx6qsabresd to export the toolchain.          We can change “MACHINE=imx6qsabresd” and repeat above 3 steps, environment will be named “cortex-A9”.          Close the current terminal, and open a new one. # cd ~/ imx-yocto-bsp # DISTRO=fsl-imx-fb MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-A9-min            Then automatically enter “~/imx-yocto-bsp/build-A9-min”, run command below. # DISTRO=fsl-imx-fb MACHINE=imx6qsabresd bitbake core-image-minimal -c populate_sdk # ~/imx-yocto-bsp/build-A9-min/tmp/deploy/sdk # ls # ./ fsl-imx-fb-glibc-x86_64-core-image-minimal-cortexa9hf-neon-toolchain-4.9.88-2.0.0.sh   Set it up in another directory: /opt/fsl-imx-fb/4.9.88 (3) Using MACHINE=imx8mqevk to export ARM64 toolchain          Export Toolchain for i.MX8MQ, create a new terminal, then run these 2 commands below. # ~/imx-yocto-bsp # DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-xwayland # DISTRO=fsl-imx-fb MACHINE=imx8mqevk bitbake core-image-minimal -c populate_sdk Done.          Copy the toolchain to /opt/fsl-imx-fb directory # cd ~/imx-yocto-bsp/build-xwayland/tmp/deploy/sdk # ls #./fsl-imx-fb-glibc-x86_64-core-image-minimal-aarch64-toolchain-4.9.88-2.0.0.sh          I installed it to a new directory: /opt/fsl-imx-fb/4.9.88-arm64 #ls ls /opt/fsl-imx-fb/4.9.88-arm64/  OK, 64bit toolchain for i.MX8MQ has been exported to the directory. 3. Compling u-boot & linux kernel under Stanalone iMX7DSabreSD --Compiling  u-boot for imx7dsabresd # cd ~/disk2/u-boot-2017-03 # source /opt/fsl-imx-fb/4.9.88-2.0.0/environment-setup-cortexa7hf-neon-poky-linux-gnueabi # export ARCH=arm # make clean # make mx7dsabresd_defconfig # make u-boot.imx Done. --Compiling kernel and dtb for imx7dsabresd # cd ~/disk2/linux-imx-4.9.88/ [comment] If environment has been configured, that is, these 2 commands have been run on the current terminal, don’t need to run them again. “source /opt/fsl-imx-fb/4.9.88-2.0.0/environment-setup-cortexa7hf-neon-poky-linux-gnueabi” and “export ARCH=arm” # make clean # make imx_v7_defconfig # make            zImage is in “~/disk2/linux-imx-4.9.88/arch/arm/boot”          dtb is in “~/disk2/linux-imx-4.9.88/arch/arm/boot/dts”            Probably users want to run “make menuconfig”, and meet the errors like below. # sudo apt-get install libncurses*  (To solve the problem below) # make menuconfig [Comment-3]  Users can also use "environment-setup-cortexa9hf-neon-poky-linux-gnueabi" to compile u-boot and kernel. iMX8MQEVK --Compiling u-boot for imx8mqevk # cd ~/disk2/u-boot-2017-03 # source /opt/fsl-imx-fb/4.9.88-arm64/environment-setup-aarch64-poky-linux # export ARCH=arm64 # make clean # make imx8mq_evk_defconfig # make u-boot.imx Done. --Compiling kernel and dtb for imx8mqevk # cd ~/disk2/linux-imx-4.9.88/ [comment] If environment has been configured, that is, these 2 commands have been run on the current terminal, don’t need to run them again. “source /opt/fsl-imx-fb/4.9.88-arm64/environment-setup-aarch64-poky-linux” and “export ARCH=arm64” # make clean # make defconfig # make          Run the command to unset LDFLAGS: # unset LDFLAGS # make Done. 4. Compiling OS Firmware for i.MX7DSabreSD board --u-boot for mfg tools # make mx7dsabresd_config # make u-boot.imx          Then rename u-boot.imx to be “u-boot-mx7dsabresd-mfg.imx”. --kernel and dtb for mfg tools          Copy imx_v7_mfg_defconfig file to “arch/arm/configs”, then run commands below. # make imx_v7_mfg_defconfig # make          zImage will be generated at path arch/arm/boot.          dtb file will be generated at path arch/arm/boot/dts            Then rename zImage to be zImage-mx7dsabre-mfg,          Rename imx7d-sdb.dtb to be zImage-imx7d-sdb-mfg.dtb 5. Copy OS Firmware to the related path of MFG tools          Up to now, 3 files for OS Firmware has been generated, then copy these 3 files to mfgtools\Profiles\Linux\OS Firmware\firmware            When MFG Tools begins to run, these 3 files and ramdisk will be downloaded to SDRAM on board, then run them, and download images(u-boot\kernel\rootfs\)  which have been ready in  “mfgtools\Profiles\Linux\OS Firmware\files”.            Above steps and commands will be performed according to list in ucl2.xml. So customer will add a new list for her downloading or change an existing list according to image’s name. NXP TIC team Weidong Sun 04-25-2019
View full article