Customer can force PCIE to work at GEN1/GEN2 mode if PCB layout is not good.
Pls refer to:
linux/Documentation/devicetree/bindings/pci/fsl,imx6q-pcie.txt:40:- fsl,max-link-speed: Specify PCI gen for link capability. Must be '2' for
i.MX8M:
diff --git a/arch/arm64/boot/dts/freescale/fsl-imx8mq.dtsi b/arch/arm64/boot/dts/freescale/fsl-imx8mq.dtsi
index f4dcf7ac3c98..262db6f93cb2 100755
--- a/arch/arm64/boot/dts/freescale/fsl-imx8mq.dtsi
+++ b/arch/arm64/boot/dts/freescale/fsl-imx8mq.dtsi
@@ -1314,7 +1314,7 @@
<&clk IMX8MQ_CLK_PCIE1_AUX>,
<&clk IMX8MQ_CLK_PCIE1_PHY>;
clock-names = "pcie", "pcie_bus", "pcie_phy";
- fsl,max-link-speed = <2>;
+ fsl,max-link-speed = <1>;
ctrl-id = <0>;
power-domains = <&pcie0_pd>;
status = "disabled";
@@ -1344,7 +1344,7 @@
<&clk IMX8MQ_CLK_PCIE2_AUX>,
<&clk IMX8MQ_CLK_PCIE2_PHY>;
clock-names = "pcie", "pcie_bus", "pcie_phy";
- fsl,max-link-speed = <2>;
+ fsl,max-link-speed = <1>;
ctrl-id = <1>;
power-domains = <&pcie1_pd>;
status = "disabled";
diff --git a/drivers/pci/dwc/pci-imx6.c b/drivers/pci/dwc/pci-imx6.c
index 54459b52f526..a63de7e7bae0 100644
--- a/drivers/pci/dwc/pci-imx6.c
+++ b/drivers/pci/dwc/pci-imx6.c
@@ -1548,6 +1548,7 @@ static int imx_pcie_establish_link(struct imx_pcie *imx_pcie)
u32 tmp;
int ret;
+ dw_pcie_dbi_ro_wr_en(pci);
/*
* Force Gen1 operation when starting the link. In case the link is
* started in Gen2 mode, there is a possibility the devices on the
i.MX8/8x:
fsl-imx8dx.dtsi
pcieb: pcie@0x5f010000 {
/*
* pcieb phyx1 lane1 in default, adjust it refer to the
* exact hw design.
*/
.
.
.
.
.
power-domains = <&pd_pcie>;
fsl,max-link-speed = <1>; /* 3=gen3, 1=gen1 */
hsio-cfg = <PCIEAX2PCIEBX1>;
hsio = <&hsio>;
ctrl-id = <1>; /* pcieb */
cpu-base-addr = <0x80000000>;
status = "disabled";
};
pci-imx6.c
@@ -1799,6 +1799,7 @@ static int imx_pcie_establish_link(struct imx6_pcie *imx6_pcie)
u32 tmp;
int ret;
+ dw_pcie_dbi_ro_wr_en(pci);
/*
* Force Gen1 operation when starting the link. In case the link is
* started in Gen2 mode, there is a possibility the devices on the
@@ -1870,11 +1871,13 @@ static int imx_pcie_establish_link(struct imx6_pcie *imx6_pcie)
dev_info(dev, "Link: Gen2 disabled\n");
}
+ dw_pcie_dbi_ro_wr_dis(pci);
tmp = dw_pcie_readl_dbi(pci, PCIE_RC_LCSR);
dev_info(dev, "Link up, Gen%i\n", (tmp >> 16) & 0xf);
return 0;
err_reset_phy:
+ dw_pcie_dbi_ro_wr_dis(pci);
dev_dbg(dev, "PHY DEBUG_R0=0x%08x DEBUG_R1=0x%08x\n",
dw_pcie_readl_dbi(pci, PCIE_PORT_DEBUG0),
dw_pcie_readl_dbi(pci, PCIE_PORT_DEBUG1));
View full article