i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
In this article, I will explain how to set up the iMX8M Plus to use the 4K Dart BCON Basler Camera module. Requirements: Evaluation Kit for the i.MX 8M Plus Applications Processor. (i.MX 8M Plus Evaluation Kit | NXP Semiconductors) Basler Camera for i.MX 8M Plus (4K dart BCON for MIPI camera module for i.MX 8M Plus | NXP Semiconductors). Embedded Linux for i.MX Applications Processors (Embedded Linux for i.MX Applications Processors | NXP Semiconductors) (For this example we will use BSP version Linux 5.15.71_2.2.0) Serial Console Emulator Basler Camera Specifications and Manuals: Basler Camera Specifications at this link: Embedded Vision Kits daA3840-30mc-IMX8MP-EVK - Embedded Vision Kits (baslerweb.com). Basler Manual to identify and setting up the hardware at this link: daA3840-30mc-IMX8MP-EVK | Basler Product Documentation (baslerweb.com) Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor. (Video: Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor | NXP Semiconductors) Steps After setting up the hardware we will need to turn on the iMX8M Plus and follow these steps: 1. Stop the boot process on Uboot by pressing any key. 2. Use the following command to list interfaces. => mmc list Output example => FSL_SDHC: 1 (SD) => FSL_SDHC: 2 The above command will show you the device number in this example for SD, the device number is 1. 3. Then use fatls <interface> <device[:partition]> [<directory>] fatls mmc 1:1 (Device 1 : Partition 1) With this command, we will be able to list device tree files. => fatls mmc 1:1 4. Select imx8mp-evk-basler.dtb or imx8mp-evk-dual-basler.dtb and use the command editenv fdtfile.  => editenv fdtfile Output example edit: imx8mp-evk-basler.dtb 5. In edit command line put the selected device tree (*.dtb). 6. Use saveenv command to save environment and continue with the boot process. 7. Using the terminal and go to /opt/imx8-isp/bin and execute the script run.sh. $ ./run.sh -c basler_1080p60 -lm 8. Use the command gst-device-monitor-1.0 to list devices. Here you will find the path to the camera device. $ gst-device-monitor-1.0 Output example Device found: name : VIV class : Video/Source caps : video/x-raw, format=YUY2, width=[ 176, 4096, 16 ], height=[ 144, 3072, 8 ], pixel-aspect-ratio=1/1, framerate={ (fraction)30/1, (fraction)29/1, (fraction)28/1, (fraction)27/1, (fraction)26/1, (fraction)25/1, (fraction)24/1, (fraction)23/1, (fraction)22/1, (fraction)21/1, (fraction)20/1, (fraction)19/1, (fraction)18/1, (fraction)17/1, (fraction)16/1, (fraction)15/1, (fraction)14/1, (fraction)13/1, (fraction)12/1, (fraction)11/1, (fraction)10/1, (fraction)9/1, (fraction)8/1, (fraction)7/1, (fraction)6/1, (fraction)5/1, (fraction)4/1, (fraction)3/1, (fraction)2/1, (fraction)1/1 } ... properties: udev-probed = true device.bus_path = platform-vvcam-video.0 sysfs.path = /sys/devices/platform/vvcam-video.0/video4linux/video2 device.subsystem = video4linux device.product.name = VIV device.capabilities = :capture: device.api = v4l2 device.path = /dev/video2 v4l2.device.driver = viv_v4l2_device v4l2.device.card = VIV v4l2.device.bus_info = platform:viv0 v4l2.device.version = 393473 (0x00060101) v4l2.device.capabilities = 2216693761 (0x84201001) v4l2.device.device_caps = 69206017 (0x04200001) gst-launch-1.0 v4l2src device=/dev/video2 ! ... 9. Finally, use gstreamer to verify proper operation. (With this gstreamer pipeline you will see a new window with the camera output. Then, just rotate the lens to acquire the correct focus) $ gst-launch-1.0 -v v4l2src device=/dev/video2 ! "video/x-raw,format=YUY2,width=1920,height=1080" ! queue ! imxvideoconvert_g2d ! waylandsink Basic description of Gstreamer Pipeline gst-launch-1.0 -v: The option -v enables the verbose mode to get detailed information of process. v4l2src device=/dev/video2: Select input device in this case the camera is on path /dev/video3. "video/x-raw,format=YUY2,width=1920,height=1080": Received format from camera. queue: This command is a buffer between camera recording process and the following image process, this command help us to interface two process and prevent blocking where each process has different speeds, in other words, when a process A is faster than process B. imxvideoconvert_g2d: This proprietary plugin uses hardware acceleration to perform rotation, scaling, and color space conversion on video frames. waylandsink : This command creates its own window and renders the decoded frames processed previously. 10. Result     I hope this article will be helpful. Best regards, Brian.
記事全体を表示
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
記事全体を表示
Platform: i.MX8MP EVK BSP: Linux 5.4.70.2.3.0 Customer reported UI on HDMI monitor is abnormal and has more line on left side when doing HDMI hot-plug on i.MX8MP running with L5.4.70.2.3.0.   This issue can’t be reproduced on latest BSP such as 5.10 and above, several patch for HDMI from latest BSP can fix this issue.  
記事全体を表示
This doc will show: i.MX8DXL EVK board without connect  hardware LCD display, using FreeRDP to share screen to remote PC which is in same network,  PC take this shared screen could  run any command on i.MX8DXL EVK board.   HW: i.MX8DXL EVK board,  PC  SW: i.MX8DXL Linux 5.15.32 BSP release, and code change in this doc   1> i.MX8DXL Linux kernel side, just use imx8dxl-evk-lcdif.dts, but did not connect any LCD display,  so Linux kernel could create related drm device, and weston could be start. But on 8DXL EVK board, ENET1_RGMII_TXD3 and ADMA_LCDIF_D03 pin conflict,  so need code change as 5.15.32-imx8dxl-evk-lcdif.dts.diff.   2> yocto/bld/conf/local.conf, add below line, as freerdp depend on ffmpeg. LICENSE_FLAGS_ACCEPTED+="commercial"   3> For i.MX8DXL,  weston use software pixman render, to use NEON optimization,  pixman need switch to  latest 0.42.0,  enter folder (yocto/bld/tmp/work/armv8a-poky-linux/pixman/1_0.40.0-r0/pixman-0.40.0),  git clone (https://github.com/freedesktop/pixman.git) and checkout to latest 0.42.0:  Also chaneg related build flag at bb file as pixman_0.40.0.bb.diff.     4> Default  freerdp need switch to 2.8.0, enter folder (yocto/bld/tmp/work/armv8a-poky-linux/freerdp/1_2.4.1-r0/git),  git clone (https://github.com/FreeRDP/FreeRDP.git), check out to 2.8.0; And to use neon accelerate freerdp related function, such as color space conversion, image codec encoding ,  need apply patch  freerdp-codechange-neon.diff. And related bb file compile flag change as freerdp_2.4.1.bb.diff     5> bitbake -c compile ffmpeg bitbake -c install ffmpeg   bitbake -c compile pixman  bitbake -c install pixman    bitbake -c compile  freerdp bitbake -c install  freerdp   Copy  generated new libs to default released i.MX8DXL rootfs, make sure ffmeg , pixman, freerdp related libs are  from your build, for example: libfreerdp-client2.so.2 -> libfreerdp-client2.so.2.8.0 libfreerdp2.so.2 -> libfreerdp2.so.2.8.0 libwinpr-tools2.so.2 -> libwinpr-tools2.so.2.8.0 libwinpr2.so.2 -> libwinpr2.so.2.8.0   6> i.MX8DXL Linux rootfs:  file /etc/xdg/weston/weston.ini,  change start-on-startup to true: [screen-share] command=/usr/bin/weston --backend=rdp-backend.so --shell=fullscreen-shell.so --no-clients-resize --rdp-tls-cert=/etc/freerdp/keys/serve start-on-startup=true   7> i.MX8DXL Linux OS, run below cmd: winpr-makecert -path $PWD copy generated files to /etc/freerdp/keys/server.crt and /etc/freerdp/keys/server.key   8> reboot i.MX8DXL EVK board,  make sure  EVK board and PC in the same network; check i.MX8DXL Linux OS , there are two process name as "weston", one process is weston rdp backend to share screen to PC.   9> PC side, get wfreerdp.exe from  https://github.com/FreeRDP/FreeRDP/wiki/Prebuilds PC side run cmd as: wfreerdp.exe /v:ipaddress_of_8DXLEVK     Reference: 1>https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX#design-resources 2>https://github.com/FreeRDP 3>https://github.com/freedesktop/pixman 4>https://github.com/DLTcollab/sse2neon  
記事全体を表示
  Anyone who want to use this solution should get reference design and firmware from Lontium. Hardware Here is the block diagram of LT9611UXC Demo Board. As the MIPI port of our EVK can provide 5V, 3V3 and 1V8.We can remove useless DC-DC chips from reference design. Below is the LT9611UXC Demo Board. Software Download the firmware into LT9611UXC. In Linux side, we need to drive the MIPI to output signals with standard timings of 1080P. Panel type diff --git a/arch/arm64/boot/dts/freescale/imx8mp-evk.dts b/arch/arm64/boot/dts/freescale/imx8mp-evk.dts index 1732b5c72380..c6a829be541f 100644 --- a/arch/arm64/boot/dts/freescale/imx8mp-evk.dts +++ b/arch/arm64/boot/dts/freescale/imx8mp-evk.dts @@ -696,13 +716,17 @@ &ldb_phy { &mipi_dsi { status = "okay"; + panel@0{ + compatible = "nxp,lt9611uxc"; + reg = <0>; + status = "okay"; }; }; &snvs_pwrkey { diff --git a/drivers/gpu/drm/panel/panel-simple.c b/drivers/gpu/drm/panel/panel-simple.c index 4f78bbf63f33..90d99f12515b 100644 --- a/drivers/gpu/drm/panel/panel-simple.c +++ b/drivers/gpu/drm/panel/panel-simple.c @@ -4997,6 +4997,34 @@ struct panel_desc_dsi { unsigned int lanes; }; +static const struct drm_display_mode lt9611_panel_mode = { + .clock = 148500, + .hdisplay = 1920, + .hsync_start = 1920 + 88, + .hsync_end = 1920 + 88 + 44, + .htotal = 1920 + 88 + 44 + 148, + .vdisplay = 1080, + .vsync_start = 1080 + 4, + .vsync_end = 1080 + 4 + 5, + .vtotal = 1080 + 4 + 5 + 36, +}; + +static const struct panel_desc_dsi lt9611_panel = { + .desc = { + .modes = &lt9611_panel_mode, + .num_modes = 1, + .bpc = 8, + .size = { + .width = 62, + .height = 110, + }, + .connector_type = DRM_MODE_CONNECTOR_DSI, + }, + .flags = MIPI_DSI_MODE_VIDEO_HSE | MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_NO_EOT_PACKET | MIPI_DSI_MODE_VIDEO_SYNC_PULSE, + .format = MIPI_DSI_FMT_RGB888, + .lanes = 4, +}; + static const struct drm_display_mode auo_b080uan01_mode = { .clock = 154500, .hdisplay = 1200, @@ -5201,6 +5229,9 @@ static const struct panel_desc_dsi osd101t2045_53ts = { static const struct of_device_id dsi_of_match[] = { { + .compatible = "nxp,lt9611uxc", + .data = &lt9611_panel, + },{ .compatible = "auo,b080uan01", .data = &auo_b080uan01 }, {
記事全体を表示
On behalf of Gopise Yuan. In case some customer may make mistake in mechanical design, they may need to flip/mirror the screen. DPR in DPU can do this in a simple way. This patch demonstrate how to enable VFLIP and HFLIP in DPR to do a V+H flip (=180 rotate) of the screen
記事全体を表示
This is simple known-how for how to implement "boot animation" with DRM under i.MX8/X + Linux:   Code to refer to: ========================================================================= 1. kmscube: Either open source one or the customized on for i.MX will be OK: https://cgit.freedesktop.org/mesa/kmscube/ https://source.codeaurora.org/external/imx/kmscube-imx/ 2. Android display HAL: KmsDisplay.cpp   Known-how: ========================================================================= 1. Only one application can grab the master role of the DRM device. If need to control DRM from two applicaiton simultanously, possible solution:     A, Use "controlD" node instead of "card" node in /dev/dri/. This requires L4.14 or before. This device node was removed by two commits in L4.14.x:           8a357d10043c75e980e7fcdb60d2b913491564af           6449b088dd51dd5aa6b38455888bbf538d21f2fc     Can be brought back by reverting these two commits in L4.14.98.     B, Use framebuffer emulator to emulate a FB device (/dev/fb0). (not recommended due to lack of vsync). 2. Some kernel functions will re-config the DRM device during boot. This will cause display abnormal after user application has configured the DRM device. Better to disable these kernel features:       CONFIG_DRM_FBDEV_EMULATION       CONFIG_FRAMEBUFFER_CONSOLE 3. Use atomic mode of KMS API instead of legacy mode for any dynamically screen drawing application, such as video, game and etc. Atomic mode will have much better performance compare to legacy mode. The kmscube has sample code for both mode. 4. Better to do commit checking before doing any real commit, especially when doing display during boot. Sometimes some internal component in DRM is not fully ready after card device is present.       DRM_MODE_ATOMIC_ALLOW_MODESET 5. If video playback will be used, some points to remind:     a, Sample code for direct video decoding (in unit-test): imx-test/test/mxc_v4l2_vpu_test/     b, VPU in i.MX8/X only support tiled NV12 output and it has pixel alignment requirement (128). Need to use CPU or G2D to do un-tile, CSC and cropping. Sample code: <android>/vendor/nxp/fsl_imx_omx/OpenMAXIL/src/component/v4l2_common/G2dProcess.cpp If using G2D under Linux, it will support un-tile directly (through OpenCL internally).
記事全体を表示
  From L5.4 BSP, the iMX8QM HDMI RX feature is removed from BSP, but it is added back in L5.10.52 2.1.0 BSP. The followed is the detail steps to use HDMI RX.   We need enable the followed kernel config to make hdmirx driver work:     CONFIG_IMX8_MEDIA_DEVICE=y     CONFIG_MHDP_HDMIRX=y apply the attached kernel patch. put hdmi firmware “hdmirxfw.bin” and “hdmitxfw.bin” to SD card’s FAT partition test command:     gst-launch-1.0 v4l2src device=/dev/video2 ! autovideosink   Note: To test the hdmi feature, the display should also use the HDMI TX. And in Uboot, to load the hdmirx firmware, we can run the followed commands first, then run the "boot" command:     run loadhdprx     hdprx load 0x9c800000     setenv fdt_file imx8qm-mek-hdmi-rx.dtb  
記事全体を表示
Use case: iMX8QXP system can be a video input source to another system.   Hardware Pins: LCDIF_D00 ~ LCDIF_D07 LCDIF_CLK LCDIF_VSYNC LCDIF_HSYNC LCDIF_EN   Reference patch: It is based on L5.4.70_2.3.0 GA BSP.  File: L5.4.70_2.3.0-iMX8QXP-LCDIF-add-YUV422-8-bits-output.patch Customer can change the timing parameters in file "panel-lcdif-yuv422.c" as needed, the default timing is a 1280x720 P30 mode: static const struct display_timing yuv422_lcd_timing = {     .pixelclock = { 74250000, 74250000, 74250000 },     .hactive = { 1280, 1280, 1280 },     .hfront_porch = { 220, 220, 220 },     .hback_porch = { 110, 110, 110 },     .hsync_len = { 40, 40, 40 },     .vactive = { 720, 720, 720 },     .vfront_porch = { 20, 20, 20 },     .vback_porch = { 5, 5, 5 },     .vsync_len = { 5, 5, 5 },     .flags = DISPLAY_FLAGS_DE_HIGH, };   Test application: drm_test_yuv.zip: it can set framebuffer to UYVY mode, in this case, no CSC is needed, the data in framebuffer memory will be same as output on display data interface. drm_test_rgb.zip: it can set framebuffer to RGBA mode, in this case, RGB to YUV CSC is needed, application can draw RGB data into framebuffer as normal, the LCDIF will convert it to YUV422 format on the fly, then output the YUV data to display interface.    
記事全体を表示
This doc share one OpenGL ES sample code, it is running on i.MX8 MEK board with QNX SDP7.1. HW: i.MX8 MEK board, HDMI display SW: QNX SDP7.1, i.MX8 MEK board BSP, and this sample code   This sample code will draw 3D object model, and with some animation. Reference: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-8-processors/i-mx-8-family-arm-cortex-a53-cortex-a72-virtualization-vision-3d-graphics-4k-video:i.MX8 https://github.com/NXPmicro/gtec-demo-framework https://github.com/syoyo/tinyobjloader-c https://github.com/nothings/stb https://3dhaupt.com/futuristic-car-game-ready-download/ https://wallpapersafari.com/w/Y5JZNh https://www.pngwing.com/en/free-png-ysaus https://www.shadertoy.com/view/Ms2SWW#
記事全体を表示
For iMX6DQ, there are two IPUs, so they can support up to 4 cameras at the same time. But the default BSP can only support up to two cameras at the same time. The attached patch can make the BSP support up to 4 cameras based on 3.10.53 GA 1.1.0 BSP.   The 4 cameras can be: - 1xCSI, 3xMIPI - 2xCSI, 2xMIPI - 4xMIPI   For 4xMIPI case, the four cameras should be combined on the single MIPI CSI2 interface, and each camera data should be transfered on a mipi virtual channel.   In this patch, we given the example driver for Maxim MAX9286, it was verified working on iMX6DQ SabreAuto board. The input to MAX9286 is four 720P30 cameras. The verified camera boards:     (1) Onsemi AR0140+AP0101+MAX9271 boards.     (2) OmniVision OV10635+MAX9271 boards.   The MIPI CSI2 CVBS camera surround view solution can be found at: iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP The MIPI CSI2 CVBS HD camera surround view solution can be found at: iMX6DQ TP2854 MIPI CSI2 720P CVBS camera surround view solution for Linux BSP   The kernel patches: 0001-IPU-update-IPU-capture-driver-to-support-up-to-four-.patch      Updated IPU common code to support up to four cameras.   0002-Add-Max9286-support-on-SabreAuto-board-which-can-sup.patch      MAX9286 driver, it includes MAX9271, AP0101 and AR0140 drivers.   0003-Remove-the-page-size-align-requirement-for-v4l2-capt.patch      With this patch, the mxc_v4l2_tvin test application can use overlay framebuffer as V4l2 capture buffer directly.   0004-Max9286-skip-AP0101-camera-re-initialization.patch      If the camera board's power had been kept after initialized, this patch will bypass the re-initialization to reduce the start up time.   0005-Max9286-set-I2C-speed-to-400Kbps.patch     Set I2C to 400Kbps to reduce the AP0101+AR0140 initialization time.   0006-Max9286-add-retry-for-MAX9271-I2C-access.patch     Added retry for MAX9271 I2C access.   0007-Max9286-Add-support-for-OV10635-camera.patch     Updated code for OV10635 camera.   0008-Max9286-support-auto-detect-camera-number.patch     Make the Max9286 driver can detect the camera number automatically.     How to builld the kernel with MAX9286 support:       make imx_v7_defconfig       make menuconfig (In this command, you should select the MAX9286 driver:             Device Drivers  --->                   <*> Multimedia support  --->                         [*]   V4L platform devices  --->                               <*>   MXC Video For Linux Video Capture                                       MXC Camera/V4L2 PRP Features support  --->                                           <*>Maxim max9286 GMSL Deserializer Input support                                               Select Camera Sensor (OmniVision OV10635 camera sensor)  // Or (Onsemi AP0101 and AR0140 camera sensor)                                           <*>mxc VADC support                                           <*>Select Overlay Rounting (Queue ipu device for overlay library)                                           <*>Pre-processor Encoder library                                           <*>IPU CSI Encoder library)       make zImage       make dtbs   The built out image file:       arch/arm/boot/dts/imx6q-sabreauto.dtb       arch/arm/boot/zImage   "mxc_v4l2_tvin_max9286.tar.gz" is the test application, test command to capture the four cameras and render on 1080P HDMI display: /mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 0 -ow 960 -oh 540 -d 1 -x 1 -g2d & /mxc_v4l2_tvin.out -ol 0 -ot 540 -ow 960 -oh 540 -d 1 -x 2 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 540 -ow 960 -oh 540 -d 1 -x 3 -g2d &   Some hardware check point on AR0140+AP0101+MAX9271 camera board (Please get MAX9286 and OV10635 schematics from Maxim): 1. In this patch, MAX9286's I2C address is 0x4D, so ADD0 and ADD1 should be connected to high. AP0101's I2C address is 0xBA, so SADDR should be connected to high.   2. AP0101's DOUT0~DOUT7 should be connected to MAX9271's DIN7~DIN0, the order should be switched, MSB connected to LSB.   3. MAX9271's GPO pin should be connected to AP0101's FRAME_SYNC pin. The pull down resistance on FRAME_SYNC pin should not be 0 ohm.   Some known limitation: 1. AP0101's VSYNC invalid time, last video line's HSYNC to VSYNC porch's max value is 255 pixel clocks, it is not enough for MAX9286 to generate the Frame End MIPI packets for each camera. So in order to let iMX6DQ to capture 1280x720 video for each camera, we had let AP0101 output 1280*724 frame size, and iMX6 will only capture 720 lines, the remained video data and Frame End will be ignored. This solution will not impact the function, but there will be "Error matching Frame Start with Frame End for Virtual Channel x" error reported from iMX6 MIPI_CSI_ERR1 register. Maxim suggested to use MAX96705 to relace the MAX9271, it can delay the VSYNC invalid time, then the MIPI error will be fixed.     2015-11-17 update: Updated for OV10635 camera support. File: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2015-11-17.zip   2015-12-04 update: File: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2015-12-04.zip Added patch 0009-Max9286-updated-PCLK-edge-setting-for-OV10635.patch to correct the OV10635 PCLK edge setting     2016-03-07 update: File L3.14.38_GA_MAX9286_Surroundview_Patch_2016-03-07.zip Added kernel patch for L3.14.38 GA 1.1.0 BSP.   2016-07-26 update: Files: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip; L3.14.38_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip; L3.14.52_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip. Added gstreamer support. Added MAX96705 support. Added patch for L3.14.52_GA1.1.0.   2017-12-11 update: Added CVBS surround view link: iMX6DQ TP2854 MIPI CSI2 720P CVBS camera surround view solution for Linux BSP     2021-04-26 update: Some customer reported, when system loading is heavy, sometimes, some camera will flicker left and right. It is caused by SFMC FIFO data lost. The original patch used IDMAC 0 and IDMAC 1 for two cameras on one IPU, this is not the best setting.  IDMAC 1 is fixed to use 1/4 SMFC FIFO and it will cause IDMAC 0 to use 1/4 SMFC FIFO too. And another 1/2 of SMFC FIFO can't be used in this case. Some code update to improve it: For each IPU, please use IDMAC 0 and IDMAC 2 to capture the two cameras. This needs change the hard coding in "drivers\media\platform\mxc\capture\ipu_csi_enc.c", "CSI_MEM1" and "IPU_IRQ_CSI1_OUT_EOF" should be changed to "CSI_MEM2" and "IPU_IRQ_CSI2_OUT_EOF". In this case, all SMFC FIFO can be used. And in "ipu_common.c", function ipu_probe(), the followed code should be changed to make IDMAC2 use high priority too. /* Set sync refresh channels and CSI->mem channel as high priority */ - ipu_idmac_write(ipu, 0x18800003L, IDMAC_CHA_PRI(0)); + ipu_idmac_write(ipu, 0x1880000FL, IDMAC_CHA_PRI(0));
記事全体を表示
In this doc will show how to use i.MX8QXP DPU do image warp.   SW: i.MX Linux BSP L5.4.24_2.1.0 bsp release and patch in this doc HW: i.MX8QXP MEK board, ov5640 camera, HDMI display   Introduction Image Warping is the process of digitally manipulating image data such that the image’s projection precisely matches a specific projection surface or shape.   i.MX8QXP DPU controller could do image warp work by its blit engine and display engine. I choose to enable blit engine’s fetchwarp9 unit to do warp work. Check i.MX8QXP RM, Blit Engine support Image Warp as: “Performs a re-sampling of the source image with any pattern. The sample point positions are read from a compressed coordinate buffer.” So you need prepare two input buffers, one buffer store original image data, the other buffer store resample point coordinate, DPU blit engine will read that two buffer by fetchwarp9 unit, then output result image buffer which contain warped image data. Note i.MX8QXP DPU blit engine fetchwarp9 unit, for the input original image buffer, support RGB and YUV 4:4:4 format. The resample point coordinate buffer contents is depend on what kind warp transformation in your use case; and for each resample point coordinate format check i.MX8QXP RM fecthwarp unit description as below. In this doc, using the 2xs12.4 format, each point x coordinate use (12+4) bit, same as y coordinate.   For DPU fetchwarp9 unit, to enable it work for image warp, check i.MX8QXP RM:   2.Patch notes and test code imx8-dpu-warp-kernel.diff contain the kernel side change for drm ioctl api permission and add vmap function of ion dma_buf_ops. libg2d.so contain the binary for adding warp feature. g2d.h is header file which add define for G2D_WARP and G2D_YUV4. imx8-ov5640-dpu-warp-render.c is a sample code which show how to call g2d lib to image warp, need open the G2D_WARP flag. And this code contain some example calculate the coordinate buffer of rotate, swirl, barrel distortion, affine transformation, perspective transformation, wave transformation. And this code will show read camera input frame then add warp process , then render warp image frame to display.   The test cmd usage as below, read 1080P frame from ov5640 camera, do warp then render warp image to drm plane. Note as dpu fetchwarp9 unit support YUV 4:4:4 input image frame, so below cmd need set parameter YUV4, which will ask ISI driver output YUV 4:4:4 image frame. imx8-ov5640-dpu-warp-render  -i /dev/video0 -f YUV4  -S 1920,1080  -M imx-drm -p 91:38 -F XB24  -b 6  -e g2d  -t 5         -i <video-node> set video node (default: /dev/video0)         -f <fourcc>     set input format using 4cc         -S <width,height>       set input resolution         -s <width,height>@<left,top>    set crop area         -M <drm-module> set DRM module         -o <connector_id>:<crtc_id>:<mode>      set a mode         -p <connector_id>:<crtc_id>     output to a plane         -F <fourcc>     set output format using 4cc         -t <warptype>   set 0 neutual 1 rotate 2 swirl 3 divisionmodel 4 affine 5 perpsptive 6 wave         -b buffer_count set number of buffers        3.Example original image:                     Reference: https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM https://www.nxp.com/webapp/Download?colCode=L5.4.24_2.1.0_MX8QXPC0&appType=license https://en.wikipedia.org/wiki/Image_geometry_correction https://lists.freedesktop.org/archives/dri-devel/2012-March/019778.html https://store.kde.org/p/1246558 https://github.com/ImageMagick/ImageMagick        
記事全体を表示
BSP: L5.4.47-2.2.0-rc2 Board: imx8QM B0 HW:  LVDS2HDMI , MIPIDSI2HDMI. It is the porting of i.MX8QM dpu loopback to isi. to the 5.4.y, with the addition of the MIPI-DSI loopback and the HDMI loopback.  Overview of the DC capture configuration: For enabling the capture: only DC 0 Stream 0  and DC 1 Stream 1 can be captured The pixel link Master address should be set to 3 because the Receiver Address at ISI is 3 and can't be changed. To continue displaying the stream, the Receiver Address at LVDS and DSI or HDMI should be changed to 3. It is possible to change the RA by using GPIO of the modules.   Patches: Create V4L2 device enabling the capture of by the ISI of DC loop-backs. Enable ISI capture from DSI 0 / LVDS 1 in 1920x1080 (at the same time.) Enable ISI capture from HDMI in 2840x2160 (half with even pixel) in 1920x2160. While capturing with the ISI, the captured screen continue to be displayed. Remark: Ov5640 cameras are also enabled in the same dtb. So 4 stream in 1920x1080 can be captured at the same time. Installation and gstreamer command: See readme
記事全体を表示
This document is a user guide for the GStreamer version 1.0 based accelerated solution included in all the i.MX 8 family SoCs supported by NXP BSP L5.4.24_1.1.0. Some instructions assume a host machine running a Linux distribution, such as Ubuntu, connected to i.MX 8 device. These commands were tested using Ubuntu 18.04 LTD, and while Ubuntu is not required on the host machine, other distributions have not been tested. These instructions are targeted for use with the following hardware: • i.MX 8MQ EVK • i.MX 8MN EVK • i.MX 8MN EVK • i.MX 8QXP MEK B0 • i.MX 8QM MEK B0   Release History v1.0 - Mar 2020 - Initial release. v2.0 - Sep 2020: Added the following content: - Mux/Demux Examples - Audio Examples - Image Examples - Transcode Examples - Streaming Examples - Multi-Display Examples - Scaling and Rotation Examples - Zero-copy Examples - Debug Examples Maintainers: . Marco Franchi . Pedro Jardim
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345148 
記事全体を表示
This document describes the i.MX 8MM EVK mini-SAS connectors features on Linux and Android use cases, covering the supported daughter cards, the process to change Device Tree (DTS) files or Boot images, and enable these different display options on the board.
記事全体を表示
This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera options on the i.MX 8 boards. Plus, this document describes some Advanced camera use cases too, such as multiples cameras output using imxcompositor_g2d plugin, GStreamer zero-copy pipelines and V4L2 API extra-controls examples.
記事全体を表示
SW: Linux 4.14.98_2.2.0 bsp release , gpu sdk 5.3.0 and patch in this doc HW: i.MX8QXP MEK board Inspired by the GIMP adjust color curve tool,  I write similar gui test code for i.MX8QXP gamma curve tuning. That is on display will show one linear curve first, use mouse to change any part of this curve, after that calculate value of point on changed curve , then pass related value to i.MX8QXP DPU gammcor unit , at last the display effect will be changed by DPU. When test code start up , will draw Y=X curve on display, that will from (0,0) to (500, 500) to (1023,1023). After you use mouse drag some part of the curve, will generated a new point (x_new, y_new) which is not on original Y=X curve. Then need draw a new curve that pass  through the (0,0) , (500, 500) , (x_new, y_new), (1023,1023).  That new curve , i choose to use Catmull-Rom Splines to get it. Use Catmull-Rom Splines for approximate a curve that pass through n point, then need n+2 control point. Extra 2 point could be selected as you want ,and they will affect the shape of the curve. Catmull-Rom Splines could pass through all control point, it is C1 continuity, no convex hull property. For example, there is four control point p0, p1 , p2 , p3,  to draw the curve pass through all of them, it could divide to segment p0 to p1 , segment p1 to p2 , segment p2 to p3. For segment p1 to p2 , select four control point as p0,p1, p2, p3, use Catmull-Rom Splines as below: For segment p0 to p1 , need use four control point as p0, p0, p1, p2: For segment p2 to p3, need use four control point as p1, p2, p3, p3: In this test code,  i will use gpu vertex shader to calculate each segment of curve, then use transform feedback to read back point value of each segment to cpu side, cpu side will pass related value to DPU gammcor unit for gamma tuning.   Test steps: Apply 8qxp_dpu_gammacor_4.14.98_2.2.0.diff on linux-imx for i.MX8QXP DPU device driver. Apply dpu_gamma_curve_gpusdk5.3.0.diff on imx-gpu-sdk for build this gui test code. Update the new kernel image, and copy test code to rootfs. Run any other application first to draw some thing on screen, for example  /usr/share/cinematicexperience-1.0/Qt5_CinematicExperience. Then run gui test code in this code, S01_SimpleTriangle_Wayland. Then there will show one linear curve on display , use mouse to change the curve as you like by put mouse cursor close to the curve, press the mouse button , drag it and release the mouse button, you will see the new curve on display , and also the display effect also be changed. Reference: 1>https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-8-processors/i-mx-8x-family-arm-cortex-a35-3d-graphics-4k-video-dsp-error-correcting-code-on-ddr:i.MX8X  2>https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab  3>https://github.com/NXPmicro/gtec-demo-framework  4>https://en.wikipedia.org/wiki/Cubic_Hermite_spline  5>http://www.mvps.org/directx/articles/catmull
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342059 
記事全体を表示
This doc show how to use i.MX8QXP Display Controller GammaCor unit to tune gamma. HW: i.MX8QXP MEK board, HDMI monitor SW: i.MX Linux 4.14.98_2.2.0 BSP release, patch in this doc 1.Introduce gamma The gamma, gamma correction, gamma encoding, gamma compression , these words all related one kind operation , see wiki page of it: The device used for image capture/print/display follow this power-law. For example the camera captured image , to view this image on display device as good as original captured image : gamma encoding when camera saved sensor data to image file,  and  gamma decoding when that image file display on your PC LCD monitor. That is : 2. i.MX8QXP Display Controller Gamma Correction Unit The Gamma Correction unit position is located between Frame Gen unit and TCon unit.   More detail see below contents from i.MX8QXP RM: So GammaCor unit could be used as adjust display gamma , or brightness or contrast. To used it, need follow the steps at RM 15.9.2.4.4.8.3.   Something need to note: You need program 33 sample point value into the register, these sample point value range is from 0 to 1023. Note, first write is start sample point value , then the other is delta value: current sample point minus previous sample point value. You can use GammaCor unit on any channel of R/G/B. If you use normalized function f(x), the following formula should be used to clut[i = 0..32] = round( f(i * 32 / 1023) * 1023) 3. i.MX8QXP Linux device driver patch and test code Apply attached  patch 8qxp_dpu_gammacor_4.14.98_2.2.0.diff on Linux kernel. In the kernel patch, function dpu_gammacor_update, I choose not calculate delta value between each sample pint , let user space application calculate delta value and passed to kernel. Apply 8qxp-dpu-gammacor-modetst.diff on libdrm-imx, to get test application which is based on modetest.  Test app will read one greyscale image file 720P.rgb, put it under same folder of test application , calculate sample point value by pow function  , and calling drmModeCrtcSetGamma to pass related value to kernel,  next loop will change sample point value, and will see that greyscale image will changed on HDMI monitor. After system boot up, run below cmd to check result of test application systemctl stop weston ./gamma_show_rgba.out -P 29@32:1280x720@AB24 Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.2.0_MX8QXP&appType=license c> https://source.codeaurora.org/external/imx/libdrm-imx/ d> https://en.wikipedia.org/wiki/Gamma_correction
記事全体を表示