i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
The following are a couple of recommendations for setting up a Host machine for building the Android Nougat 7.1.1_1.0.0 BSP. Some of these recommendations are not exclusive of the Nougat release and may help in other scenarios. These also apply to using Virtual Machines as Host. Installing Open JDK 8 on Ubuntu 14.04 As mentioned on the Android guide for Establishing a Build Environment (http://source.android.com/source/initializing.html) there are no available supported OpenJDK 8 packages for Ubuntu 14.04, which is the version recommended and tested on the Nougat Android BSP. An alternative is downloading the Ubuntu 15.04 Open JDK 8 packages and installing them manually, which can be done by following this procedure: Download the .deb packages for 64-bit architecture from archive.ubuntu.com: openjdk-8-jre-headless_8u45-b14-1_amd64.deb with SHA256 0f5aba8db39088283b51e00054813063173a4d8809f70033976f83e214ab56c0 http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jre-headless_8u45-b14-1_amd64.deb  openjdk-8-jre_8u45-b14-1_amd64.deb with SHA256 9ef76c4562d39432b69baf6c18f199707c5c56a5b4566847df908b7d74e15849 http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jre_8u45-b14-1_amd64.deb  openjdk-8-jdk_8u45-b14-1_amd64.deb with SHA256 6e47215cf6205aa829e6a0a64985075bd29d1f428a4006a80c9db371c2fc3c4c http://archive.ubuntu.com/ubuntu/pool/universe/o/openjdk-8/openjdk-8-jdk_8u45-b14-1_amd64.deb  Once you have downloaded these three packages and checked the checksum for them install the packages (optional) install them by running: $ sudo apt-get update $ sudo dpkg -i openjdk-8-jre-headless_8u45-b14-1_amd64.deb $ sudo dpkg -i openjdk-8-jre_8u45-b14-1_amd64.deb $ sudo dpkg -i openjdk-8-jdk_8u45-b14-1_amd64.deb‍‍‍‍   Increasing SWAP to compensate for the lack of RAM Having insufficient RAM especially on the linking part of the image build may cause a number of issues that are difficult to troubleshoot. In these cases it’s good to take a look at the resource monitor to see if indeed the RAM was depleted. One way to make up for the limited RAM is using a bigger swap. Google recommends at least 16GB of RAM/swap so it’s not uncommon to create a 10GB swap when working in VM, to do this please use the following commands.    $ sudo fallocate -l 10g /mnt/10GB.swap $ sudo chmod 600 /mnt/10GB.swap $ sudo mkswap /mnt/10GB.swap $ sudo swapon /mnt/10GB.swap‍‍‍‍   Increasing heap size to avoid out of memory errors It is possible to encounter an out of memory error with the recommendation “try increasing heap size witj java option ‘-Xmx<size>’. If you encounter this error or would like to proactively avoid it you may run the following commands that will increase heap size to four gigabytes and then reset the Jack Server by killing it and starting it again. With the android environment initialized: $ cd my android $ export JACK_SERVER_VM_ARGUMENTS="-Dfile.encoding=UTF-8 -XX:+TieredCompilation -Xmx4g" $ jack-admin kill-server && jack-admin start-server‍‍‍‍‍‍  Fixing Jack Servers errors due to multiple users on the Host Android Nougat uses Jack Server as mono-user by default. If this is not the case for your host you would need to choose different port numbers for each user and adjust SERVER_NB_COMPILE accordingly. You can also disable the Jack server by setting SERVER=false in your $HOME/.jack. Alternatively, you may also use the patch available on the following link to myandroid/prebuilts/sdk. It will help to fix the mono-user build restriction. When installing the jack-server, it will detect if Jack server is running in the same build machine and then generate a random ports for my build instead of using the default one. https://groups.google.com/forum/#!topic/android-building/UWhJrXH8Vig
記事全体を表示
The decommission of the git.freescale.com has caused some problems to BSPs dependent on packages stored in this repository. All contents on git.freescale.com have been moved to one of three locations: NXP · GitHub  (github.com/NXP) NXP Micro · GitHub  (github.com/NXPMicro) https://source.codeaurora.org/external/imx/   In the case of some older Android BSP this causes an error when fetching the imx-firmware packages originally stored in this repository. A workaround to this is to switch the original location to the new location. To do this we would need to manually create a build directory and initialize repo to locally load the manifest files and then make this change. Android BSP won’t require this workaround. Please note that this workaround only addresses this specific error that may show up when running the script included on the BSP release. We will be using the Oreo o8.0.0_1.0.0_ga BSP release as an example. Sources for this BSP can be found on the following link: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/android-os-for-i-mx-applications-processors:IMXANDROID?tab=Design_Tools_Tab Documentation for this BSP can be found on the following link: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/android-os-for-i-mx-applications-processors:IMXANDROID?tab=Documentation_Tab    1) Initialize the repo. If you have tried running the imx_android_setup.sh script the android build directory should already have been created. If this is the case, please skip to the next step. If not, please create it either by running imx_android_setup.sh or manually with the following commands (using the android setup script is preferred): $ mkdir android_build Once inside the build directory, initialize the repo and then sync it: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest.git -b imx-android-oreo -m imx-o8.0.0_1.0.0_ga.xml $ repo sync   2) Find and edit the Android Manifest. Once inside the build directory after synching, enter the repo manifests directory by executing the following command while inside the android build directory $ cd .repo/manifests  And look for the corresponding Android manifest. In this case imx-o8.0.0_1.0.0_ga.xml Open this file in any text editor (use sudo if running in a directory which requires it) In this case we’ll exemplify with nano $nano imx-o8.0.0_1.0.0_ga.xml And change the git://git.freescale.com/proprietary/  to git://github.com/NXP/ Also the path for imx-firmware so the complete line goes from: <project path="vendor/nxp/imx-firmware" name="imx-firmware" remote="imx-proprietary" revision="87ba304b9efbb2e8dbdd54af4c087584fb259535" />‍‍‍ To the following: <project path="imx-firmware" name="imx-firmware" remote="imx-proprietary" revision="87ba304b9efbb2e8dbdd54af4c087584fb259535" />‍‍‍ The manifest should look like the following. Save the file with these changes.   Now you can run the imx_android_setup.sh build script successfully. Since the repo was already synced it won’t fetch the manifests again and the change we made will persist, which will allow to find the imx-firmware package on its new location.
記事全体を表示
All below changes are done based on imx_android-10.0_5.4.y. mek_8qm enable uSD 8987 wifi            1. hardware rework                no hardware rework required            2. patches The patch is attached as 0001-8qm-usd-8987-wifi.patch mek_8qm enable M.2 8987 wifi            1. hardware rework                no hardware rework required            2. patches The patch is attached as 0001-8qm-m2-8987-wifi.patch evk_8mq enable uSD 8987 wifi            1. hardware rework                no hardware rework required            2. patches diff --git a/imx8m/evk_8mq/BoardConfig.mk b/imx8m/evk_8mq/BoardConfig.mk index db7c4991..4d130cc0 100644 --- a/imx8m/evk_8mq/BoardConfig.mk +++ b/imx8m/evk_8mq/BoardConfig.mk @@ -136,7 +136,8 @@ ifeq ($(TARGET_USE_DYNAMIC_PARTITIONS),true) TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-no-product.dtb else # imx8mq with HDMI display - TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-pcie1-m2.dtb + TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-usd-wifi.dtb + # imx8mq with MIPI-HDMI display TARGET_BOARD_DTS_CONFIG += imx8mq-mipi:imx8mq-evk-lcdif-adv7535.dtb # imx8mq with HDMI and MIPI-HDMI display diff --git a/imx8m/evk_8mq/SharedBoardConfig.mk b/imx8m/evk_8mq/SharedBoardConfig.mk index 330ab1c5..a6654bad 100644 --- a/imx8m/evk_8mq/SharedBoardConfig.mk +++ b/imx8m/evk_8mq/SharedBoardConfig.mk @@ -7,10 +7,10 @@ PRODUCT_IMX_TRUSTY := true #Enable this to disable product partition build. #IMX_NO_PRODUCT_PARTITION := true -#NXP 8997 wifi driver module +# NXP 8987 wifi driver module BOARD_VENDOR_KERNEL_MODULES += \ - $(KERNEL_OUT)/drivers/net/wireless/marvell/mrvl8997/wlan_src/mlan.ko \ - $(KERNEL_OUT)/drivers/net/wireless/marvell/mrvl8997/wlan_src/pcie8xxx.ko + $(KERNEL_OUT)/drivers/net/wireless/nxp/mxm_wifiex/wlan_src/mlan.ko \ + $(KERNEL_OUT)/drivers/net/wireless/nxp/mxm_wifiex/wlan_src/moal.ko # mipi-panel touch driver module BOARD_VENDOR_KERNEL_MODULES += \ diff --git a/imx8m/evk_8mq/UbootKernelBoardConfig.mk b/imx8m/evk_8mq/UbootKernelBoardConfig.mk index 5aa1ce35..4c3378f0 100644 --- a/imx8m/evk_8mq/UbootKernelBoardConfig.mk +++ b/imx8m/evk_8mq/UbootKernelBoardConfig.mk @@ -14,7 +14,7 @@ endif TARGET_BOOTLOADER_CONFIG += imx8mq-evk-uuu:imx8mq_evk_android_uuu_defconfig TARGET_KERNEL_DEFCONFIG := imx_v8_android_defconfig -# TARGET_KERNEL_ADDITION_DEFCONF ?= android_addition_defconfig +TARGET_KERNEL_ADDITION_DEFCONF ?= android_addition_defconfig diff --git a/imx8m/evk_8mq/android_addition_defconfig b/imx8m/evk_8mq/android_addition_defconfig new file mode 100644 index 00000000..f51bd5ff --- /dev/null +++ b/imx8m/evk_8mq/android_addition_defconfig @@ -0,0 +1,2 @@ +CONFIG_WLAN_VENDOR_NXP=y +CONFIG_MXMWIFIEX=m diff --git a/imx8m/evk_8mq/early.init.cfg b/imx8m/evk_8mq/early.init.cfg index 9262d953..70097a1c 100644 --- a/imx8m/evk_8mq/early.init.cfg +++ b/imx8m/evk_8mq/early.init.cfg @@ -1,3 +1,3 @@ insmod vendor/lib/modules/mlan.ko -insmod vendor/lib/modules/pcie8xxx.ko sta_name=wlan uap_name=wlan wfd_name=p2p max_vir_bss=1 cfg80211_wext=0xf cal_data_cfg=none p2p_enh=1 fw_name=pcieuart8997_combo_v4.bin +insmod vendor/lib/modules/moal.ko sta_name=wlan uap_name=wlan wfd_name=p2p max_vir_bss=1 cfg80211_wext=0xf cal_data_cfg=none fw_name=sdiouart8987_combo_v0.bin insmod vendor/lib/modules/synaptics_dsx_i2c.ko diff --git a/imx8m/evk_8mq/evk_8mq.mk b/imx8m/evk_8mq/evk_8mq.mk index 7db1b212..210f8971 100644 --- a/imx8m/evk_8mq/evk_8mq.mk +++ b/imx8m/evk_8mq/evk_8mq.mk @@ -250,9 +250,9 @@ PRODUCT_PACKAGES += \ PRODUCT_PACKAGES += \ bt_vendor.conf -# NXP 8997 Wifi and Bluetooth Combo Firmware +# NXP 8987 Wifi and Bluetooth Combo Firmware PRODUCT_COPY_FILES += \ - vendor/nxp/imx-firmware/nxp/FwImage_8997/pcieuart8997_combo_v4.bin:vendor/firmware/pcieuart8997_combo_v4.bin + vendor/nxp/imx-firmware/nxp/FwImage_8987/sdiouart8987_combo_v0.bin:vendor/firmware/sdiouart8987_combo_v0.bin # Wifi regulatory PRODUCT_COPY_FILES += \ The patch is attached as 0001-8mq-usd-8987-wifi.patch evk_8mq enable M.2 8987 wifi            1. hardware rework                hardware rework required ( Be aware: after this rework, uSD is not working!)            2. patches diff --git a/imx8m/evk_8mq/BoardConfig.mk b/imx8m/evk_8mq/BoardConfig.mk index db7c4991..0cca9b8e 100644 --- a/imx8m/evk_8mq/BoardConfig.mk +++ b/imx8m/evk_8mq/BoardConfig.mk @@ -136,7 +136,8 @@ ifeq ($(TARGET_USE_DYNAMIC_PARTITIONS),true) TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-no-product.dtb else # imx8mq with HDMI display - TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-pcie1-m2.dtb + TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-usdhc2-m2.dtb + # imx8mq with MIPI-HDMI display TARGET_BOARD_DTS_CONFIG += imx8mq-mipi:imx8mq-evk-lcdif-adv7535.dtb # imx8mq with HDMI and MIPI-HDMI display diff --git a/imx8m/evk_8mq/SharedBoardConfig.mk b/imx8m/evk_8mq/SharedBoardConfig.mk index 330ab1c5..a6654bad 100644 --- a/imx8m/evk_8mq/SharedBoardConfig.mk +++ b/imx8m/evk_8mq/SharedBoardConfig.mk @@ -7,10 +7,10 @@ PRODUCT_IMX_TRUSTY := true #Enable this to disable product partition build. #IMX_NO_PRODUCT_PARTITION := true -#NXP 8997 wifi driver module +# NXP 8987 wifi driver module BOARD_VENDOR_KERNEL_MODULES += \ - $(KERNEL_OUT)/drivers/net/wireless/marvell/mrvl8997/wlan_src/mlan.ko \ - $(KERNEL_OUT)/drivers/net/wireless/marvell/mrvl8997/wlan_src/pcie8xxx.ko + $(KERNEL_OUT)/drivers/net/wireless/nxp/mxm_wifiex/wlan_src/mlan.ko \ + $(KERNEL_OUT)/drivers/net/wireless/nxp/mxm_wifiex/wlan_src/moal.ko # mipi-panel touch driver module BOARD_VENDOR_KERNEL_MODULES += \ diff --git a/imx8m/evk_8mq/UbootKernelBoardConfig.mk b/imx8m/evk_8mq/UbootKernelBoardConfig.mk index 5aa1ce35..4c3378f0 100644 --- a/imx8m/evk_8mq/UbootKernelBoardConfig.mk +++ b/imx8m/evk_8mq/UbootKernelBoardConfig.mk @@ -14,7 +14,7 @@ endif TARGET_BOOTLOADER_CONFIG += imx8mq-evk-uuu:imx8mq_evk_android_uuu_defconfig TARGET_KERNEL_DEFCONFIG := imx_v8_android_defconfig -# TARGET_KERNEL_ADDITION_DEFCONF ?= android_addition_defconfig +TARGET_KERNEL_ADDITION_DEFCONF ?= android_addition_defconfig # absolute path is used, not the same as relative path used in AOSP make diff --git a/imx8m/evk_8mq/android_addition_defconfig b/imx8m/evk_8mq/android_addition_defconfig new file mode 100644 index 00000000..f51bd5ff --- /dev/null +++ b/imx8m/evk_8mq/android_addition_defconfig @@ -0,0 +1,2 @@ +CONFIG_WLAN_VENDOR_NXP=y +CONFIG_MXMWIFIEX=m diff --git a/imx8m/evk_8mq/early.init.cfg b/imx8m/evk_8mq/early.init.cfg index 9262d953..70097a1c 100644 --- a/imx8m/evk_8mq/early.init.cfg +++ b/imx8m/evk_8mq/early.init.cfg @@ -1,3 +1,3 @@ insmod vendor/lib/modules/mlan.ko -insmod vendor/lib/modules/pcie8xxx.ko sta_name=wlan uap_name=wlan wfd_name=p2p max_vir_bss=1 cfg80211_wext=0xf cal_data_cfg=none p2p_enh=1 fw_name=pcieuart8997_combo_v4.bin +insmod vendor/lib/modules/moal.ko sta_name=wlan uap_name=wlan wfd_name=p2p max_vir_bss=1 cfg80211_wext=0xf cal_data_cfg=none fw_name=sdiouart8987_combo_v0.bin insmod vendor/lib/modules/synaptics_dsx_i2c.ko diff --git a/imx8m/evk_8mq/evk_8mq.mk b/imx8m/evk_8mq/evk_8mq.mk index 7db1b212..210f8971 100644 --- a/imx8m/evk_8mq/evk_8mq.mk +++ b/imx8m/evk_8mq/evk_8mq.mk @@ -250,9 +250,9 @@ PRODUCT_PACKAGES += \ PRODUCT_PACKAGES += \ bt_vendor.conf -# NXP 8997 Wifi and Bluetooth Combo Firmware +# NXP 8987 Wifi and Bluetooth Combo Firmware PRODUCT_COPY_FILES += \ - vendor/nxp/imx-firmware/nxp/FwImage_8997/pcieuart8997_combo_v4.bin:vendor/firmware/pcieuart8997_combo_v4.bin + vendor/nxp/imx-firmware/nxp/FwImage_8987/sdiouart8987_combo_v0.bin:vendor/firmware/sdiouart8987_combo_v0.bin The patch is attached as 0001-8mq-m2-8987-wifi.patch
記事全体を表示
In order to improve the speed of compilation, VMWare Player 14.0 is installed on local hard disk, and Ubuntu 18.04 LTS is installed on a SSD with at least 500GB size and USB3.1 specification. When installing ubuntu 18.04 LTS to SSD, it should be allocated at least 350GB of disk space, because compiling this version of android requires a larger disk space. The following are detailed compilation steps: Part l Configuring Ubuntu 18.04 LTS 1. Installing Ubuntu 18.04 on VMplayer 14.0 After installation is done, root user should be set at first. # sudo passwd root Then follow these steps to configuration ubuntu 18.04 for environment of compiliation --Changing sources of ubuntu 18.04 mirror If you are Chinese users, you can do the step, which can improve your system performance. # sudo cp /etc/apt/sources.list /etc/apt/sources.list.bak # sudo geit /etc/apt/source.list Comment I.MX customers outside China do not need to modify Ubuntu source list, or can modify it to local mirror site of Ubuntu 18.04, which can improve the speed of software upgrade.    Delet all sources and copy following lines here, Then save it and exit Changing ubuntu source deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse    Then running these 2 commands to update sources and packages    # sudo apt-get update    # sudo apt-get upgrade 2. Installing packages for compiliation Packages for compiliation # sudo apt-get install flex bison gperf build-essential zlib1g-dev lib32ncurses5-dev x11proto-core-dev libx11-dev lib32z1-dev libgl1-mesa-dev tofrodos python-markdown libxml2-utils xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 gcc-multilib g++-multilib subversion openssh-server openssh-client uuid uuid-dev zlib1g-dev liblz-dev lzop liblzo2-2 liblzo2-dev git-core curl # sudo apt-get install u-boot-tools mtd-utils android-tools-fsutils openjdk-8-jdk device-tree-compiler aptitude libcurl4-openssl-dev nss-updatedb # sudo apt-get install chrpath texinfo gawk cpio diffstat gdisk m4 libz-dev libssl-dev Part 2 Compiling Android Q10.0.0_2.1.0 BSP 1. Downloading NXP source code for Android Q10.0.0_2.1.0    File name is imx-android-10.0.0_2.1.0.tar.gz.    Copy the file to ~/, and decompress it.    # cd ~/    # tar zxvf ./imx-android-10.0.0_2.1.0.tar.gz    Then “imx-android-10.0.0_2.1.0” directory is created at ~/, now run the command to download android source code. # source ./imx-android-10.0.0_2.1.0/imx_android_setup.sh Comment imx_android_setup.sh is a script file, which includes all steps needed by the environment of android Q10.0.0_2.1.0 BSP. If network environment is enough good, several hours later, it will be done. 2. Compiling Android Q10.0.0_2.1.0 Referring to steps in Android_User's_Guide.pdf, We summaries steps for compilation here: (1) Preparing cross-compile tool chain    In Android_User's_Guide.pdf, 2 kinds of tool chain are recommended for users. --- gcc-arm-8.3-2019.03-x86_64-aarch64-elf.tar.xz --- gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz    Users can select one of them, and then decompress it to /opt/ directory. On how to download them or more details, see Android_User's_Guide.pdf, page 3. Here we will use gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz as tool chain. (2) Beginning to Compile Android Q10.0.0_2.1.0 BSP    Since this version of Android BSP requires high memory capacity when compiling, if the memory configuration of the virtual machine is incorrect, it is very likely to cause the compilation to fail. The following is a list of variable tests for user reference: # cd android_build # export AARCH64_GCC_CROSS_COMPILE=/opt/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/aarch64-linux-gnu- # source build/envsetup.sh # lunch evk_8mp-userdebug # ./imx-make.sh -j2 2>&1 | tee build-log.txt Part 3 Errors During Compilation 1. Allocating 8GB Memory For VMware Player # ./imx-make.sh -j1 2>&1 | tee build-log.txt 2. Allocating 12GB Memory For VMware Player # ./imx-make.sh -j4 2>&1 | tee build-log.txt # ./imx-make.sh -j4 2>&1 | tee build-log.txt (Run it again) # ./imx-make.sh -j4 2>&1 | tee build-log.txt (Run it again)       So if we use 4 thread to compile BSP, command for compilation will have to be run for 3 times. NXP TIC Team Weidong Sun 2020/4/30
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342877 
記事全体を表示
[中文翻译版] 见附件   原文链接: i.MX Create Android SDCard Mirror 
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343079 
記事全体を表示
Hardware : i.MX8MNLPDDR4EVK Build Yocto Image [Linux 4.14.98_2.3.1] Yocto Project Setup          $: mkdir imx-yocto-bsp          $: cd imx-yocto-bsp                $: repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.3.1.xml          $: repo sync  copy marvell bb.file into yocto source         $: cp  0001-Porting-mrvl-8987-wifi.patch   imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp         $: git apply 0001-Porting-mrvl-8987-wifi.patch Image Build         $: DISTRO=fsl-imx-xwayland MACHINE=imx8mnlpddr4evk source fsl-setup-release.sh -b build-xwayland         $:bitbake fsl-image-qt5-validation-imx Enable wifi and BT (These operations is on EVK) WiFi $:insmod /lib/modules/4.14.98-2.3.1+g860ec89/extra/sd8xxx.ko fw_name=/mrvl/sduart8987_combo.bin cal_data_cfg=none cfg80211_wext=0xf BT $:hciattach /dev/ttymxc0 any -s 115200 115200 flow dtron $:hciconfig hci0 reset $:hcitool -ihci0 cmd 0x3f 0x0009 0xc0 0xc6 0x2d 0x00 & $:killall hcitool $:killall hciattach $:hciattach /dev/ttymxc0 any -s 3000000 3000000 flow dtron Build  Android Image[Android P9_2.3.4] These patches in  Android-2.3.4-patch. Getting i.MX Android release source code        $: cd ~ (or any other directory you like)        $: tar xzvf imx-p9.0.0_2.3.4.tar.gz        $: mkdir ~/bin        $: curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo        $: chmod a+x ~/bin/repo        $: export PATH=${PATH}:~/bin        $: source ~/imx-p9.0.0_2.3.0/imx_android_setup.sh        # By default, the imx_android_setup.sh script will create the source code build environemnt        in the folder ~/android_build        # ${MY_ANDROID} will be refered as the i.MX Android source code root directory in all i.MX        Andorid release documentation.        $ : export MY_ANDROID=~/android_build Copy 88W8987 firmware and driver into  Android release code        $:copy -r Android-2.3.4-patch/mrvl    android_build/vendor/nxp/fsl-proprietary  Apply these patches.The name of these patches is the patche installation path.            example:  0001-android_build-hardware-marvell-wlan.patch         $: cp 0001-android_build-hardware-marvell-wlan.patch   android_build/hardware/marvell/wlan            (if not exist android_build/hardware/marvell/wlan, mkdir -p android_build/hardware/marvell/wlan)         $: git apply 0001-android_build-hardware-marvell-wlan.patch  Building Android images          $: cd  android_build          $: source build/envsetup.sh          $: lunch evk_8mn-userdebug          $: make 
記事全体を表示
Default Ethernet feature is removed for Android Auto (both Android_Pie9.0 and Android10) Below are the patched to bring Ethernet feature back to Android Auto. Please try to apply the according patches if you want to enable Ethernet. For Android_Pie9.0_Auto(example with car2 build): --- a/arch/arm64/configs/android_car2_defconfig +++b/arch/arm64/configs/android_car2_defconfig @@ -245,7 +245,7 @@ CONFIG_DM_VERITY_FEC=y CONFIG_NETDEVICES=y CONFIG_MACVTAP=m CONFIG_TUN=y -# CONFIG_ETHERNET is not set +CONFIG_ETHERNET=y CONFIG_MDIO_BUS_MUX_MMIOREG=m CONFIG_AT803X_PHY=m CONFIG_MARVELL_PHY=m @@ -517,7 +517,7 @@ CONFIG_SQUASHFS=y CONFIG_SQUASHFS_DECOMP_MULTI=y CONFIG_SQUASHFS_XATTR=y CONFIG_SQUASHFS_LZ4=y -# CONFIG_NETWORK_FILESYSTEMS is not set +CONFIG_NETWORK_FILESYSTEMS=y   --- a/imx8q/mek_8q/mek_8q.mk +++ b/imx8q/mek_8q/mek_8q.mk @@ -46,6 +46,7 @@ PRODUCT_COPY_FILES += \      $(IMX_DEVICE_PATH)/fstab.freescale.car:$(TARGET_COPY_OUT_VENDOR)/etc/fstab.freescale \      $(IMX_DEVICE_PATH)/early.init_car.cfg:$(TARGET_COPY_OUT_VENDOR)/etc/early.init.cfg \      $(IMX_DEVICE_PATH)/required_hardware_auto.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/required_hardware.xml \ +    frameworks/native/data/etc/android.hardware.ethernet.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.ethernet.xml \      device/fsl/imx8q/init.recovery.freescale.car.rc:root/init.recovery.freescale.rc   For Android10_Auto,(example with car build): --- a/arch/arm64/configs/android_car_defconfig +++ b/arch/arm64/configs/android_car_defconfig @@ -23,6 +23,8 @@ CONFIG_SCHED_AUTOGROUP=y CONFIG_SCHED_TUNE=y CONFIG_RELAY=y CONFIG_BLK_DEV_INITRD=y +CONFIG_FEC=y +CONFIG_AT803X_PHY=y # CONFIG_RD_BZIP2 is not set # CONFIG_RD_LZMA is not set # CONFIG_RD_XZ is not set @@ -246,7 +248,6 @@ CONFIG_DM_VERITY=y CONFIG_DM_VERITY_FEC=y CONFIG_NETDEVICES=y CONFIG_TUN=y -# CONFIG_ETHERNET is not set   --- a/imx8q/mek_8q/mek_8q.mk +++ b/imx8q/mek_8q/mek_8q.mk @@ -46,6 +46,7 @@ PRODUCT_COPY_FILES += \      $(IMX_DEVICE_PATH)/fstab.freescale.car:$(TARGET_COPY_OUT_VENDOR)/etc/fstab.freescale \      $(IMX_DEVICE_PATH)/early.init_car.cfg:$(TARGET_COPY_OUT_VENDOR)/etc/early.init.cfg \      $(IMX_DEVICE_PATH)/required_hardware_auto.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/required_hardware.xml \ +    frameworks/native/data/etc/android.hardware.ethernet.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.ethernet.xml \      device/fsl/imx8q/init.recovery.freescale.car.rc:root/init.recovery.freescale.rc   Note: Please also check for below file, if fec1 is disabled, please also apply below diff. --- a/arch/arm64/boot/dts/freescale/imx8qm-mek-car2.dts +++ b/arch/arm64/boot/dts/freescale/imx8qm-mek-car2.dts @@ -147,10 +147,6 @@ status = "disabled"; }; -&fec1 { - status = "disabled"; -}; - &fec2 { status = "disabled"; };
記事全体を表示
Brief introduction on i.MX Android
記事全体を表示
The Android O8.1.0_2.0.0 GA (4.14.98 kernel) is now available on IMX software landing page. Overview -> i.MX BSP Updates and Releases -> Android -> Android O8.1.0_2.0.0   Files available:   # Name Description 1 android_o8.1.0_2.0.0-GA_docs.zip Android O8.1.0_2.0.0  Documentation 2 imx-o8.1.0_2.0.0-ga.tar.gz i.MX Android Automotive proprietary source code for Android O8.1.0_2.0.0 3 android_o8.1.0_2.0.0-ga_image_8qmek.tar.gz Prebuilt images with NXP extended features for the i.MX8QMax and 8QXPlus MEK   Supported boards: i.MX 8QuadMax MEK i.MX 8QuadXPlus MEK   Features and Known issues For features and known issues, please consult the Release Notes in detail.  ============================================================= The Android O8.1.0_2.1.0_AUTO GA (4.14.98 kernel) is now available on IMX software landing page. Overview -> i.MX BSP Updates and Releases -> Android AUTO-> Android O8.1.0_2.1.0_AUTO   Files available:   # Name Description 1 android_o8.1.0_2.1.0-auto-GA_docs.zip Android O8.1.0_2.1.0_AUTO Documentation 2 imx-o8.1.0_2.1.0-auto-ga.tar.gz i.MX Android Automotive proprietary source code for Android O8.1.0_2.1.0_AUTO 3 android_o8.1.0_2.1.0-auto-ga_image_8qmek.tar.gz Prebuilt images with NXP extended features with the EVS function enabled in the Cortex-M4 CPU core for the i.MX 8QuadMax/8QuadXPlus MEK 4 android_o8.1.0_2.1.0-auto-ga_image_8qmek2.tar.gz Prebuilt images with NXP extended features for the i.MX8QMax and 8QXPlus MEK, without the EVS in M4 Core. Supported boards: i.MX 8QuadMax MEK i.MX 8QuadXPlus MEK   Features and Known issues For features and known issues, please consult the Release Notes in detail. 
記事全体を表示
The Android P9.0.0_2.0.0 GA (4.14.98 kernel) is now available on IMX software landing page. Overview -> i.MX BSP Updates and Releases -> Android -> Android P9.0.0_2.0.0 (4.14.98 kernel)    Files available:   # Name Description 1 android_p9.0.0_2.0.0-ga_docs.zip Android P9.0.0_2.0.0 Documentation 2 imx-p9.0.0_2.0.0-ga.tar.gz i.MX Android proprietary surce code for Android P9.0.0_2.0.0 3 android_p9.0.0_2.0.0-ga_image_8mmevk.tar.gz Prebuilt images with NXP extended features for the i.MX 8M Mini EVK 4 android_p9.0.0_2.0.0-ga_image_8mqevk.tar.gz Prebuilt images with NXP extended features for the i.MX 8M Quad EVK 5 android_p9.0.0_2.0.0-ga_image_8qmek.tar.gz Prebuilt images with NXP extended features for the i.MX8QMax and 8QXPlus MEK 6 fsl_aacp_dec_p9.0.0_2.0.0-ga.tar.gz AAC Plus Codec for P9.0.0_2.0.0_GA   Supported boards: i.MX 8MMini MEK Board i.MX 8MQuad EVK Board i.MX 8QuadMax MEK i.MX 8QuadXPlus MEK   Features and Known issues For features and known issues, please consult the Release Notes in detail.  ======================================================================================= The Android P9.0.0_2.1.0_AUTO GA (4.14.98 kernel) is now available on IMX software landing page. Overview -> i.MX BSP Updates and Releases -> Android AUTO-> Android P9.0.0_2.1.0_AUTO   Files available:   # Name Description 1 android_p9.0.0_2.1.0-auto-ga_docs.zip Android P9.0.0_2.1.0_AUTO  Documentation 2 imx-p9.0.0_2.1.0-auto-ga.tar.gz i.MX Android Automotive proprietary source code for Android P9.0.0_2.1.0_AUTO 3 android_p9.0.0_2.1.0-auto-ga_image_8qmek.tar.gz Prebuilt images with NXP extended features with the EVS function enabled in the Cortex-M4 CPU core for the i.MX 8QuadMax/8QuadXPlus MEK 4 android_p9.0.0_2.1.0-auto-ga_image_8qmek2.tar.gz Prebuilt images with NXP extended features for the i.MX8QMax and 8QXPlus MEK, without the EVS in M4 Core.   Supported boards: i.MX 8QuadMax MEK i.MX 8QuadXPlus MEK   Features and Known issues For features and known issues, please consult the Release Notes in detail.
記事全体を表示
Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of Tsinghua University. Preparations 1. Installing Ubuntu16.04.2 LTS Customer can download ubuntu-16.04.2-desktop-amd64.iso from https://www.ubuntu.com/download/desktop Then install it to VMware workstation player v12 or PC, after finishing installation, use “Software Update” to update system. In order to compile android9.0.0-2.0.0 BSP, necessary packages should also be installed on Ubuntu 16.04. $ sudo apt-get install gnupg $ sudo apt-get install flex $ sudo apt-get install bison $ sudo apt-get install gperf $ sudo apt-get install build-essential $ sudo apt-get install zip $ sudo apt-get install zlib1g-dev $ sudo apt-get install libc6-dev $ sudo apt-get install lib32ncurses5-dev $ sudo apt-get install x11proto-core-dev $ sudo apt-get install libx11-dev $ sudo apt-get install lib32z1-dev $ sudo apt-get install libgl1-mesa-dev $ sudo apt-get install tofrodos $ sudo apt-get install python-markdown $ sudo apt-get install libxml2-utils $ sudo apt-get install xsltproc $ sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 $ sudo apt-get install gcc-multilib g++-multilib $ sudo apt-get install subversion $ sudo apt-get install openssh-server openssh-client $ sudo apt-get install uuid uuid-dev $ sudo apt-get install zlib1g-dev liblz-dev $ sudo apt-get install liblzo2-2 liblzo2-dev $ sudo apt-get install lzop $ sudo apt-get install git-core curl $ sudo apt-get install u-boot-tools $ sudo apt-get install mtd-utils $ sudo apt-get install android-tools-fsutils $ sudo apt-get install openjdk-8-jdk $ sudo apt-get install device-tree-compiler $ sudo apt-get install gdisk $ sudo apt-get install liblz4-tool $ sudo apt-get install m4 $ sudo apt-get install libz-dev More detail, see Android_User’s_Guide.pdf ( android 9.0.0-2.0.0 BSP documents) 2. Downloading and unpacking Android release package [ For android 9.0.0_2.2.0, see commemts, please!] https://www.nxp.com/support/developer-resources/evaluation-and-developmentboards/ sabre-development-system/android-os-for-i.mx-applicationsprocessors: IMXANDROID?tab=Design_Tools_Tab -- P9.0.0_2.0.0_GA_ANDROID_SOURCE File name is imx-p9.0.0_2.0.0-ga.tar.gz # cd ~ # tar xzvf imx-p9.0.0_2.0.0-ga.tar.gz Downloading Android 9.0.0-2.0.0 source code 1. Getting repo # cd ~ # mkdir bin # cd bin # curl https://mirrors.tuna.tsinghua.edu.cn/git/git-repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin 2. Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL = ' https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/ ' 3、Setting email address # git config --global user.email "[email protected]" # git config --global user.name "xxxx" [ Email & Name should be yours] 4、Modifying android setup script and Running it Open ~/imx-p9.0.0_2.0.0-ga/imx_android_setup.sh and add a line like below: ... ... if [ "$rc" != 0 ]; then echo "---------------------------------------------------" echo "-----Repo Init failure" echo "---------------------------------------------------" return 1 fi find -name 'aosp-p9.0.0_2.0.0-ga.xml'| \ xargs perl -pi -e 's|https://android.googlesource.com/|https://aosp.tuna.tsinghua.edu.cn/|g' fi ... ... Then save it and exit. # cd ~/ # source ~/imx-p9.0.0_2.0.0-ga/imx_android_setup.sh Then android_build directory is created at ~/ If fetching errors occur, like below, run “repo sync” again. # repo sync # export MY_ANDROID=~/android_build [Note] imx_android_setup.sh will be in charge of downloading all android source code. 5.Begin to compile android 9.0.0-2.0.0 BSP $ export ARCH=arm64 $ export CROSS_COMPILE=${MY_ANDROID}/prebuilts/gcc/linuxx86/aarch64/aarch64-linuxandroid-4.9/bin/aarch64-linux-android- $ cd ~/android_build/vendor $ cp -r ~/imx-p9.0.0_2.0.0-ga/vendor/* ./ $ cd ~/android_build $ source build/envsetup.sh $ lunch evk_8mm-userdebug $ make –j4 NXP TIC team Weidong sun 2019-05-05
記事全体を表示
The following document contains a list of document, questions and discussions that are relevant in the community based on amount of views. If you are having a problem, doubt or getting started in i.MX processors, you should check the following links to see if your doubt is in there. Yocto Project Freescale Yocto Project main page‌ Yocto Training - HOME‌ i.MX Yocto Project: Frequently Asked Questions‌ Useful bitbake commands‌ Yocto Project Package Management - smart  How to add a new layer and a new recipe in Yocto  Setting up the Eclipse IDE for Yocto Application Development Guide to the .sdcard format  Yocto NFS &amp; TFTP boot  YOCTO project clean  Yocto with a package manager (ex: apt-get)  Yocto Setting the Default Ethernet address and disable DHCP on boot.  i.MX x Building QT for i.MX6  i.MX6/7 DDR Stress Test Tool V3.00  i.MX6DQSDL DDR3 Script Aid  Installing Ubuntu Rootfs on NXP i.MX6 boards  iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP i.MX Design&amp;Tool Lists  Simple GPIO Example - quandry  i.MX6 GStreamer-imx Plugins - Tutorial &amp; Example Pipelines  Streaming USB Webcam over Network  Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53  Linux / Kernel Copying Files Between Windows and Linux using PuTTY  Building Linux Kernel  Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)  load kernel from SD card in U-boot  Changing the Kernel configuration for i.MX6 SABRE  Android  The Android Booting process  What is inside the init.rc and what is it used for.  Others How to use qtmultimedia(QML) with Gstreamer 1.0
記事全体を表示
This documents describes how to add the NFC support to i.MX8M mini evk running Android Pie. Hardware setup: The i.MX8M mini evk (see i.MX 8M Mini Evaluation Kit | NXP) featuring Raspberry Pi compliant connector, the OM5578/RPI PN7150 demo kit can be used to perform this porting (see NFC Development Kits for Arduino and more|NXP). However a small modification must be done because some of the signals required by PN7150 are not mapped to i.MX8M mini expansion connector pins. OM5578 IRQ signal must be mapped to Raspberry Pi connector pin #19 and OM5578 VEN signal must be mapped to Raspberry Pi connector pin #21. See below a picture of the modification: Then, the two boards can fit together as shown in the picture below: Quick start using demo image: The demo image including support for PN7150, is based on Android P9.0.0 Pie (P9.0.0_1.0.0, 4.14 kernel) i.MX software release (see i.MX Software | NXP). Related documentation can be downloaded from here: https://www.nxp.com/docs/en/supporting-information/android_p9.0.0_1.0.0-ga_docs.zip. Just flash the demo image (downloaded from here:https://www.nxp.com/lgfiles/updates/NFC/ANDROID_P9-0-0_PN7150_IMAGE_8MMEVK.zip) following guidelines from i.MX_Android_Quick_Start document (part of Android P9.0.0_1.0.0 Documentation package mentioned above). The NFC support is then included in the device settings, as shown in below screenshot of the device: Approaching the NFC tag, provided as reference in the OM5578 demo kit, to the NFC Antenna will trigger a sound notification: Unfortunately the Android demo image doesn't embed a web browser, so it won't be automatically open when the NFC tag content (an URL to the demo kit web page) is read. Otherwise (if a web browser is installed) you could see such page opening on the device: Adding PN7150 support to imx-android-pie release: If you wish to add PN7150 support to your imx-android-pie environment, just apply the patches (imx-p9.0.0_1.0.0-ga_pn7150_patches.tar.gz file attached) from the ${MY_ANDROID} source code root folder (refer to i.MX_Android_User_Guide document part of Android P9.0.0_1.0.0 Documentation package mentioned above).  $ patch -p1 -d device/fsl/ <device_fsl.patch  $ patch -p1 -d packages/apps/Nfc <packages_apps_Nfc.patch  $ patch -p1 -d hardware/nxp/nfc <hardware_nxp_nfc.patch  $ patch -p1 -d vendor/nxp <vendor_nxp.patch  $ patch -p1 -d vendor/nxp-opensource/kernel_imx/ <vendor_nxp-opensource_kernel_imx.patch When building, the PN7150 support will then be included to the android image, as shown in the demo image described above. Reference: This porting have been done (demo image and patches creation) following guidelines provided in AN11690_NXP-NCI_Android_Porting_Guidelines document.
記事全体を表示
   Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of Tsinghua University. Customers in other areas can refer to the configurations of ubuntu 18.04 in the document. Updating software packages for ubuntu18.04 LTS 1、Using software updater to update software packages Press Install Now button to update software. Restart ubuntu18.04 2、Installing necessary software packages #sudo apt-get install flex # sudo apt-get install bison # sudo apt-get install gperf # sudo apt-get install build-essential # sudo apt-get install zlib1g-dev # sudo apt-get install lib32ncurses5-dev # sudo apt-get install x11proto-core-dev # sudo apt-get install libx11-dev # sudo apt-get install lib32z1-dev # sudo apt-get install libgl1-mesa-dev # sudo apt-get install tofrodos # sudo apt-get install python-markdown # sudo apt-get install libxml2-utils # sudo apt-get install xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 # sudo apt-get install gcc-multilib g++-multilib # sudo apt-get install subversion # sudo apt-get install openssh-server openssh-client # sudo apt-get install uuid uuid-dev # sudo apt-get install zlib1g-dev liblz-dev # sudo apt-get install liblzo2-2 liblzo2-dev # sudo apt-get install lzop # sudo apt-get install git-core curl # sudo apt-get install u-boot-tools # sudo apt-get install mtd-utils # sudo apt-get install android-tools-fsutils # sudo apt-get install openjdk-8-jdk # sudo apt-get install device-tree-compiler # sudo apt-get install aptitude # sudo aptitude install libcurl4-openssl-dev nss-updatedb 3、Downloading and unpacking Android release package https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applications-processors/android-os-for-i.mx-applications-processors:IMXANDROID?tab=Design_Tools_Tab --O8.1.0_1.3.0_ANDROID_SOURCE_8MQ_GA File name is imx-o8.1.0_1.3.0_8m.tar.gz # cd ~ # tar xzvf imx-o8.1.0_1.3.0_8m.tar.gz Downloading android8.1.0-1.3.0 source code Getting repo # cd ~ # mkdir bin # cd bin # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin   Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL = 'https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/' 3、Setting email address # git config --global user.email "[email protected]" # git config --global user.name "xxxx" [ Email & Name should be yours] 4、Modifying android setup script and Running it Open ~/ imx-o8.1.0_1.3.0_8m /imx_android_setup.sh and add a line like below: ...       if [ "$rc" != 0 ]; then          echo "---------------------------------------------------"          echo "-----Repo Init failure"          echo "---------------------------------------------------"          return 1       fi find -name 'aosp-O8.1.0-1.3.0.xml'| xargs perl -pi -e 's|https://android.googlesource.com/|https://aosp.tuna.tsinghua.edu.cn/|g' fi   # Don't Delete .repo directory and hidden files #rm -rf $android_builddir/.??* ... Then save it and exit. # cd ~/ # source ~/ imx-o8.1.0_1.3.0_8m/imx_android_setup.sh Then android_build directory is created at ~/ # export MY_ANDROID=~/android_build          48 hours later: Compiling android8.1.0-1.3.0 BSP # cd ~/android_build # gedit ./prebuilts/sdk/tools/jack-admin               And find “JACK_SERVER_COMMAND” ,change it to be: JACK_SERVER_COMMAND="java -XX:MaxJavaStackTraceDepth=-1 -Djava.io.tmpdir=$TMPDIR $JACK_SERVER_VM_ARGUMENTS -Xmx4096m -cp $LAUNCHER_JAR $LAUNCHER_NAME"          Save and exit. And run: # ./prebuilts/sdk/tools/jack-admin stop-server # ./prebuilts/sdk/tools/jack-admin start-server # export ARCH=arm64 # export CROSS_COMPILE=~/android_build/prebuilts/gcc/linux-x86/aarch64/aarch64-linuxandroid-4.9/bin/aarch64-linux-android- # export LC_ALL=C # source build/envsetup.sh # lunch evk_8mq-userdebug               Begin to build android BSP for i.MX8MQ # make –j4 NXP TIC weidong sun 2018-08-15
記事全体を表示
The Android O8.0.0_1.4.0 for i.MX 7ULP RFP(GA) release is now available on IMX_SW web page. Overview -> BSP Updates and Releases -> Android O8.1.0 for i.MX 7ULP GA.   Files available:   # Name Description 1 android_o8.1.0_1.4.0_7ulp-ga_docs.tar.gz Android O8.1.0_1.4.0 for 7ULP GA Documentation 2 imx-o8.1.0_1.4.0_7ulp-ga.tar.gz i.MX Android proprietary source code for Android O8.1.0_1.4.0_7ULP_GA 3 android_o8.1.0_1.4.0_7ulp-ga_image_7ulpevk.tar.gz Prebuilt images with NXP extended features for the i.MX7ULP EVK board 4 android_o8.1.0_1.4.0_7ulp-ga_tools.tar.gz Manufacturing Toolkit and VivanteVTK for Android O8.1.0_1.4.0_7ULP_GA 5 fsl_aacp_dec_O8.1.0-7ULP_GA.tar.gz AAC Plus Codec for  O8.1.0_1.4.0_7ULP_GA   Target boards: i.MX 7ULP EVK   Features and Known issues For features and known issues, please consult the Release Notes in detail.#
記事全体を表示
   Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of University of Science and Technology of China. Preparations Installing Ubuntu16.04.2 LTS Customer can download ubuntu-16.04.2-desktop-amd64.iso from https://www.ubuntu.com/download/desktop        Then install it to VMware workstation player v12 or PC, after finishing installation, use “Software Update” to update system. In order to compile android8.0.0-1.0.0 BSP, necessary packages should also be installed on Ubuntu 16.04. $ sudo apt-get install gnupg $ sudo apt-get install flex $ sudo apt-get install bison $ sudo apt-get install gperf $ sudo apt-get install build-essential $ sudo apt-get install zip $ sudo apt-get install zlib1g-dev $ sudo apt-get install libc6-dev $ sudo apt-get install lib32ncurses5-dev   $ sudo apt-get install x11proto-core-dev $ sudo apt-get install libx11-dev $ sudo apt-get install lib32z1-dev   $ sudo apt-get install libgl1-mesa-dev $ sudo apt-get install tofrodos $ sudo apt-get install python-markdown $ sudo apt-get install libxml2-utils $ sudo apt-get install xsltproc $ sudo apt-get install uuid-dev:i386 liblzo2-dev:i386   $ sudo apt-get install gcc-multilib g++-multilib $ sudo apt-get install subversion $ sudo apt-get install openssh-server openssh-client $ sudo apt-get install uuid uuid-dev $ sudo apt-get install zlib1g-dev liblz-dev $ sudo apt-get install liblzo2-2 liblzo2-dev $ sudo apt-get install lzop $ sudo apt-get install git-core curl $ sudo apt-get install u-boot-tools $ sudo apt-get install mtd-utils $ sudo apt-get install android-tools-fsutils $ sudo apt-get install openjdk-8-jdk More detail, see Android_User’s_Guide.pdf ( android 8.0.0-1.0.0 BSP documents) Downloading and unpacking Android release package https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applications-processors/android-os-for-i.mx-applications-processors:IMXANDROID?tab=Design_Tools_Tab --IMX_O8.0.0_1.0.0_ANDROID_SOURCE File name is mx-o8.0.0_1.0.0_ga.tar.gz # cd ~ # tar xzvf mx-o8.0.0_1.0.0_ga.tar Downloading Android 8.0.0-1.0.0 source code Getting repo # cd ~ # mkdir bin # cd bin # curl https://storage-googleapis.proxy.ustclug.org/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From            REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL ='git-repo - Git at Google ' 3、Setting email address # git config --global user.email "[email protected]" # git config --global user.name "xxxx"  [ Email & Name should be yours]   4、Modifying android setup script and Running it          Open ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh and add a line like below: ......       if [ "$rc" != 0 ]; then          echo "---------------------------------------------------"          echo "-----Repo Init failure"          echo "---------------------------------------------------"          return 1       fi find -name 'aosp-O8.0.0-1.0.0.xml'| xargs perl -pi -e 's|https://android.googlesource.com/|git://mirrors.ustc.edu.cn/aosp/|g' fi   # Don't Delete .repo directory and hidden files #rm -rf $android_builddir/.??*    Then save it and exit. # cd ~/ # source ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh Then android_build directory is created at ~/ # export MY_ANDROID=~/android_build [Note] imx_android_setup.sh will be in charge of downloading all android source code. 5.Begin to compile android 8.0.0 BSP $ export ARCH=arm $ export CROSS_COMPILE=${MY_ANDROID}/prebuilts/gcc/linux-x86/arm/arm-linuxandroideabi-4.9/bin/arm-linux-androideabi- $ cd ~/android_build $ source build/envsetup.sh $ lunch sabreauto_6q-userdebug $ make –j4 Errors: ...... “Try increasing heap size with java option '-Xmx<size>'.” ...... Logs for compiling     weidong@ubuntu:~/android_build$ lunch sabreauto_6q-userdebug   ============================================ PLATFORM_VERSION_CODENAME=REL PLATFORM_VERSION=8.0.0 TARGET_PRODUCT=sabreauto_6q TARGET_BUILD_VARIANT=userdebug TARGET_BUILD_TYPE=release TARGET_PLATFORM_VERSION=OPD1 TARGET_BUILD_APPS= TARGET_ARCH=arm TARGET_ARCH_VARIANT=armv7-a-neon TARGET_CPU_VARIANT=cortex-a9 TARGET_2ND_ARCH= TARGET_2ND_ARCH_VARIANT= TARGET_2ND_CPU_VARIANT= HOST_ARCH=x86_64 HOST_2ND_ARCH=x86 HOST_OS=linux HOST_OS_EXTRA=Linux-4.4.0-116-generic-x86_64-with-Ubuntu-16.04-xenial HOST_CROSS_OS=windows HOST_CROSS_ARCH=x86 HOST_CROSS_2ND_ARCH=x86_64 HOST_BUILD_TYPE=release BUILD_ID=1.0.0-rfp-rc4 OUT_DIR=out AUX_OS_VARIANT_LIST= ============================================ weidong@ubuntu:~/android_build$ make -j4 ============================================     ============================================ PLATFORM_VERSION_CODENAME=REL PLATFORM_VERSION=8.0.0 TARGET_PRODUCT=sabreauto_6q TARGET_BUILD_VARIANT=userdebug TARGET_BUILD_TYPE=release TARGET_ARCH=arm TARGET_ARCH_VARIANT=armv7-a-neon TARGET_CPU_VARIANT=cortex-a9 HOST_ARCH=x86_64 HOST_2ND_ARCH=x86 HOST_OS=linux HOST_OS_EXTRA=Linux-4.4.0-116-generic-x86_64-with-Ubuntu-16.04-xenial HOST_CROSS_OS=windows HOST_CROSS_ARCH=x86 HOST_CROSS_2ND_ARCH=x86_64 HOST_BUILD_TYPE=release BUILD_ID=1.0.0-rfp-rc4 OUT_DIR=out ============================================ [38/38] bootstrap out/soong/.minibootstrap/build.ninja.in [1/2] out/soong/.bootstrap/bin/minibp out/soong/.minibootstrap/build.ninja.in [4/4] out/soong/.bootstrap/bin/minibp out/soong/.bootstrap/build.ninja [791/792] glob vendor/*/*/Android.bp [47/47] out/soong/.bootstrap/bin/soong_build out/soong/build.ninja out/build-sabreauto_6q.ninja is missing, regenerating... [9/1005] including ./cts/Android.mk ... cts/hostsidetests/os/test-apps/StaticSharedNativeLibProvider/Android.mk:23: warning: FindEmulator: find: `cts/hostsidetests/os/test-apps/StaticSharedNativeLibProvider/src': No such file or directory cts/hostsidetests/os/test-apps/StaticSharedNativeLibProvider1/Android.mk:23: warning: FindEmulator: find: `cts/hostsidetests/os/test-apps/StaticSharedNativeLibProvider1/src': No such file or directory [690/1005] including ./system/sepolicy/Android.mk ... ./system/sepolicy/Android.mk:107: warning: BOARD_SEPOLICY_VERS not specified, assuming current platform version [1005/1005] including ./vendor/nxp/linux-firmware-imx/firmware/Android.mk ... No private recovery resources for TARGET_DEVICE sabreauto_6q platform_testing/build/tasks/tests/instrumentation_metric_test_list.mk: warning: continuous_instrumentation_metric_tests: Unknown installed file for module perf-setup.sh platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module RecyclerViewTests platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module SettingsFunctionalTests platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module LauncherFunctionalTests platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module EmergencyInfoTests platform_testing/build/tasks/tests/native_metric_test_list.mk: warning: continuous_native_metric_tests: Unknown installed file for module perf-setup.sh test/vts/tools/build/tasks/vts_package.mk:222: warning: FindEmulator: cd: vendor/google_vts/testcases: No such file or directory test/vts/tools/build/tasks/vts_package.mk:222: warning: FindEmulator: cd: vendor/google_vts/testcases: No such file or directory test/vts/tools/build/tasks/vts_package.mk:222: warning: FindEmulator: cd: vendor/google_vts/testcases: No such file or directory ./test/vts/utils/python/archive/Android.mk:28: warning: overriding commands for target `default' ./test/vts/runners/host/tcp_server/Android.mk:19: warning: ignoring old commands for target `default' build/core/Makefile:34: warning: overriding commands for target `out/target/product/sabreauto_6q/root/init.rc' build/core/base_rules.mk:378: warning: ignoring old commands for target `out/target/product/sabreauto_6q/root/init.rc' ...... ......  CC      lib/vsprintf.o   CC      lib/panic.o   CC      lib/strto.o   CC      lib/strmhz.o   LD      lib/built-in.o   CC      examples/standalone/hello_world.o   CC      examples/standalone/stubs.o   LD      examples/standalone/libstubs.o   LD      examples/standalone/hello_world   OBJCOPY examples/standalone/hello_world.bin   OBJCOPY examples/standalone/hello_world.srec   LD      u-boot   OBJCOPY u-boot-nodtb.bin   OBJCOPY u-boot.srec   SHIPPED dts/dt.dtb   SYM     u-boot.sym   COPY    u-boot.dtb   CAT     u-boot-dtb.bin   COPY    u-boot.bin   CFGS    board/freescale/mx6qsabreauto/mx6qp.cfg.cfgtmp   MKIMAGE u-boot-dtb.imx   CFGCHK  u-boot.cfg make[1]: Leaving directory '/home/weidong/android_build/out/target/product/sabreauto_6q/obj/BOOTLOADER_OBJ' make: Leaving directory '/home/weidong/android_build/vendor/nxp-opensource/uboot-imx' /bin/bash: line 0: [: =: unary operator expected [  3% 2129/63758] Check module type: out/target/common/obj/APPS/Browser2_intermediates/link_type packages/apps/Browser2/Android.mk: warning: Browser2 (java:sdk) should not link to legacy-android-test (java:platform) [  3% 2171/63758] Ensuring Jack server is installed and started Jack server already installed in "/home/weidong/.jack-server" Launching Jack server java -XX:MaxJavaStackTraceDepth=-1 -Djava.io.tmpdir=/tmp -Dfile.encoding=UTF-8 -XX:+TieredCompilation -cp /home/weidong/.jack-server/launcher.jar com.android.jack.launcher.ServerLauncher Server updated, waiting for restart ...... ...... D [M]  drivers/rpmsg/imx_rpmsg_tty.ko   LD [M]  drivers/video/backlight/l4f00242t03.ko   CC      arch/arm/boot/compressed/misc.o   LD [M]  drivers/video/backlight/platform_lcd.ko   LD [M]  drivers/video/backlight/lcd.ko   CC      arch/arm/boot/compressed/decompress.o   CC      arch/arm/boot/compressed/string.o   SHIPPED arch/arm/boot/compressed/hyp-stub.S   SHIPPED arch/arm/boot/compressed/lib1funcs.S   SHIPPED arch/arm/boot/compressed/ashldi3.S   SHIPPED arch/arm/boot/compressed/bswapsdi2.S   AS      arch/arm/boot/compressed/hyp-stub.o   AS      arch/arm/boot/compressed/lib1funcs.o   AS      arch/arm/boot/compressed/ashldi3.o   AS      arch/arm/boot/compressed/bswapsdi2.o   AS      arch/arm/boot/compressed/piggy.o   LD      arch/arm/boot/compressed/vmlinux   OBJCOPY arch/arm/boot/zImage   Kernel: arch/arm/boot/zImage is ready make[1]: Leaving directory '/home/weidong/android_build/out/target/product/sabreauto_6q/obj/KERNEL_OBJ' make: Leaving directory '/home/weidong/android_build/vendor/nxp-opensource/kernel_imx' make: Entering directory '/home/weidong/android_build/vendor/nxp-opensource/kernel_imx' make[1]: Entering directory '/home/weidong/android_build/out/target/product/sabreauto_6q/obj/KERNEL_OBJ'   CHK     include/config/kernel.release   GEN     ./Makefile   CHK     include/generated/uapi/linux/version.h   Using /home/weidong/android_build/vendor/nxp-opensource/kernel_imx as source for kernel   CHK     include/generated/utsrelease.h   CHK     include/generated/timeconst.h   CHK     include/generated/bounds.h   CHK     include/generated/asm-offsets.h   CALL    /home/weidong/android_build/vendor/nxp-opensource/kernel_imx/scripts/checksyscalls.sh make[1]: Leaving directory '/home/weidong/android_build/out/target/product/sabreauto_6q/obj/KERNEL_OBJ' make: Leaving directory '/home/weidong/android_build/vendor/nxp-opensource/kernel_imx'   ...... ...... [ 83% 53244/63758] Building with Jack: out/target/co...ARIES/framework_intermediates/with-local/classes.dex FAILED: out/target/common/obj/JAVA_LIBRARIES/framework_intermediates/with-local/classes.dex /bin/bash out/target/common/obj/JAVA_LIBRARIES/framework_intermediates/with-local/classes.dex.rsp Out of memory error (version 1.3-rc7 'Douarn' (445000 d7be3910514558d6715ce455ce0861ae2f56925a by [email protected])). GC overhead limit exceeded. Try increasing heap size with java option '-Xmx<size>'. Warning: This may have produced partial or corrupted output. [ 83% 53247/63758] //external/llvm/lib/CodeGen/SelectionDAG:libLLVMSelectionDAG clang++ DAGCombiner.cpp ninja: build stopped: subcommand failed. 19:17:25 ninja failed with: exit status 1 build/core/main.mk:21: recipe for target 'run_soong_ui' failed make: *** [run_soong_ui] Error 1   ******************************************************* solve the issue: Try increasing heap size with java option '-Xmx<size>'. -- run commands below on command line #export JACK_SERVER_VM_ARGUMENTS="-Dfile.encoding=UTF-8 -XX:+TieredCompilation -Xmx4g" #./prebuilts/sdk/tools/jack-admin kill-server #./prebuilts/sdk/tools/jack-admin start-server ******************************************************* #make -j4   //continue compiling   ...... ...... [ 50% 1/2] glob vendor/*/*/Android.bp [  0% 1/10515] Ensuring Jack server is installed and started Jack server already installed in "/home/weidong/.jack-server" Server is already running ...... ...... Creating filesystem with parameters:     Size: 1585446912     Block size: 4096     Blocks per group: 32768     Inodes per group: 8064     Inode size: 256     Journal blocks: 6048     Label: system     Blocks: 387072     Block groups: 12     Reserved block group size: 95 Created filesystem with 2216/96768 inodes and 171147/387072 blocks Running:  build_verity_tree -A aee087a5be3b982978c923f566a94613496b417f2af592639bc80d141e34dfe7 out/target/product/sabreauto_6q/obj/PACKAGING/systemimage_intermediates/system.img /tmp/tmpPnRk1H_verity_images/verity.img f26a84a2c66d866f5322986e7a093812329d87579e5859aa32a2cf4c21f69661 aee087a5be3b982978c923f566a94613496b417f2af592639bc80d141e34dfe7 Running:  system/extras/verity/build_verity_metadata.py build 1585446912 /tmp/tmpPnRk1H_verity_images/verity_metadata.img f26a84a2c66d866f5322986e7a093812329d87579e5859aa32a2cf4c21f69661 aee087a5be3b982978c923f566a94613496b417f2af592639bc80d141e34dfe7 /dev/block/by-name/system verity_signer build/target/product/security/verity.pk8 ['verity_signer', '/tmp/tmpvXftO2.table', 'build/target/product/security/verity.pk8', '/tmp/tmpbfl4fq.sig'] appending /tmp/tmpPnRk1H_verity_images/verity_metadata.img to /tmp/tmpPnRk1H_verity_images/verity.img Running:  fec -e -p 0 out/target/product/sabreauto_6q/obj/PACKAGING/systemimage_intermediates/system.img /tmp/tmpPnRk1H_verity_images/verity.img /tmp/tmpPnRk1H_verity_images/verity_fec.img encoding RS(255, 253) to '/tmp/tmpPnRk1H_verity_images/verity_fec.img' for input files:        1: 'out/target/product/sabreauto_6q/obj/PACKAGING/systemimage_intermediates/system.img'        2: '/tmp/tmpPnRk1H_verity_images/verity.img' appending /tmp/tmpPnRk1H_verity_images/verity_fec.img to /tmp/tmpPnRk1H_verity_images/verity.img Running:  append2simg out/target/product/sabreauto_6q/obj/PACKAGING/systemimage_intermediates/system.img /tmp/tmpPnRk1H_verity_images/verity.img   [100% 10515/10515] Install system fs image: out/target/product/sabreauto_6q/system.img out/target/product/sabreauto_6q/system.img+out/target/product/sabreauto_6q/obj/PACKAGING/recovery_patch_intermediates/recovery_from_boot.p maxsize=1644331392 blocksize=4224 total=704129669 reserve=16612992   #### make completed successfully (01:21:12 (hh:mm:ss)) ####   NXP TIC team Weidong sun 2018-06-01
記事全体を表示