iMX6 Quad Android 13.4 handup issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Quad Android 13.4 handup issue

iMX6 Quad Android 13.4 handup issue

Dear IMX community,

We usingiMX6 Quad processor and run Android 13.4, After below log file and android handup, We also run DDR stress test without problems found,

Can anyone give a suggestions on this issue

Best Regards, Jim

================================

U-Boot 2009.08-00008-g5f5b708-dirty (Mar 18 2013 - 17:23:58)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Temperature:   52 C, calibration data 0x5b051d69
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock     : 66000000Hz
ipg per clock : 66000000Hz
uart clock    : 80000000Hz
cspi clock    : 60000000Hz
ahb clock     : 132000000Hz
axi clock   : 264000000Hz
emi_slow clock: 29333333Hz
ddr clock     : 528000000Hz
usdhc1 clock  : 198000000Hz
usdhc2 clock  : 198000000Hz
usdhc3 clock  : 198000000Hz
usdhc4 clock  : 198000000Hz
nfc clock     : 24000000Hz
Board: MX6Q-SABRELITE:[ POR]
Boot Device: I2C
I2C:   ready
DRAM:   1 GB
MMC:   FSL_USDHC: 0,FSL_USDHC: 1
JEDEC ID: 0x20:0x20:0x16
*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
Net:   got MAC address from IIM: 00:00:00:00:00:00
FEC0 [PRIME]
Hit any key to stop autoboot:  0
mmc0(part 0) is current device
reading /6q_bootscript

353 bytes read
## Executing script at 10008000
reading uimage

4016476 bytes read
reading uramdisk.img

212592 bytes read
## Booting kernel from Legacy Image at 10800000 ...
   Image Name:   Linux-3.0.35
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    4016412 Bytes =  3.8 MB
   Load Address: 10008000
   Entry Point:  10008000
   Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 12800000 ...
   Image Name:   Android Root Filesystem
   Image Type:   ARM Linux RAMDisk Image (uncompressed)
   Data Size:    212528 Bytes = 207.5 kB
   Load Address: 12800000
   Entry Point:  12800000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Initializing cgroup subsys cpuset
Initializing cgroup subsys cpu
Linux version 3.0.35 (leo@pluto) (gcc version 4.6.2 20120613 (release) [ARM/embedded-4_6-bra                                 nch revision 188521] (GNU Tools for ARM Embedded Processors) ) #10 SMP PREEMPT Tue Mar 19 11                                 :34:02 CST 2013
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad Sabre-Lite Board
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @c1119000 s5760 r8192 d14720 u32768
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 210944
Kernel command line: arm_freq=1000 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1                                 :off console=ttymxc0,115200 init=/init rw no_console_suspend androidboot.console=ttymxc0 vma                                 lloc=400M
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 576MB 256MB = 832MB total
Memory: 833728k/833728k available, 214848k reserved, 442368K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)
    vmalloc : 0xd9800000 - 0xf2000000   ( 392 MB)
    lowmem  : 0xc0000000 - 0xd9000000   ( 400 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .init : 0xc0008000 - 0xc0041000   ( 228 kB)
      .text : 0xc0041000 - 0xc0770fb0   (7360 kB)
      .data : 0xc0772000 - 0xc07e0da0   ( 444 kB)
       .bss : 0xc07e0dc4 - 0xc090f7d0   (1211 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:496
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Initializing cgroup subsys cpuacct
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
CPU2: Booted secondary processor
CPU3: Booted secondary processor
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2800 <--> 3150 mV at 3000 mV fast normal
------------ Board type Sabre Lite
Flexcan NXP tja1040
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B
IMX usb wakeup probe
bio: create slab <bio-0> at 0
print_constraints: VDDA: 2500 mV
print_constraints: VDDIO: 3300 mV
machine_constraints_voltage: VDDD: unsupportable voltage constraints
reg-fixed-voltage reg-fixed-voltage.2: Failed to register regulator: -22
reg-fixed-voltage: probe of reg-fixed-voltage.2 failed with error -22
print_constraints: vmmc: 3300 mV
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
add wake up source irq 75
i2c i2c-0: Invalid 7-bit I2C address 0x00
i2c i2c-0: Can't create device at 0x00
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Unpacking initramfs...
Freeing initrd memory: 204K
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = d9880000 suspend_iram_base=d98fc000
PM driver module loaded
IMX usb wakeup probe
i.MXC CPU frequency driver
highmem bounce pool size: 64 pages
ashmem: initialized
JFFS2 version 2.2. (NAND) ? 2001-2006 Red Hat, Inc.
msgmni has been set to 764
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver hdmi
mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
mxc_sdc_fb mxc_sdc_fb.1: Can't get fb option for mxcfb1!
mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver ldb
_regulator_get: get() with no identifier
mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 0(VIC 16):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 1(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 2(VIC 1):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 3(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 4(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 5(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 6(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 7(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 8(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 9(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 10(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 11(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 12(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 13(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 14(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 15(VIC 0):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 16(VIC 16):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 18(VIC 1):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 19(VIC 2):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 20(VIC 3):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 21(VIC 4):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 22(VIC 31):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 23(VIC 19):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 24(VIC 17):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 25(VIC 18):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 29(VIC 16):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 30(VIC 3):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 31(VIC 4):
mxc_hdmi mxc_hdmi: mxc_hdmi_edid_rebuild_modelist: Added mode 32(VIC 18):
fbcvt: 1920x1080@60: CVT Name - 2.073M9
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
loop: module loaded
m25p80 spi0.0: m25p32 (4096 Kbytes)
Creating 3 MTD partitions on "m25p80":
0x000000000000-0x0000000c0000 : "bootloader"
0x0000000c0000-0x0000000c2000 : "ubparams"
mtd: partition "ubparams" doesn't end on an erase block -- force read-only
0x0000000c2000-0x000000400000 : "unused"
mtd: partition "unused" doesn't start on an erase block boundary -- force read-only
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
flexcan imx6q-flexcan.0: device registered (reg_base=d9970000, irq=142)
FEC Ethernet Driver
fec_enet_mii_bus: probed
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
PPP BSD Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
PPTP driver version 0.8.5
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver option
option: v0.7.2:USB Driver for GSM modems
USB Serial support registered for Qualcomm USB modem
usbcore: registered new interface driver qcserial
ARC USBOTG Device Controller driver (1 August 2005)
android_usb gadget: Mass Storage Function, version: 2009/09/11
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
Gadget Android: controller 'fsl-usb2-udc' not recognized
android_usb gadget: android_usb ready
Suspend udc for OTG auto detect
fsl-usb2-udc: bind to driver android_usb
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
egalax_ts 2-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
input: ak4183ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
using rtc device, snvs_rtc, for alarms
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
ov5640_read_reg:write reg error:reg=300a
ov5640_probe:cannot find camera
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.1.0)
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
usb 2-1: new high speed USB device number 2 using fsl-ehci
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCIATH3K protocol initialized
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
sdhci sdhci-esdhc-imx.3: no write-protect pin available!
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
revserved_memory_account:viv_gpu registerd
Thermal calibration data is 0x5b051d69
anatop_thermal_counting_ratio: raw25c=1456 raw_hot=1309 hot_temp=105
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
hub 2-1:1.0: USB hub found
logger: created 256K log 'log_radio'
logger: created 256K log 'log_system'
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
Cirrus Logic CS42888 ALSA SoC Codec Driver
i2c-core: driver [cs42888] using legacy suspend method
i2c-core: driver [cs42888] using legacy resume method
hub 2-1:1.0: 4 ports detected
mmc0: new high speed MMC card at address 0001
mmcblk0: mmc0:0001 eMMC   3.71 GiB
mmcblk0boot0: mmc0:0001 eMMC   partition 1 2.00 MiB
mmcblk0boot1: mmc0:0001 eMMC   partition 2 2.00 MiB
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
mmcblk0boot1: unknown partition table
mmcblk0boot0: unknown partition table
asoc: sgtl5000 <-> imx-ssi.1 mapping ok
imx_3stack asoc driver
asoc: mxc-hdmi-soc <-> imx-hdmi-soc-dai.0 mapping ok
ALSA device list:
  #0: sgtl5000-audio
  #1: imx-hdmi-soc
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (13030 buckets, 52120 max)
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
xt_time: kernel timezone is -0000
IPv4 over IPv4 tunneling driver
GRE over IPv4 demultiplexor driver
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP cubic registered
NET: Registered protocol family 10
ip6_tables: (C) 2000-2006 Netfilter Core Team
IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
L2TP core driver, V2.0
PPPoL2TP kernel driver, V2.0
L2TP IP encapsulation support (L2TPv3)
L2TP netlink interface
L2TP ethernet pseudowire support (L2TPv3)
lib80211: common routines for IEEE802.11 drivers
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: VDDIO: incomplete constraints, leaving on
regulator_init_complete: VDDA: incomplete constraints, leaving on
regulator_init_complete: vddpu: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-02 00:04:27 UTC (86667)
Freeing init memory: 228K
usb 2-1.4: new low speed USB device number 3 using fsl-ehci
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
input: HID 04d9:0499 as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.4/2-1.4:1.0/input/input2
generic-usb 0003:04D9:0499.0001: input,hidraw0: USB HID v1.10 Mouse [HID 04d9:0499] on usb-f                                 sl-ehci.1-1.4/input0
EXT4-fs (mmcblk0p5): recovery complete
EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk0p7): recovery complete
EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: noauto_da_alloc,errors                                 =panic
EXT4-fs (mmcblk0p6): warning: mounting unchecked fs, running e2fsck is recommended
EXT4-fs (mmcblk0p6): mounted filesystem without journal. Opts: (null)
init: cannot find '/system/bin/gpu_init.sh', disabling 'gpu_init'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
android_usb: already disabled
adb_open
mtp_bind_config
adb_bind_config
warning: `rild' uses 32-bit capabilities (legacy support in use)
root@android:/ # ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
request_suspend_state: wakeup (3->0) at 20324699670 (1970-01-02 00:04:45.205101336 UTC)
eth0: Freescale FEC PHY driver [Micrel KSZ9021 Gigabit PHY] (mii_bus:phy_addr=1:07, irq=284)
ADDRCONF(NETDEV_UP): eth0: link is not ready
acc_open
acc_release
PHY: 1:07 - Link is Up - 100/Full
ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
CPU3: shutdown
CPU2: shutdown
Unable to handle kernel paging request at virtual address f40c4010
pgd = d3e04000
[f40c4010] *pgd=02011452(bad)
Internal error: Oops: 2d [#1] PREEMPT SMP
Modules linked in:
CPU: 0    Not tainted  (3.0.35 #10)
PC is at _clk_arm_get_rate+0xc/0x28
LR is at clk_get_rate+0x40/0x50
pc : [<c005ac7c>]    lr : [<c006650c>]    psr: a0000193
sp : d3e51db0  ip : c004c6b0  fp : d3ceae00
r10: 00100100  r9 : c111a588  r8 : 00200200
r7 : 010da000  r6 : 00000001  r5 : d6f15e8c  r4 : c07e1040
r3 : f40c4000  r2 : d3e51dd8  r1 : 00000000  r0 : c0790430
Flags: NzCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment user
Control: 10c53c7d  Table: 23e0404a  DAC: 00000015

PC: 0xc005abfc:
abfc  1affffdc eaffffee c078f07c c07e1654 c078f0d0 e92d4010 e59f304c e5900028
ac1c  e1500003 0a000007 e59f3040 e1500003 13a04001 0a000003 eb002e24 e1a01004
ac3c  eb076b36 e8bd8010 e3a03901 e34f340c e5934014 eb002e1d e7e24dd4 e2844001
ac5c  e1a01004 eb076b2d e8bd8010 c078f124 c078e260 e3a03901 e34f240c e92d4010
ac7c  e5934010 e5900028 eb002e10 e2041007 e2811001 eb076b21 e8bd8010 e92d4038
ac9c  e1a05001 e5900028 eb002e08 e1a01005 e1a04000 eb076b19 e2501000 03a01001
acbc  0a000001 e3510040 23a01040 e1a00004 eb076b12 e8bd8038 e92d40f8 e1a05001
acdc  e5900028 eb002df9 e1a01005 e1a07000 eb076b0a e2504000 01a06004 03a04001

LR: 0xc006648c:
648c  c07e1684 c0574908 c06a6f80 e59f3010 e3500000 e593000c 1a000000 ea000167
64ac  ea000189 c07e15fc e3500000 012fff1e e3700a01 91d003d0 83a00000 e12fff1e
64cc  e3500000 e92d4008 08bd8008 e3700a01 83a00000 9a000005 e8bd8008 e5900028
64ec  e3500000 0a000006 e3700a01 8a000005 e590303c e3530000 0afffff7 e12fff33
650c  e8bd8008 e8bd8008 e3a00000 e8bd8008 e92d4008 e2503000 01a00003 08bd8008
652c  e3730a01 83a00000 88bd8008 e5933044 e3530000 0a000001 e12fff33 e8bd8008
654c  e1a00003 e8bd8008 e3500000 012fff1e e3700a01 95900028 83a00000 e12fff1e
656c  e3500000 e92d4010 e1a04001 1a000003 ea00000d e5900028 e3500000 0a00000a

SP: 0xd3e51d30:
1d30  c111a040 c1119040 00000006 00000003 00000006 c1119040 00000000 393f7476
1d50  00000006 0000040f 0000000d 00000001 010da000 c00469d0 c0790430 00000000
1d70  d3e51dd8 f40c4000 c07e1040 d6f15e8c 00000001 010da000 00200200 c111a588
1d90  00100100 d3ceae00 c004c6b0 d3e51db0 c006650c c005ac7c a0000193 ffffffff
1db0  c07e1040 c006650c c0059e84 c0059e90 c0059e84 c006650c c004c6d8 c004c6ec
1dd0  d3e51dd8 c00a799c d3e51dd8 d3e51dd8 c0783cd0 d3e50000 c003fc18 00000000
1df0  00000000 d3e51e20 d6085a00 c00412c0 ffffffff f2a00100 00000405 00000001
1e10  00000000 d3e50000 d6085a00 c0046a4c 00000000 010da000 00000000 d3e50000

IP: 0xc004c630:
c630  e59f3018 e1a0000c e5933004 e12fff33 e28dd014 e8bd8000 c078b1c8 c004c16c
c650  c0783a2c e3510003 e1a0c00d e3cc2d7f 93a03000 83a03001 e3510001 03833001
c670  e3c2203f e3530000 e5922014 1a000009 e3520003 ca000007 e2822008 e7d0c002
c690  e20cc0fc e18c1001 e6ef1071 e7c01002 e1a00003 e12fff1e e3e03015 eafffffb
c6b0  e3013040 e34c307e e1a01000 e3a00000 e5933000 e5932008 e5831004 e3822001
c6d0  e5832008 e12fff1e e92d4010 e3014040 e34c407e e5940004 eb006777 e1a0300d
c6f0  e3c3cd7f e3032cd0 e3ccc03f e34c2078 e594300c e59cc014 e792210c e1a01000
c710  e5840008 e7930002 e8bd4010 ea015288 e59f304c e593000c e3500000 012fff1e

FP: 0xd3cead80:
ad80  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
ada0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
adc0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
ade0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
ae00  c10d5580 00000001 00000000 00000000 00000000 00000000 c10d5580 00000001
ae20  00000000 00000000 00000000 00000000 c10d5580 00000001 00000000 00000000
ae40  00000000 00000000 c10d5580 00000001 00000000 00000000 00000000 00000000
ae60  c10d5580 00000001 00000000 00000000 00000000 00000000 c10d5580 00000001

R0: 0xc07903b0:
03b0  c06a7998 c078f9ac c07903cc c07903a4 c06a79a4 c06a9e14 c0791738 c07903e0
03d0  c07903b8 c06a79b4 c06a9e14 c079178c c07903f4 c07903cc c06a79c4 c06a9e14
03f0  c07917e0 c0790408 c07903e0 00000000 c06a79d4 c07906d0 c079041c c07903f4
0410  00000000 c06a79e0 c078f568 c07cd698 c0790408 00000000 c06a79ec c078f5bc
0430  5f757063 006b6c63 00000000 00000000 00000000 00000000 00000000 00000000
0450  d40a0228 00000000 c078f4c0 00000000 00000001 00000000 00000000 c005ac70
0470  c005bc28 00000000 00000000 00000000 00000000 61746173 6b6c635f 00000000
0490  00000000 00000000 00000000 00000000 00000000 d4044aa8 00000000 c078f370

R2: 0xd3e51d58:
1d58  0000000d 00000001 010da000 c00469d0 c0790430 00000000 d3e51dd8 f40c4000
1d78  c07e1040 d6f15e8c 00000001 010da000 00200200 c111a588 00100100 d3ceae00
1d98  c004c6b0 d3e51db0 c006650c c005ac7c a0000193 ffffffff c07e1040 c006650c
1db8  c0059e84 c0059e90 c0059e84 c006650c c004c6d8 c004c6ec d3e51dd8 c00a799c
1dd8  d3e51dd8 d3e51dd8 c0783cd0 d3e50000 c003fc18 00000000 00000000 d3e51e20
1df8  d6085a00 c00412c0 ffffffff f2a00100 00000405 00000001 00000000 d3e50000
1e18  d6085a00 c0046a4c 00000000 010da000 00000000 d3e50000 d67c9c60 0000002a
1e38  00000001 00000001 c10d5580 00000000 d6085a00 d3ceae00 00000000 d3e51e68

R3: 0xf40c3f80:
3f80  ******** ******** ******** ******** ******** ******** ******** ********
3fa0  ******** ******** ******** ******** ******** ******** ******** ********
3fc0  ******** ******** ******** ******** ******** ******** ******** ********
3fe0  ******** ******** ******** ******** ******** ******** ******** ********
4000  ******** ******** ******** ******** ******** ******** ******** ********
4020  ******** ******** ******** ******** ******** ******** ******** ********
4040  ******** ******** ******** ******** ******** ******** ******** ********
4060  ******** ******** ******** ******** ******** ******** ******** ********

R4: 0xc07e0fc0:
0fc0  412fc09a 00000000 00000000 00000000 00000000 00000000 00000000 00000000
0fe0  c07a0b20 c07ccc64 00000000 00000000 00000000 c0798518 00000001 00000000
1000  00000001 00000000 00000000 d8fff000 00000000 c0067230 c00542e0 00000000
1020  10004000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
1040  d9800600 c0790874 0bcd3d80 c0043028 00000000 00000000 00030000 00000005
1060  00000001 00000001 00000004 00000000 00000000 c078c518 00000000 00000000
1080  00000000 00000000 00000000 d60e8000 d60e9000 d60ea000 d60eb000 d60ec000
10a0  d60ed000 d60ee000 d60ef000 d60f0000 d60f1000 d60f2000 d60f3000 d60f4000

R5: 0xd6f15e0c:
5e0c  00000002 00000001 c0046a4c c0574e78 00000005 f2a01000 00000001 d6f15e8c
5e2c  c111a580 00000000 c111a580 010da000 c111a588 00000001 c0574f04 00000000
5e4c  d6f15e60 c004bbac c00a708c 20000113 ffffffff d6f14000 00000000 c004c6d8
5e6c  00000001 c0574f00 c0783cd0 d6f15f3c c00a71c0 c0041eb0 d6134600 80002001
5e8c  00100100 00200200 c004c6d8 00000000 00000001 00018d00 ffffffff c07ccdcc
5eac  00000000 d6f15f3c 00000001 d6f15f3c c004c850 c004c808 c0098c2c c07ff7fc
5ecc  c07ff7e4 00000000 00000001 ffffffff c0098d80 00000000 001312d0 00000000
5eec  d6f15f3c d63128e0 00000000 c0783ac4 00000004 c0783b00 c0098db4 00000000

R9: 0xc111a508:
a508  00008288 00000000 2b85e900 00000006 00000000 00000000 0008f4da 00000000
a528  ffff968e ffffffe5 d6f93800 00000000 00000000 00000000 00000000 00000000
a548  00000000 00000000 00000000 00000000 00000000 00000000 c07740e0 00200200
a568  c00972ac 00000000 00000000 00000000 00000000 00000000 c111a580 c111a580
a588  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
a5a8  00000000 00000000 00000000 00000000 00000000 00000000 00000000 c111a5c0
a5c8  c111a5c8 c111a5c8 00000000 c111a5d4 c111a5d4 00000000 00000000 00000000
a5e8  00000084 00000000 00000000 00000000 00000000 00000000 00000000 00000000
Process WindowManagerPo (pid: 2301, stack limit = 0xd3e502f0)
Stack: (0xd3e51db0 to 0xd3e52000)
1da0:                                     c07e1040 c006650c c0059e84 c0059e90
1dc0: c0059e84 c006650c c004c6d8 c004c6ec d3e51dd8 c00a799c d3e51dd8 d3e51dd8
1de0: c0783cd0 d3e50000 c003fc18 00000000 00000000 d3e51e20 d6085a00 c00412c0
1e00: ffffffff f2a00100 00000405 00000001 00000000 d3e50000 d6085a00 c0046a4c
1e20: 00000000 010da000 00000000 d3e50000 d67c9c60 0000002a 00000001 00000001
1e40: c10d5580 00000000 d6085a00 d3ceae00 00000000 d3e51e68 c0103478 c0114ba8
1e60: 60000013 ffffffff c0103478 c0114b38 60000013 c0103478 00000000 00000001
1e80: d3e51f40 00000001 00000001 0000000e d3e50000 d4288e7c ffffffff fffffdee
1ea0: d6085a00 00000000 00000000 d3e51f80 d3e50000 00000000 5c66e6f4 c00fb338
1ec0: 00000000 00000000 d61e0f8c 00000000 00000000 00000001 ffffffff d6085a00
1ee0: 00000000 00000000 00000000 00000000 d6f93be0 c0047184 00000000 00000000
1f00: 00000000 00000000 d3e51f08 d3e51f08 00000001 d3e50000 00000001 d624ea48
1f20: d6ee11a0 00000001 00000001 00000000 00000000 00000000 5eacafff d624ea48
1f40: 4007a0e4 00000000 d6085a00 00000001 4007a0e3 d3e51f80 00000001 c00fba3c
1f60: 00000000 c00fd050 d6085a00 4007a0e3 00000000 00000000 00000001 c00fbcac
1f80: 00000000 00000000 006ae0fc 00000001 4007a0e3 006ae0e8 00000000 00000004
1fa0: c0047184 c0047000 4007a0e3 006ae0e8 0000005d 4007a0e3 00000001 5bc63d90
1fc0: 4007a0e3 006ae0e8 00000000 00000004 5c66e6e0 5bc63d38 00000000 5c66e6f4
1fe0: 4007d058 5c66e6b8 40075d1b 400c5474 20000010 0000005d 00000000 00000000
[<c005ac7c>] (_clk_arm_get_rate+0xc/0x28) from [<c006650c>] (clk_get_rate+0x40/0x50)
[<c006650c>] (clk_get_rate+0x40/0x50) from [<c0059e90>] (_clk_twd_get_rate+0xc/0x14)
[<c0059e90>] (_clk_twd_get_rate+0xc/0x14) from [<c006650c>] (clk_get_rate+0x40/0x50)
[<c006650c>] (clk_get_rate+0x40/0x50) from [<c004c6ec>] (twd_update_frequency+0x14/0x48)
[<c004c6ec>] (twd_update_frequency+0x14/0x48) from [<c00a799c>] (generic_smp_call_function_s                                 ingle_interrupt+0xd0/0x130)
[<c00a799c>] (generic_smp_call_function_single_interrupt+0xd0/0x130) from [<c00412c0>] (do_I                                 PI+0xec/0x208)
[<c00412c0>] (do_IPI+0xec/0x208) from [<c0046a4c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xd3e51e20 to 0xd3e51e68)
1e20: 00000000 010da000 00000000 d3e50000 d67c9c60 0000002a 00000001 00000001
1e40: c10d5580 00000000 d6085a00 d3ceae00 00000000 d3e51e68 c0103478 c0114ba8
1e60: 60000013 ffffffff
[<c0046a4c>] (__irq_svc+0x4c/0xe8) from [<c0114ba8>] (mnt_drop_write+0x70/0xa4)
[<c0114ba8>] (mnt_drop_write+0x70/0xa4) from [<c0103478>] (pipe_write+0x26c/0x510)
[<c0103478>] (pipe_write+0x26c/0x510) from [<c00fb338>] (do_sync_write+0xa4/0xe4)
[<c00fb338>] (do_sync_write+0xa4/0xe4) from [<c00fba3c>] (vfs_write+0xa8/0x138)
[<c00fba3c>] (vfs_write+0xa8/0x138) from [<c00fbcac>] (sys_write+0x40/0x6c)
[<c00fbcac>] (sys_write+0x40/0x6c) from [<c0047000>] (ret_fast_syscall+0x0/0x30)
Code: c078e260 e3a03901 e34f240c e92d4010 (e5934010)
---[ end trace dcbcbc34e4f8c36f ]---
Kernel panic - not syncing: Fatal exception in interrupt
[<c004cdb0>] (unwind_backtrace+0x0/0xf8) from [<c056c398>] (panic+0x74/0x18c)
[<c056c398>] (panic+0x74/0x18c) from [<c004aad4>] (die+0x220/0x284)
[<c004aad4>] (die+0x220/0x284) from [<c056c1a8>] (__do_kernel_fault.part.3+0x54/0x74)
[<c056c1a8>] (__do_kernel_fault.part.3+0x54/0x74) from [<c0050ae0>] (do_translation_fault+0x                                 0/0xa0)
[<c0050ae0>] (do_translation_fault+0x0/0xa0) from [<f40c4010>] (0xf40c4010)
CPU1: stopping
[<c004cdb0>] (unwind_backtrace+0x0/0xf8) from [<c00413a8>] (do_IPI+0x1d4/0x208)
[<c00413a8>] (do_IPI+0x1d4/0x208) from [<c0046a4c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xd6f15e18 to 0xd6f15e60)
5e00:                                                       c0574e78 00000005
5e20: f2a01000 00000001 d6f15e8c c111a580 00000000 c111a580 010da000 c111a588
5e40: 00000001 c0574f04 00000000 d6f15e60 c004bbac c00a7088 20000113 ffffffff
[<c0046a4c>] (__irq_svc+0x4c/0xe8) from [<c00a7088>] (generic_exec_single+0x70/0x90)
[<c00a7088>] (generic_exec_single+0x70/0x90) from [<c00a71c0>] (smp_call_function_single+0x1                                 18/0x1d0)
[<c00a71c0>] (smp_call_function_single+0x118/0x1d0) from [<c004c850>] (twd_cpufreq_transitio                                 n+0x48/0x58)
[<c004c850>] (twd_cpufreq_transition+0x48/0x58) from [<c0098c2c>] (notifier_call_chain+0x44/                                 0x84)
[<c0098c2c>] (notifier_call_chain+0x44/0x84) from [<c0098d80>] (__srcu_notifier_call_chain+0                                 x44/0x60)
[<c0098d80>] (__srcu_notifier_call_chain+0x44/0x60) from [<c0098db4>] (srcu_notifier_call_ch                                 ain+0x18/0x20)
[<c0098db4>] (srcu_notifier_call_chain+0x18/0x20) from [<c037e508>] (cpufreq_notify_transiti                                 on+0xa0/0xe0)
[<c037e508>] (cpufreq_notify_transition+0xa0/0xe0) from [<c006959c>] (mxc_set_target+0x194/0                                 x220)
[<c006959c>] (mxc_set_target+0x194/0x220) from [<c037dcc4>] (__cpufreq_driver_target+0x50/0x                                 64)
[<c037dcc4>] (__cpufreq_driver_target+0x50/0x64) from [<c0382aa8>] (cpufreq_interactive_up_t                                 ask+0x168/0x1b4)
[<c0382aa8>] (cpufreq_interactive_up_task+0x168/0x1b4) from [<c00939b0>] (kthread+0x80/0x88)
[<c00939b0>] (kthread+0x80/0x88) from [<c0047ae4>] (kernel_thread_exit+0x0/0x8)

ラベル(1)
添付
コメント

Hi Jim,

The best way to get your question answered is to Start a Discussion in the i.MX Community. Documents are mostly used to provide documentation and answers.

5-21-2013 11-26-58.png

I hope this helps!

This stack dump indicates that you don't have the LDO ramp patch applied, so the clock rate is being changed before a couple of LDOs have completed ramping to the new voltage.

This was done in an update to R13.4.1-GA (I can't recall which... check Enrique's posts).

評価なし
バージョン履歴
最終更新日:
‎04-12-2013 02:51 AM
更新者: