i.MX6 Android 13.4.1.03 Patch Release

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Android 13.4.1.03 Patch Release

i.MX6 Android 13.4.1.03 Patch Release

The i.MX 6 Android 13.4.1.03 patch release is now available on www.freescale.com

IMX6_R13.4103_ANDROID_LDO_PATCH

This patch release is based on the i.MX6 Android R13.4.1 release. The purpose of this patch release is to manage the LDO and PMIC ramp-up time correctly.

ラベル(5)
タグ(3)
コメント

This link seems to be broken. I get:

Error 500--Internal Server Error

From RFC 2068 Hypertext Transfer Protocol -- HTTP/1.1:

10.5.1 500 Internal Server Error

The server encountered an unexpected condition which prevented it from fulfilling the request.

This patch is no longer available because all the content of this patch was also incorporated on the Android R13.4.1.04.

What is the build host configuration needed to build Freescale's Android releases?  I've had difficulty on a Ubuntu 12.04 64bit configuration... it would be nice to see a description of the build host and pre-reqs needed in the Android releases.

Tim

I think the most successful host so far is Ubuntu 10.04 64bits. For newer Ubuntu's versions, there are some patches but you may run into issues even if these are applied.

BTW, post the error's log.

Leo

評価なし
バージョン履歴
最終更新日:
‎03-05-2013 09:22 AM
更新者: