The edit-compile-test loop is the quickest way so can test your changes.
1. Go to the package's source code folder and edit your files.
2. Compile that particular package, e.g.
bitbake linux-imx -c compile -f
3. Deploy, e.g.
bitbake linux-imx -c deploy
4. Insert the SD card into your host, and copy the Linux kernel into the the first partition
sudo cp tmp/deploy/images/uImage /media/Boot
5. Insert the SD card into your board, boot and test your changes
6. In case you are satisfied with the results, you need to create a patch and add into the package's recipe. Check this document to execute this step.
Corrected. Thanks!
I use (modified) wandboard linux for developing and I use this command line:
bitbake linux-wandboard -c compile -f && ./sendkernel.sh
The content of sendkernel is:
#!/bin/sh
ssh root@imx 'mount /dev/mmcblk0p1 /mnt/mmcblk0p1'
scp tmp/work/wandboard_quad-poky-linux-gnueabi/linux-wandboard/3.0.35-r0/git/arch/arm/boot/uImage root@imx:/mnt/mmcblk0p1
ssh root@imx reboot
It copies only the kernel itself without the modules and do not do "deploy" what is much slower.
Hope it helps. :smileyhappy:
Thanks. You are avoiding the deploying step. I usually execute the deploy task, because I may deploy other kernels and the link /tmp/deploy/images/uImage will point to the latest, so TFTP transfer (from u-boot) will always pick this one...
Leo
Dear Leonardo Sandoval Gonzalez,
Thanks for your document it was helpful to me.
I am having a few doubts.
My purpose:I have to boot t4240qds.
using:Ubuntu 12.04 , SDK 1.4 , created a fsl-image-core.
I have seen the information center and other references but still i am quite doubtful.
1) should I surely modify the u-boot? in the sense what can be achieved by doing so ? Also what i have to modify to boot t4240qds ?
2) can i boot from sd card ? if so then do i need a tftp server?
Can you please clarify?
Thanks
Aravind
Aravind, I am not familiar with that board. In general, for a board boot-up, you do not need yocto at this point.In the other hand, the TFTP server is commonly used for kernel development, in the sense that you recompile the kernel, move the Image to the server and reboot the board to see the changes.
Leo
Dear Leo,
Never mind.
Thanks for your response.
Do you have any idea for testing of mport driver ( IDT Tsi721 PCI Express SRIO Controller support ) ?
I have modified the kernel to enable the above support and also copied the images.
Any procedures or test cases for the testing will be very helpful.
Thanks
Aravind
Hi Aravind
Sorry for the delay.
1. -f means force a task to be executed. This is necessary when code is modified on tmp folder, otherwise it would not take into account all changes you have done.
2. I have no idea about the testing you need.
Dear Leo
Thanks for your response.
Aravind
On Sep 8, 2014 11:24 PM, "Leonardo Sandoval Gonzalez" <
Dear Leo,
Thanks for your document.
Why do we use compile?
Does not compile when I use compile?
Thanks
Yasarcan