i.MX Linux L4.1.15_2.0.3 Patch for i.MX 6ULL@900MHz Release Announcement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Linux L4.1.15_2.0.3 Patch for i.MX 6ULL@900MHz Release Announcement

i.MX Linux L4.1.15_2.0.3 Patch for i.MX 6ULL@900MHz Release Announcement

  1. The Linux L4.1.15_2.0.3 Patch for i.MX 6ULL@900MHz Release is now available on www.nxp.com. BSP Updates and Releases -> Linux -> Linux 4.1.15_2.0.3 Patch.

 

  • Files available:

#

Name

Description

1

L4.1.15_2.0.3_6ULL_patch_images.tar.gz

i.MX 6ULL-EVK@900MHz Linux Binary Demo Files

 

  • Information of release, see:

README: http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-4.1-krogoth

ChangeLog: http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/ChangeLog?h=imx-4.1-krogoth

Labels (2)
Comments

I see this link BSP Updates and Releases -> Linux -> Linux 4.1.15_2.0.3 Patch-> Source Code, when I click the link of Source Code under Linux 4.1.15_2.0.3 Patch, the webpage jump to “Freescale Public GIT”, how can I find the detailed source code patch?

No ratings
Version history
Last update:
‎04-11-2017 10:57 PM
Updated by: