i.MX 8MP LVDS seamless display (连续显示) between U-boot and Kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8MP LVDS seamless display (连续显示) between U-boot and Kernel

i.MX 8MP LVDS seamless display (连续显示) between U-boot and Kernel

Please notice the following patches are only tested in the environment that is listed below. For the environment with other software versions or hardware equipment, some other editing  may be required

Environment:

  • i.MX 8MP EVK

  • LVDS:LVDS BOE EV121WXM-N10-1850 

  • LVDS to MiniSAS panel:XMX-LVDS-MINISAS

  • Software: LF5.15.71

U-boot:

1. Apply '0001-Enable-DY1212W-4856-in-U-boot-for-i.MX8MP.patch' to enable EV121WXM-N10-1850  in U-boot stage. If other LVDS panel is used here, you will need porting your specific LVDS device in this step.

2. Apply '0002-Modify-u-boot-to-show-logo-seamlessly-for-i.MX8MP.patch' to make sure display related models won't be power off, which will help to achieve seamless display.

3. In the original U-boot driver, PWM isn't enable. Therefore, apply '0003-Enable-PWM-and-BACKLIGHT-in-U-boot-and-modify-to-sho.patch' to enable PWM.

Kernel:

1. Apply '0001-Enable-DY1212W-4856-in-Kernl-for-i.MX8MP.patch' to enable EV121WXM-N10-1850  in Kernel. If other LVDS panel is used here, you will need porting your specific LVDS device in this step.

2. Apply '0002-Modify-Kernel-to-show-logo-seamlessly-for-i.MX8MP.patch' to make sure LVDS related models won't be init in the booting progress.

3. Apply '0003-Enable-PWM-and-BACKLIGHT-in-Kernel-and-modify-to-sho.patch' to make sure we could edit backlight of panel in Kernel. 

附件
无评分
版本历史
最后更新:
‎12-09-2024 09:08 AM
更新人: