Important: If you have any questions or would like to report any issues with the DDR tools or
supporting documents please create a support ticket in the i.MX community. Please note that any
private messages or direct emails are not monitored and will not receive a response.
NOTE: Please note that DDR support for the i.MX 8M Family and has also been added in the
Config Tools for i.MX Applications Processors | NXP Semiconductors
Please consider using this tool with more enhanced features.
The i.MX 8M Family DDR Tool is a Windows-based software to help users to do LPDDR4/DDR4/DDR3L training, stress test and DDR initial code generation for u-boot SPL. This page contains the latest releases for the i.MX 8M Family DDR Tools and cover the following SoCs :
NOTE: For the i.MX 8/8X Family of DDR tools please refer to the:
i.MX 8/8X Family DDR Tools Release
The purpose of the i.MX 8M Family DDR Tools is to enable users to generate and test a custom DRAM initialization based on their device configuration (density, number of chip selects, etc.) and board layout (data bus bit swizzling, etc.). This process equips the user to then proceed with the bring-up of a boot loader and an OS. Once the OS is brought up, it is recommended to run an OS-based memory test (like Linux memtester) to further verify and test the DDR memory interface.
The i.MX 8M Family DDR Tools consist of:
For more details regarding these DDR tools and their usage, refer to the i.MX 8M DDR Tools User Guide.
The i.MX 8M Family DDR stress test tool is a Windows-based software tool that is used as a mechanism to verify that the DDR initialization is operational for use with u-boot and OS bring-up. To install the DDR Stress Test, save and extract the zip file mscale_ddr_tool_vXXX_setup.exe.zip (where 'xxx' is the current version number) and follow the on-screen installation instructions.
The i.MX 8M DDR tool includes the document: MSCALE_DDR_Tool_User_Guide
NOTE: Please read the MSCALE_DDR_Tool_User_Guide inside the package carefully before you
use this tool.
|
Rev |
Major Changes* (Features) | Comments |
|---|---|---|
| 3.31 |
|
|
| 3.30 |
|
|
| 3.20 |
|
|
| 3.10 |
|
|
| 3.00 |
|
Note that the DDR3L and LPDDR4 RPAs contain the name preliminary only to denote that these RPAs are based on internal NXP validation boards where the DDR4 RPA is based on the released EVK. |
| 2.10 |
|
|
| 2.00 |
|
* Further details available in the release notes
Sample configuration in the .ds script for i.MX 8M debug UART2:
################step 0: configure debug uart port. Assumes use of UART IO Pads. #####
|
||||
##### If using non-UART pads (i.e. using other pads to mux out the UART signals), #####
|
||||
##### then it is up to the user to overwrite the following IO register settings #####
|
||||
memory set
|
0x3033023C
|
32
|
0x00000000
|
#IOMUXC_SW_MUX_UART2_RXD
|
memory set
|
0x30330240
|
32
|
0x00000000
|
#IOMUXC_SW_MUX_UART2_TXD
|
memory set
|
0x303304A4
|
32
|
0x0000000E
|
#IOMUXC_SW_PAD_UART2_RXD
|
memory set
|
0x303304A8
|
32
|
0x0000000E
|
#IOMUXC_SW_PAD_UART2_TXD
|
memory set
|
0x303304FC
|
32
|
0x00000000
|
#IOMUXC_SW_MUX_UART2_SEL_RXD
|
sysparam set
|
debug_uart
|
1
|
#UART index from 0 ('0' = UART1, '1' = UART2, '2' = UART3, '3' = UART4)
|
|
Sample configuration in the front of the .ds script for i.MX 8M debug UART3
################step 0: configure debug uart port. Assumes use of UART IO Pads. #####
|
||||
##### If using non-UART pads (i.e. using other pads to mux out the UART signals), #####
|
||||
##### then it is up to the user to overwrite the following IO register settings #####
|
||||
memory set
|
0x30330244
|
32
|
0x00000000
|
#IOMUXC_SW_MUX_UART3_RXD
|
memory set
|
0x30330248
|
32
|
0x00000000
|
#IOMUXC_SW_MUX_UART3_TXD
|
memory set
|
0x303304AC
|
32
|
0x0000000E
|
#IOMUXC_SW_PAD_UART3_RXD
|
memory set
|
0x303304B0
|
32
|
0x0000000E
|
#IOMUXC_SW_PAD_UART3_TXD
|
memory set
|
0x30330504
|
32
|
0x00000002
|
#IOMUXC_SW_MUX_UART3_SEL_RXD
|
sysparam set
|
debug_uart
|
2
|
#UART index from 0 ('0' = UART1, '1' = UART2, '2' = UART3, '3' = UART4)
|
|
Sample configuration in the front of the .ds script for i.MX 8M Mini PMIC configuration:
##############step 0.5: configure I2C port IO pads according to your PCB design. ##### ########### You can modify the following instructions to adapt to your board PMIC #######
memory set
|
0x30330214
|
32
|
0x00000010
|
#IOMUXC_SW_MUX_I2C1_SCL
|
memory set
|
0x30330218
|
32
|
0x00000010
|
#IOMUXC_SW_MUX_I2C1_SDA
|
memory set
|
0x3033047C
|
32
|
0x000000C6
|
#IOMUXC_SW_PAD_I2C1_SCL
|
memory set
|
0x30330480
|
32
|
0x000000C6
|
#IOMUXC_SW_PAD_I2C1_SDA
|
sysparam set
|
pmic_cfg
|
0x004B
|
#bit[7:0] = PMIC addr,bit[15:8]=I2C Bus.
|
Bus index from 0 ('0' = I2C1, '1' = I2C2, '2' = I2C3, '3' = I2C4)
|
sysparam set
|
pmic_set
|
0x2F01
|
#bit[7:0] = Reg val, bit[15:8]=Reg addr.
|
#REG(0x2F) = 0x01
|
sysparam set
|
pmic_set
|
0x0C02
|
#REG(0x0C) = 0x02
|
|
sysparam set
|
pmic_set
|
0x171E
|
#REG(0x17) = 0x1E
|
|
sysparam set
|
pmic_set
|
0x0C00
|
#REG(0x0C) = 0x00
|
|
sysparam set
|
pmic_set
|
0x2F11
|
#REG(0x2F)=0x11
|
The i.MX 8M DDR RPA (or simply RPA) is an Excel spreadsheet tool used to develop DDR initialization for a user’s specific DDR configuration (DDR device type, density, etc.). The RPA generates the DDR initialization(in a separate Excel worksheet tab):
i.MX 8M Family DDR Register Programming Aid (RPA): Current Versions
To obtain the latest RPAs, please refer to the following links (note, existing RPAs have been removed from this main page and moved to the SoC specific links below):
i.MX 8M Quad :
i.MX 8M Mini :
i.MX 8M Nano:
i.MX 8M Plus:
| Processor | Mask Revisions | Memory Supported | Latest RPA Version * |
|---|---|---|---|
| i.MX 8M Quad & Derivatives | All | LPDDR4 | Rev 33 |
| i.MX 8M Quad & Derivatives | All | DDR4 | Rev 18 |
| i.MX 8M Quad & Derivatives | All | DDR3L | Rev 9 |
| i.MX 8M Mini & Derivatives | A0 | LPDDR4 | Rev 22 |
| i.MX 8M Mini & Derivatives | A0 | DDR4 | Rev 21 |
| i.MX 8M Mini & Derivatives | A0 | DDR3L | Rev 10 |
| i.MX 8M Nano & Derivatives | A0 | LPDDR4 | Rev 9 |
| i.MX 8M Nano & Derivatives | A0 | DDR4 | Rev 12 |
| i.MX 8M Nano & Derivatives | A0 | DDR3L | Rev 6 |
| i.MX 8M Plus & Derivatives | A1 | LPDDR4 | Rev 9 |
| i.MX 8M Plus & Derivatives | A1 | DDR4 | Rev 9 |
* For the details about the updates, please refer to the Revision History tab of the respective RPA.
To modify the DRAM Frequency for a custom setting refer to iMX 8M Mini Register Programming Aid DRAM PLL setting
Related Resources Links:
Scroll down to “Other Resources --> Tools --> DDR Tools”
Great. Thank You