i.MX 6 D/Q/DL/S/SL Android jb4.3_1.1.0 GA release

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 6 D/Q/DL/S/SL Android jb4.3_1.1.0 GA release

i.MX 6 D/Q/DL/S/SL Android jb4.3_1.1.0 GA release

Hi All,

The new Android JB4.3_1.1.0-GA release is now available on www.freescale.com

·         Files available

         

Name

Description

IMX6_JB43_110_ANDROID_DOCS

i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0 BSP Documentation. Includes Release Notes, User's Guide, QSG and   FAQ Sheet.

IMX6_JB43_110_ANDROID_SOURCE_BSP

i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0 BSP, Documentation and Source Code for BSP and Codecs.

IMX6_JB43_110_ANDROID_DEMO_BSP

i.MX   6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Android   jb4.3_1.1.0  BSP Binary Demo Files

IMX6_JB43_110_AACP_CODEC_CODA

AAC   Plus Codec for i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX   6Sololite Android jb4.3_1.1.0

·         Target HW boards

o   i.MX6DL  SABRE SD board

o   i.MX6Q  SABRE SD board

o   i.MX6DQ SABRE AI board

o   i.MX6DL SABRE AI board

o   i.MX6SL EVK board

·         Release Description

i.MX Android jb4.3_1.1.0 release includes all necessary codes, documents and tools to assist users in building and running Android 4.3 on the i.MX 6Quad, i.MX 6DualLite and i.MX6SoloLite hardware board from the scratch.

The prebuilt images are also included for a quick trial on Freescale i.MX 6Quad and i.MX 6DualLite SABRE-SD Board and Platform, i.MX 6Quad and i.MX 6DualLite SABRE-AI Board and Platforms and i.MX6SoloLite EVK Board and Platforms.

This release includes all Freescale porting and enhancements based on Android open source code. Most of deliveries in this release are provided in source code with the exception of some proprietary modules/libraries from third parties.

·         What's in this release

       

Android Source Code Patch

All   Freescale i.MX specific patches (apply to Google Android

repo)   to enable Android on i.MX based boards. For example

Hardware   Abstraction Layer implementation, hardware codec

acceleration,   etc.

Packed in   android_jb4.3_1.1.0-ga_source.tar.gz

Documents

The   following documents are included in android_jb4.3_1.1.0-ga_docs.tar.gz:

●   i.MX Android jb4.3_1.1.0-ga Quick Start:

A   manual explains how to run android on i.MX board by using prebuilt images.

●   i.MX Android jb4.3_1.1.0-ga User Guide:

A   detailed manual for this release package.

●   i.MX Android jb4.3_1.1.0-ga FAQ:

A document lists   “Frequently Asked Questions”.

●   i.MX Android Codec Release Notes:

A   document to describes the Freescale Codec Package

●   i.MX Android Wi-FI Display Sink API Introduction

A   document to describes how to use i.MX Android Wi-Fi Display Sink API

●   i.MX6 G2D API User Guide document to introduce how to use i.MX6 G2D API for   2D BLT usage

●   i.MX Android jb4.3_1.1.0-ga Release Note

A   document to introduce the key updates and known issues in this release.

Tools

Tools   in android_jb4.3_1.1.0-ga_tools.tar.gz

  MFGTool. Manufacturing tools for i.MX platform

  USB tethering windows .inf driver configure file.tool/tetherxp.inf

Prebuilt Images

You   can test Android on i.MX with prebuilt image on i.MX board before building   any code.

android_jb4.3_1.1.0-ga_image_6qsabresd.tar.gz:

Prebuilt   images for the SABRE-SD board.

  android_jb4.3_1.1.0-ga_image_6qsabreauto.tar.gz:

Prebuilt   images for the SABRE-AI board.

  android_jb4.3_1.1.0-ga_image_6slevk.tar.gz: Prebuilt images for the 6SL   SABRE-AI board.

All   prebuilt images are in another package. See "i.MX Android jb4.3_1.1.0-ga   Quick Start" and "i.MX Android jb4.3_1.1.0-ga User Guide" to   understand which image should be used in which case.

·         Known issues

For known issues and limitations please consult the release notes

标记 (2)
无评分
版本历史
最后更新:
‎12-20-2013 12:02 PM
更新人: