help in porting Android Jb to imx6q custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

help in porting Android Jb to imx6q custom board

help in porting Android Jb to imx6q custom board

Hi all,

I'm trying to port Android JB to a custom board based on imx6q.

I'm not able to get the launcher. And even the display is shifting to right. The kernel i've tested with linux where the display is proper.

Below is log.

In the log Marked are the issues I'm facing.

Any advice is helpful.

I'm in very critical stage. Please help me to resolve this. I'm the source from android_jb4.2.2_1.0.0-ga_source bundle package.

Uncompressing Linux... done, booting the kernel.

Initializing cgroup subsys cpu

Linux version 3.0.35-gcbaa4e0-dirty (rangam@PHYTECIndia) (gcc version 4.4.1 (Sourcery G++ Lite 2009q3-67) ) #11 SMP PREEMPT Fri Jul 26 16:57:13 IST 2013

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Phytec

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @c13ec000 s6592 r8192 d13888 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 215040

Kernel command line: console=ttymxc3,115200 androidboot.hardware=freescale androidboot.console=ttymxc3  init=/init vmalloc=256M video=mxcfb1:dev=ldb,Primeview-PM070WL4,bpp

=16 fbmem=10M vt.global_cursor_default=0 consoleblank=0 board_mx6q_phyflex.csi0=none board_mx6q_phyflex.csi1=none video=mxcfb1:off video=mxcfb2:off ip=none root=/dev/mmcbl

k0p2 rootfstype=ext4 noinitrd rootwait mtdparts=n25q128:512k(barebox)ro,128k(bareboxenv),2M(splash),-(kernel);gpmi-nand:512k(barebox)ro,128k(bareboxenv),2M(splash),8M(kern

el),-(root)

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 592MB 256MB = 848MB total

Memory: 847036k/847036k available, 201540k reserved, 311296K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)

    vmalloc : 0xe2800000 - 0xf2000000   ( 248 MB)

    lowmem  : 0xc0000000 - 0xe2000000   ( 544 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .init : 0xc0008000 - 0xc0047000   ( 252 kB)

      .text : 0xc0047000 - 0xc09dbebc   (9812 kB)

      .data : 0xc09dc000 - 0xc0a59f18   ( 504 kB)

       .bss : 0xc0a59f3c - 0xc0be2d40   (1572 kB)

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x21f0000 (options '115200')

bootconsole [ttymxc3] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 789.70 BogoMIPS (lpj=3948544)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys cpuacct

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

CPU2: Booted secondary processor

CPU3: Booted secondary processor

Brought up 4 CPUs

SMP: Total of 4 processors activated (3158.83 BogoMIPS).

devtmpfs: initialized

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

imx_add_mxc_pwm:pdata=  (null)

imx_add_mxc_pwm:pdata=  (null)

imx_add_mxc_pwm:pdata=  (null)

imx_add_mxc_pwm:pdata=  (null)

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B

bio: create slab <bio-0> at 0

mxs-dma mxs-dma-apbh: initialized

print_constraints: vmmc: 3300 mV

print_constraints: IOVDD: 3300 mV

print_constraints: DVDD: 1800 mV

print_constraints: AVDD: 3300 mV

print_constraints: DRVDD: 3300 mV

vgaarb: loaded

i2c-core: driver [da9063] using legacy suspend method

i2c-core: driver [da9063] using legacy resume method

SCSI subsystem initialized

spi_imx imx6q-ecspi.2: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

i2c-gpio i2c-gpio.3: using pins 109 (SDA) and 108 (SCL)

print_constraints: VDDCORE: 730 <--> 1280 mV at 1300 mV at 2000 mA normal

print_constraints: VDDSOC: 730 <--> 1280 mV at 1300 mV at 500 mA normal

print_constraints: VDD_DDR3: 1500 mV at 2000 mA

print_constraints: VDD_3V3: 3300 mV at 1500 mA

print_constraints: VDD_BUCKMEM: 3300 mV at 1500 mA

print_constraints: VDD_ETH: 1200 mV at 3000 mA

print_constraints: VDD_ETH_IO: 3300 mV

print_constraints: VDD_MX6_SNVS: 3300 mV

print_constraints: VDD_3V3_PMIC_IO: 3300 mV

print_constraints: VDD_SD0: 3300 mV

print_constraints: VDD_SD1: 3300 mV

print_constraints: VDD_MX6_HIGH: 3000 mV

da9063 0-0058: Device detected DA9063

max7300: probe of 0-0040 failed with error -5

stmpe 1-0041: stmpe811 detected, chip id: 0x811

stmpe 2-0041: failed to read regs 0x0: -5

stmpe: probe of 2-0041 failed with error -5

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

cfg80211: Calling CRDA to update world regulatory domain

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

TCP: Hash tables configured (established 131072 bind 65536)

TCP reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Static Power Management for Freescale i.MX6

wait mode is enabled for i.MX6

cpaddr = e2880000 suspend_iram_base=e291c000

PM driver module loaded

link up failed, DB_R0:0x00913b00, DB_R1:0x08200000!

IMX PCIe port: link down with power supply 0!

IMX usb wakeup probe

add wake up source irq 75

IMX usb wakeup probe

cpu regulator mode:ldo_bypass

_regulator_get: get() with no identifier

mx6_cpu_regulator_init: failed to get pu regulator

i.MXC CPU frequency driver

highmem bounce pool size: 64 pages

ashmem: initialized

NTFS driver 2.1.30 [Flags: R/O].

JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.

fuse init (API version 7.16)

msgmni has been set to 1046

NET: Registered protocol family 38

cryptodev: driver loaded.

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb

_regulator_get: get() with no identifier

ldb_clk to di clk: ldb_di0_clk -> ipu1_di0_clk

mxc_sdc_fb mxc_sdc_fb.1: mxcfb1 is turned off!

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX

console [ttymxc3] enabled, bootconsole disabled

console [ttymxc3] enabled, bootconsole disabled

loop: module loaded

at24 0-0050: 4096 byte 24c32 EEPROM, writable, 8 bytes/write

at24 2-0052: 512 byte 24c04 EEPROM, writable, 16 bytes/write

No sata disk.

m25p80 spi2.0: unrecognized id n25q128

m25p80 spi2.0: unrecognized JEDEC id 20ba18

GPIO NAND driver, �© 2004 Simtec Electronics

NAND device: Manufacturer ID: 0xec, Chip ID: 0xd3 (Samsung NAND 1GiB 3,3V 8-bit)

5 cmdlinepart partitions found on MTD device gpmi-nand

Creating 5 MTD partitions on "gpmi-nand":

0x000000000000-0x000000080000 : "barebox"

0x000000080000-0x0000000a0000 : "bareboxenv"

0x0000000a0000-0x0000002a0000 : "splash"

0x0000002a0000-0x000000aa0000 : "kernel"

0x000000aa0000-0x000040000000 : "root"

GPMI NAND driver registered. (IMX)

vcan: Virtual CAN interface driver

CAN device driver interface

flexcan netdevice driver

flexcan imx6q-flexcan.0: device registered (reg_base=e29b0000, irq=142)

FEC Ethernet Driver

fec_enet_mii_bus: probed

PPP generic driver version 2.4.2

PPP Deflate Compression module registered

PPP BSD Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

PPTP driver version 0.8.5

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: Freescale On-Chip EHCI Host Controller

usb usb1: Manufacturer: Linux 3.0.35-gcbaa4e0-dirty ehci_hcd

usb usb1: SerialNumber: fsl-ehci.0

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

add wake up source irq 72

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb2: Product: Freescale On-Chip EHCI Host Controller

usb usb2: Manufacturer: Linux 3.0.35-gcbaa4e0-dirty ehci_hcd

usb usb2: SerialNumber: fsl-ehci.1

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

Gadget Android: controller 'fsl-usb2-udc' not recognized

android_usb gadget: android_usb ready

Suspend udc for OTG auto detect

fsl-usb2-udc: bind to driver android_usb

mousedev: PS/2 mouse device common for all mice

input: stmpe-ts as /devices/virtual/input/input0

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

using rtc device, da9063-rtc, for alarms

da9063-rtc da9063-rtc: rtc core: registered da9063-rtc as rtc0

da9063-rtc da9063-rtc: Failed to request ALARM IRQ.

rtc-pcf8563 1-0051: chip found, driver version 0.4.3

rtc-pcf8563 1-0051: rtc core: registered rtc-pcf8563 as rtc1

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc2

i2c /dev entries driver

Linux video capture interface: v2.00

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17

usbcore: registered new interface driver uvcvideo

USB Video Class driver (v1.1.0)

Driver for 1-wire Dallas network protocol.

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCILL protocol initialized

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA

w1_master_driver w1 bus master: Family 43 for 43.000000436e56.c7 is not registered.

mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA

VPU initialized

mxc_asrc registered

revserved_memory_account:viv_gpu registerd

Thermal calibration data is 0x5914c97d

Thermal sensor with ratio = 185

w1_master_driver w1 bus master: Family 43 for 43.0000003be6e7.b6 is not registered.

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

HDMI CEC initialized

leds-pca953x 1-0062: setting platform data

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

usb 2-1: new high speed USB device number 2 using fsl-ehci

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

usbcore: registered new interface driver snd-usb-audio

mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio

imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.

tlv320aic3x-codec 1-0018: asoc: failed to add kcontrol Left Line1R Mux

tlv320aic3x-codec 1-0018: asoc: failed to add kcontrol Left Line1L Mux

asoc: tlv320aic3x-hifi <-> imx-ssi.1 mapping ok

Initialize HDMI-audio failed. Load HDMI-video first!

ALSA device list:

  #0: imx_tlv320aic3007-audio

oprofile: using arm/armv7-ca9

GACT probability NOT on

Mirror/redirect action on

u32 classifier

    Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (13234 buckets, 52936 max)

ctnetlink v0.93: registering with nfnetlink.

NF_TPROXY: Transparent proxy support initialized, version 4.1.0

NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.

xt_time: kernel timezone is -0000

IPv4 over IPv4 tunneling driver

GRE over IPv4 demultiplexor driver

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

TCP cubic registered

NET: Registered protocol family 10

Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

mmc0: new SD card at address e624

NET: Registered protocol family 15

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

mmcblk0: mmc0:e624 SU02G 1.84 GiB

mmcblk0: p1 p2 p3

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

L2TP core driver, V2.0

PPPoL2TP kernel driver, V2.0

L2TP IP encapsulation support (L2TPv3)

L2TP netlink interface

L2TP ethernet pseudowire support (L2TPv3)

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

usb 2-1: New USB device found, idVendor=0451, idProduct=8042

usb 2-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0

hub 2-1:1.0: USB hub found

hub 2-1:1.0: 4 ports detected

DVFS driver module loaded

regulator_init_complete: VDD_MX6_HIGH: incomplete constraints, leaving on

regulator_init_complete: VDD_SD1: incomplete constraints, leaving on

regulator_init_complete: VDD_SD0: incomplete constraints, leaving on

regulator_init_complete: VDD_3V3_PMIC_IO: incomplete constraints, leaving on

regulator_init_complete: VDD_MX6_SNVS: incomplete constraints, leaving on

regulator_init_complete: VDD_ETH_IO: incomplete constraints, leaving on

regulator_init_complete: VDD_ETH: incomplete constraints, leaving on

regulator_init_complete: VDD_3V3: incomplete constraints, leaving on

regulator_init_complete: VDD_DDR3: incomplete constraints, leaving on

regulator_init_complete: VDDSOC: incomplete constraints, leaving on

regulator_init_complete: VDDCORE: incomplete constraints, leaving on

regulator_init_complete: DRVDD: incomplete constraints, leaving on

regulator_init_complete: AVDD: incomplete constraints, leaving on

regulator_init_complete: DVDD: incomplete constraints, leaving on

regulator_init_complete: IOVDD: incomplete constraints, leaving on

da9063-rtc da9063-rtc: setting system clock to 2000-01-01 00:01:34 UTC (946684894)

EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

VFS: Mounted root (ext4 filesystem) on device 179:2.

devtmpfs: mounted

Freeing init memory: 252K

init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.

init: cannot open '/initlogo.rle'

EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)

init: Unable to open persistent property directory /data/property errno: 2

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'

android_usb: already disabled

android_usb: already disabled

mtp_bind_config

root@android:/ # request_suspend_state: wakeup (3->0) at 8290682004 (2000-01-01 00:01:39.585311336 UTC)

init: untracked pid 2494 exited

request_suspend_state: wakeup (0->0) at 8890367671 (2000-01-01 00:01:40.184997336 UTC)

init: untracked pid 2543 exited

root@android:/ #

root@android:/ #

root@android:/ #

root@android:/ #

root@android:/ #

root@android:/ # lrequest_suspend_state: wakeup (0->0) at 14500371003 (2000-01-01 00:01:45.795000669 UTC)

init: untracked pid 2551 exited

root@android:/ # logcat                                                      

--------- beginning of /dev/log/main

I/installd( 2495): installd firing up

E/cutils  ( 2495): Failed to read /data/.layout_version: No such file or directory

E/installd( 2495): Could not create directories; exiting.

--------- beginning of /dev/log/system

I/Vold    ( 2489): Vold 2.1 (the revenge) firing up

D/Vold    ( 2489): Volume udisk state changing -1 (Initializing) -> 0 (No-Media)

D/Vold    ( 2489): Volume extsd state changing -1 (Initializing) -> 0 (No-Media)

D/Vold    ( 2489): Volume sdcard state changing -1 (Initializing) -> 0 (No-Media)

D/Vold    ( 2489): Volume sdcard state changing 0 (No-Media) -> 2 (Pending)

D/Vold    ( 2489): Volume sdcard state changing 2 (Pending) -> 1 (Idle-Unmounted)

I/SurfaceFlinger( 2491): SurfaceFlinger is starting

I/SurfaceFlinger( 2491): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...

D/libEGL  ( 2491): loaded /system/lib/egl/libEGL_VIVANTE.so

D/libEGL  ( 2491): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so

D/libEGL  ( 2491): loaded /system/lib/egl/libGLESv2_VIVANTE.so

W/imx6.gralloc( 2491): using (fd=15)

W/imx6.gralloc( 2491): id           = DISP3 BG

W/imx6.gralloc( 2491): xres         = 800 px

W/imx6.gralloc( 2491): yres         = 480 px

W/imx6.gralloc( 2491): xres_virtual = 800 px

W/imx6.gralloc( 2491): yres_virtual = 1536 px

W/imx6.gralloc( 2491): bpp          = 16

W/imx6.gralloc( 2491): r            = 11:5

W/imx6.gralloc( 2491): g            =  5:6

W/imx6.gralloc( 2491): b            =  0:5

W/imx6.gralloc( 2491): width        = 127 mm (160.000000 dpi)

W/imx6.gralloc( 2491): height       = 76 mm (160.421051 dpi)

W/imx6.gralloc( 2491): refresh rate = 35.70 Hz

I/FslHwcomposer( 2491): fb0 is ldb

I/FslHwcomposer( 2491):  device

I/FslHwcomposer( 2491): fb1 is overlay device

W/FslHwcomposer( 2491): open /sys/class/graphics/fb2 failed

W/FslHwcomposer( 2491): open /sys/class/graphics/fb3 failed

W/FslHwcomposer( 2491): open /sys/class/graphics/fb4 failed

W/FslHwcomposer( 2491): open /sys/class/graphics/fb5 failed

I/FslHwcomposer( 2491): hwcomposer: open framebuffer fb0

I/v_hwc   ( 2491): Detected display /dev/graphics/fb0

I/v_hwc   ( 2491): xres         = 800 px

I/v_hwc   ( 2491): yres         = 480 px

I/v_hwc   ( 2491): xres_virtual = 800 px

I/v_hwc   ( 2491): yres_virtual = 1536 px

I/v_hwc   ( 2491): width        = -1 mm (0.0 dpi)

I/v_hwc   ( 2491): height       = -1 mm (0.0 dpi)

I/v_hwc   ( 2491): refresh rate = 35.0 Hz

E/v_hwc   ( 2491): open /dev/graphics/fb0 failed

I/v_hwc   ( 2491): Vivante HWComposer v2.4

I/v_hwc   ( 2491): Device:               0x40039008

I/v_hwc   ( 2491): Separated 2D:         YES

I/v_hwc   ( 2491): 2D PE20:              YES

I/v_hwc   ( 2491): Multi-source blit:    NO

I/v_hwc   ( 2491): Multi-source blit Ex: NO

I/v_hwc   ( 2491): OPF/YUV blit/Tiling : NO

I/v_hwc   ( 2491): Filter stretch      : NO

I/FslHwcomposer( 2491): hwc_device_open,367

I/SurfaceFlinger( 2491): Using composer version 1.1

W/SurfaceFlinger( 2491): no suitable EGLConfig found, trying without EGL_FRAMEBUFFER_TARGET_ANDROID

E/Trace   ( 2491): error opening trace file: No such file or directory (2)

E/SurfaceFlinger( 2491): HWComposer: framebufferTarget is null

E/SurfaceFlinger( 2491): HWComposer: framebufferTarget is null

E/SurfaceFlinger( 2491): HWComposer: framebufferTarget is null

E/SurfaceFlinger( 2491): HWComposer: framebufferTarget is null

I/SurfaceFlinger( 2491): EGL informations:

I/SurfaceFlinger( 2491): vendor    : Android

I/SurfaceFlinger( 2491): version   : 1.4 Android META-EGL

I/SurfaceFlinger( 2491): extensions: EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_renderbuffer_image EGL_KHR_fence_sync EGL

_ANDROID_image_native_buffer

I/SurfaceFlinger( 2491): Client API: OpenGL_ES

I/SurfaceFlinger( 2491): EGLSurface: 8-8-8-8, config=0x4b7d5138

I/SurfaceFlinger( 2491): OpenGL ES informations:

I/SurfaceFlinger( 2491): vendor    : Vivante Corporation

I/SurfaceFlinger( 2491): renderer  : GC2000 Graphics Engine

I/SurfaceFlinger( 2491): version   : OpenGL ES-CM 1.1

I/SurfaceFlinger( 2491): extensions: GL_EXT_debug_marker GL_OES_blend_equation_separate GL_OES_blend_func_separate GL_OES_blend_subtract GL_OES_byte_coordinates GL_OES_com

pressed_ETC1_RGB8_texture GL_OES_compressed_paletted_texture GL_OES_draw_texture GL_OES_extended_matrix_palette GL_OES_fixed_point GL_OES_framebuffer_object GL_OES_matrix_

get GL_OES_matrix_palette GL_OES_point_size_array GL_OES_point_sprite GL_OES_query_matrix GL_OES_read_format GL_OES_single_precision GL_OES_stencil_wrap GL_OES_texture_cub

e_map GL_OES_texture_mirrored_repeat GL_OES_EGL_image GL_OES_depth24 GL_OES_element_index_uint GL_OES_fbo_render_mipmap GL_OES_mapbuffer GL_OES_rgb8_rgba8 GL_OES_stencil1

GL_OES_stencil4 GL_OES_stencil8 GL_OES_texture_npot GL_OES_vertex_half_float GL_OES_packed_depth_stencil GL_EXT_texture_format_BGRA8888 GL_IMG_read_format GL_IMG_user_clip

_plane GL_APPLE_texture_2D_limited_npot GL_EXT_texture_lod_bias GL_EXT_blend_minmax GL_EXT_read_format_bgra GL_EXT_multi_draw_arrays GL_OES_EGL_sync GL_APPLE_texture_forma

t_BGRA8888 GL_APPLE_te

I/SurfaceFlinger( 2491): GL_MAX_TEXTURE_SIZE = 8192

I/SurfaceFlinger( 2491): GL_MAX_VIEWPORT_DIMS = 8192 x 8192

D/AndroidRuntime( 2492):

D/AndroidRuntime( 2492): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime( 2492): CheckJNI is OFF

I/AndroidRuntime( 2492): JNI options: '-Xjniopts:warnonly'

D/SurfaceFlinger( 2491): Screen acquired, type=0 flinger=0x404f0318

D/libEGL  ( 2531): loaded /system/lib/egl/libEGL_VIVANTE.so

D/libEGL  ( 2531): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so

D/libEGL  ( 2531): loaded /system/lib/egl/libGLESv2_VIVANTE.so

E/Trace   ( 2531): error opening trace file: No such file or directory (2)

E/BufferQueue( 2491): [BootAnimation] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

I/mediaserver( 2494): ServiceManager: 0x40a56ef8

I/AudioFlinger( 2494): Using default 3000 mSec as standby time.

I/CameraService( 2494): CameraService started (pid=2494)

I/v_hwc   ( 2491): Display(0x4010c008) detected: format=306 800x480

I/v_hwc   ( 2491): Display buffer(0x40050de0) detected: physical=0x2f800000

I/v_hwc   ( 2491): Display buffer(0x40050e08) detected: physical=0x2f8bb800

I/FslCameraHAL( 2494): Face Back Camera is ov5642, orient is 0

I/FslCameraHAL( 2494): Face Front Camera is 0, orient is 0

I/FslCameraHAL( 2494): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path

I/v_hwc   ( 2491): Display buffer(0x400d57a8) detected: physical=0x2f977000

I/AudioPolicyManagerBase( 2494): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf

W/audio_hw_primary( 2494): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio

W/audio_hw_primary( 2494): out rate 44100

W/audio_hw_primary( 2494): in rate 44100, channels 1 format 0

I/AudioFlinger( 2494): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 2494): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2

W/audio_hw_primary( 2494): opened out stream...1086925552

I/AudioFlinger( 2494): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 2494): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 2494): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

D/dalvikvm( 2492): Trying to load lib libjavacore.so 0x0

D/dalvikvm( 2492): Added shared lib libjavacore.so 0x0

D/dalvikvm( 2492): Trying to load lib libnativehelper.so 0x0

D/dalvikvm( 2492): Added shared lib libnativehelper.so 0x0

I/SamplingProfilerIntegration( 2492): Profiling disabled.

I/Zygote  ( 2492): Preloading classes...

D/dalvikvm( 2492): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 1ms+0ms, total 3ms

W/Environment( 2492): EXTERNAL_STORAGE undefined; falling back to default

W/dalvikvm( 2492): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;

D/AndroidRuntime( 2492): Shutting down VM

W/dalvikvm( 2492): threadid=1: thread exiting with uncaught exception (group=0x4143c930)

I/installd( 2542): installd firing up

E/cutils  ( 2542): Failed to read /data/.layout_version: No such file or directory

E/installd( 2542): Could not create directories; exiting.

I/ServiceManager( 2488): service 'media.camera' died

I/ServiceManager( 2488): service 'media.audio_flinger' died

I/ServiceManager( 2488): service 'media.player' died

D/AndroidRuntime( 2544):

D/AndroidRuntime( 2544): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime( 2544): CheckJNI is OFF

I/AndroidRuntime( 2544): JNI options: '-Xjniopts:warnonly'

D/dalvikvm( 2544): Trying to load lib libjavacore.so 0x0

D/dalvikvm( 2544): Added shared lib libjavacore.so 0x0

D/dalvikvm( 2544): Trying to load lib libnativehelper.so 0x0

D/dalvikvm( 2544): Added shared lib libnativehelper.so 0x0

I/mediaserver( 2543): ServiceManager: 0x40a68ef8

I/AudioFlinger( 2543): Using default 3000 mSec as standby time.

I/CameraService( 2543): CameraService started (pid=2543)

I/FslCameraHAL( 2543): Face Back Camera is ov5642, orient is 0

I/FslCameraHAL( 2543): Face Front Camera is 0, orient is 0

I/FslCameraHAL( 2543): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path

I/AudioPolicyManagerBase( 2543): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf

W/audio_hw_primary( 2543): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio

W/audio_hw_primary( 2543): out rate 44100

W/audio_hw_primary( 2543): in rate 44100, channels 1 format 0

I/AudioFlinger( 2543): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 2543): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2

W/audio_hw_primary( 2543): opened out stream...1086774000

I/AudioFlinger( 2543): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 2543): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 2543): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

I/SamplingProfilerIntegration( 2544): Profiling disabled.

I/Zygote  ( 2544): Preloading classes...

D/dalvikvm( 2544): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 1ms+0ms, total 3ms

W/Environment( 2544): EXTERNAL_STORAGE undefined; falling back to default

W/dalvikvm( 2544): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;

D/AndroidRuntime( 2544): Shutting down VM

W/dalvikvm( 2544): threadid=1: thread exiting with uncaught exception (group=0x40b1a930)

I/ServiceManager( 2488): service 'media.camera' died

I/ServiceManager( 2488): service 'media.audio_flinger' died

I/ServiceManager( 2488): service 'media.player' died

I/mediaserver( 2551): ServiceManager: 0x41f7b000

I/AudioFlinger( 2551): Using default 3000 mSec as standby time.

I/CameraService( 2551): CameraService started (pid=2551)

I/FslCameraHAL( 2551): Face Back Camera is ov5642, orient is 0

I/FslCameraHAL( 2551): Face Front Camera is 0, orient is 0

I/FslCameraHAL( 2551): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path

I/AudioPolicyManagerBase( 2551): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf

W/audio_hw_primary( 2551): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio

W/audio_hw_primary( 2551): out rate 44100

W/audio_hw_primary( 2551): in rate 44100, channels 1 format 0

I/AudioFlinger( 2551): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 2551): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2

W/audio_hw_primary( 2551): opened out stream...1106785632

I/AudioFlinger( 2551): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 2551): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 2551): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

I/installd( 2562): installd firing up

E/cutils  ( 2562): Failed to read /data/.layout_version: No such file or directory

E/installd( 2562): Could not create directories; exiting.

D/AndroidRuntime( 2561):

D/AndroidRuntime( 2561): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime( 2561): CheckJNI is OFF

I/AndroidRuntime( 2561): JNI options: '-Xjniopts:warnonly'

D/dalvikvm( 2561): Trying to load lib libjavacore.so 0x0

D/dalvikvm( 2561): Added shared lib libjavacore.so 0x0

D/dalvikvm( 2561): Trying to load lib libnativehelper.so 0x0

D/dalvikvm( 2561): Added shared lib libnativehelper.so 0x0

I/SamplingProfilerIntegration( 2561): Profiling disabled.

I/Zygote  ( 2561): Preloading classes...

D/dalvikvm( 2561): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 0ms+1ms, total 3ms

W/Environment( 2561): EXTERNAL_STORAGE undefined; falling back to default

W/dalvikvm( 2561): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;

D/AndroidRuntime( 2561): Shutting down VM

W/dalvikvm( 2561): threadid=1: thread exiting with uncaught exception (group=0x4200b930)

I/ServiceManager( 2488): service 'media.audio_flinger' died

I/ServiceManager( 2488): service 'media.player' died

I/ServiceManager( 2488): service 'media.camera' died

I/mediaserver( 2566): ServiceManager: 0x417df000

I/AudioFlinger( 2566): Using default 3000 mSec as standby time.

I/CameraService( 2566): CameraService started (pid=2566)

I/FslCameraHAL( 2566): Face Back Camera is ov5642, orient is 0

I/FslCameraHAL( 2566): Face Front Camera is 0, orient is 0

I/FslCameraHAL( 2566): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path

I/AudioPolicyManagerBase( 2566): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf

W/audio_hw_primary( 2566): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio

W/audio_hw_primary( 2566): out rate 44100

W/audio_hw_primary( 2566): in rate 44100, channels 1 format 0

I/AudioFlinger( 2566): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 2566): open output stream drequest_suspend_state: wakeup (0->0) at 19200353004 (2000-01-01 00:01:50.494982670 UTC)

evices 2, format 1, channels 3, sinit: untracked pid 2566 exited

ample_rate 48000, flag 2

W/audio_hw_primary( 2566): opened out stream...1098806624

I/AudioFlinger( 2566): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 2566): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 2566): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

I/v_hwc   ( 2491): vsync thread exit: callback procs not registered.

I/installd( 2572): installd firing up

E/cutils  ( 2572): Failed to read /data/.layout_version: No such file or directory

E/installd( 2572): Could not create directories; exiting.

D/AndroidRuntime( 2571):

D/AndroidRuntime( 2571): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime( 2571): CheckJNI is OFF

I/AndroidRuntime( 2571): JNI options: '-Xjniopts:warnonly'

D/dalvikvm( 2571): Trying to load lib libjavacore.so 0x0

D/dalvikvm( 2571): Added shared lib libjavacore.so 0x0

D/dalvikvm( 2571): Trying to load lib libnativehelper.so 0x0

D/dalvikvm( 2571): Added shared lib libnativehelper.so 0x0

I/SamplingProfilerIntegration( 2571): Profiling disabled.

I/Zygote  ( 2571): Preloading classes...

D/dalvikvm( 2571): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 0ms+0ms, total 2ms

W/Environment( 2571): EXTERNAL_STORAGE undefined; falling back to default

W/dalvikvm( 2571): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;

D/AndroidRuntime( 2571): Shutting down VM

W/dalvikvm( 2571): threadid=1: thread exiting with uncaught exception (group=0x412e5930)

I/ServiceManager( 2488): service 'media.audio_flinger' died

I/ServiceManager( 2488): service 'media.player' died

I/ServiceManager( 2488): service 'media.camera' died

I/mediaserver( 2576): ServiceManager: 0x41724000

I/AudioFlinger( 2576): Using default 3000 mSec as standby time.

I/CameraService( 2576): CameraService started (pid=2576)

I/FslCameraHAL( 2576): Face Back Camera is ov5642, orient is 0

I/FslCameraHAL( 2576): Face Front Camera is 0, orient is 0

I/FslCameraHAL( 2576): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path

I/AudioPolicyManagerBase( 2576): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf

W/audio_hw_primary( 2576): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio

W/audio_hw_primary( 2576): out rate 44100

W/audio_hw_primary( 2576): in rate 44100, channels 1 format 0

I/AudioFlinger( 2576): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 2576): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2

W/audio_hw_primary( 2576): opened out stream...1098040672

I/AudioFlinger( 2576): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 2576): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 2576): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

I/installd( 2581): installd firing up

E/cutils  ( 2581): Failed to read /data/.layout_version: No such file or directory

E/installd( 2581): Could not create directories; exiting.

D/AndroidRuntime( 2580):

D/AndroidRuntime( 2580): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime( 2580): CheckJNI is OFF

I/AndroidRuntime( 2580): JNI options: '-Xjniopts:warnonly'

D/dalvikvm( 2580): Trying to load lib libjavacore.so 0x0

D/dalvikvm( 2580): Added shared lib libjavacore.so 0x0

D/dalvikvm( 2580): Trying to load lib libnativehelper.so 0x0

D/dalvikvm( 2580): Added shared lib libnativehelper.so 0x0

I/SamplingProfilerIntegration( 2580): Profiling disabled.

I/Zygote  ( 2580): Preloading classes...

D/dalvikvm( 2580): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 0ms+0ms, total 3ms

W/Environment( 2580): EXTERNAL_STORAGE undefined; falling back to default

W/dalvikvm( 2580): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;

D/AndroidRuntime( 2580): Shutting down VM

W/dalvikvm( 2580): threadid=1: thread exiting with uncaught exception (group=0x40e62930)

request_suspend_state: wakeup (0->0) at 23810412672 (2000-01-01 00:01:55.105042004 UTC)

I/ServiceManager( 2488): service init: untracked pid 2576 exited

'media.audio_flinger' died

I/ServiceManager( 2488): service 'media.player' died

I/ServiceManager( 2488): service 'media.camera' died

I/mediaserver( 2585): ServiceManager: 0x40bcdfb0

I/AudioFlinger( 2585): Using default 3000 mSec as standby time.

I/CameraService( 2585): CameraService started (pid=2585)

I/FslCameraHAL( 2585): Face Back Camera is ov5642, orient is 0

I/FslCameraHAL( 2585): Face Front Camera is 0, orient is 0

I/FslCameraHAL( 2585): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path

I/AudioPolicyManagerBase( 2585): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf

W/audio_hw_primary( 2585): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio

W/audio_hw_primary( 2585): out rate 44100

W/audio_hw_primary( 2585): in rate 44100, channels 1 format 0

I/AudioFlinger( 2585): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 2585): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2

W/audio_hw_primary( 2585): opened out stream...1074431624

I/AudioFlinger( 2585): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 2585): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 2585): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

I/installd( 2590): installd firing up

E/cutils  ( 2590): Failed to read /data/.layout_version: No such file or directory

E/installd( 2590): Could not create directories; exiting.

D/AndroidRuntime( 2589):

D/AndroidRuntime( 2589): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime( 2589): CheckJNI is OFF

I/AndroidRuntime( 2589): JNI options: '-Xjniopts:warnonly'

D/dalvikvm( 2589): Trying to load lib libjavacore.so 0x0

D/dalvikvm( 2589): Added shared lib libjavacore.so 0x0

D/dalvikvm( 2589): Trying to load lib libnativehelper.so 0x0

D/dalvikvm( 2589): Added shared lib libnativehelper.so 0x0

I/SamplingProfilerIntegration( 2589): Profiling disabled.

I/Zygote  ( 2589): Preloading classes...

D/dalvikvm( 2589): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 0ms+1ms, total 3ms

W/Environment( 2589): EXTERNAL_STORAGE undefined; falling back to default

W/dalvikvm( 2589): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;

D/AndroidRuntime( 2589): Shutting down VM

W/dalvikvm( 2589): threadid=1: thread exiting with uncaught exception (group=0x40ef1930)

request_suspend_state: wakeup (0->0) at 29440367339 (2000-01-01 00:02:00.734997005 UTC)

init: untracked pid 2585 exited

I/ServiceManager( 2488): service 'media.audio_flinger' died

I/ServiceManager( 2488): service 'media.player' died

I/ServiceManager( 2488): service 'media.camera' died

I/mediaserver( 2594): ServiceManager: 0x40b80fb0

I/AudioFlinger( 2594): Using default 3000 mSec as standby time.

I/CameraService( 2594): CameraService started (pid=2594)

I/FslCameraHAL( 2594): Face Back Camera is ov5642, orient is 0

I/FslCameraHAL( 2594): Face Front Camera is 0, orient is 0

I/FslCameraHAL( 2594): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path

I/AudioPolicyManagerBase( 2594): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf

W/audio_hw_primary( 2594): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio

W/audio_hw_primary( 2594): out rate 44100

W/audio_hw_primary( 2594): in rate 44100, channels 1 format 0

I/AudioFlinger( 2594): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 2594): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2

W/audio_hw_primary( 2594): opened out stream...1074105088

I/AudioFlinger( 2594): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 2594): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 2594): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

The above issue is resolved now i'm able to get the home screen, but the display is divided in to 2, the actual left half shifted to right and actual right half shifted to left. and even the display color changed to dark yellow and the image latency is too low. I'll update with the images(screenshots) soon.

This document was generated from the following discussion: help in porting Android Jb to imx6q custom board

Comments

\\E/v_hwc   ( 2491): open /dev/graphics/fb0 failed


Check permissions in ueventd.rc

What should the permissions be? I have the following:

ueventd.freescale.rc:/dev/graphics/fb0         0660   system     graphics

ueventd.freescale.rc:/sys/devices/platform/mxc_sdc_fb.0/graphics/fb* fsl_disp_property 0660 system graphics

ueventd.freescale.rc:/sys/devices/platform/mxc_sdc_fb.1/graphics/fb* fsl_disp_property 0660 system graphics

ueventd.freescale.rc:/sys/devices/platform/mxc_sdc_fb.0/graphics/fb* mode 0660 system graphics

ueventd.freescale.rc:/sys/devices/platform/mxc_sdc_fb.1/graphics/fb* mode 0660 system graphics

You need a SDcard. Debug.java is trying to create a trace file on it and can't open the sdcard path. Follow this guide and it'll be fine:  Typical Configuration Examples | Android Developers

No ratings
Version history
Last update:
‎07-30-2013 06:26 PM
Updated by: