Using i.MX283 as smart server for home automation

cancel
Showing results for 
Search instead for 
Did you mean: 

Using i.MX283 as smart server for home automation

No ratings

Using i.MX283 as smart server for home automation

Hi,


this is a smart server called Duckbill in a thumb-drive format based on the i.MX283. It's a really low cost solution usable with or without casing.

It is intended to be set up as a small home-server for automation purposes. It comes with Debian Linux as operation system but without any specific user programs. 

The stick can be operated either at a USB power adaptor or at a USB port of your router. 

Since Duckbill runs Linux you are totally free in software development.


The internal connectors can be used as UART, SPI, I2C, ADC or GPIO. So it's up to everyone to develop his own expansion board.


Duckbill_Board_Top_n.gif

1. Duckbill without casing (top)

Duckbill_Board_Bottom_n.gif

2. Duckbill without casing (bottom)


Duckbill_n.gif

3. Duckbill with casing


Duckbill_Pins_Gehaeuse_n.gif

4. Duckbill for development purposes


Duckbill_EnOcean_offen_n.gif

5. Duckbill with integrated EnOcean module


If you want to know more about this product:

http://www.i2se.com/homeautomation.html

Version history
Last update:
‎07-25-2014 01:46 AM
Updated by: