The following document contains a list of document, questions and discussions that are relevant in the community based on amount of views. If you are having a problem, doubt or getting started in i.MX processors, you should check the following links to see if your doubt is in there.
Freescale Yocto Project main page
i.MX Yocto Project: Frequently Asked Questions
Yocto Project Package Management - smart
How to add a new layer and a new recipe in Yocto
Setting up the Eclipse IDE for Yocto Application Development
Yocto with a package manager (ex: apt-get)
Yocto Setting the Default Ethernet address and disable DHCP on boot.
i.MX6/7 DDR Stress Test Tool V3.00
Installing Ubuntu Rootfs on NXP i.MX6 boards
iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP
i.MX6 GStreamer-imx Plugins - Tutorial & Example Pipelines
Streaming USB Webcam over Network
Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53
Copying Files Between Windows and Linux using PuTTY
load kernel from SD card in U-boot
Changing the Kernel configuration for i.MX6 SABRE
What is inside the init.rc and what is it used for.