Question:
Can i.MX6S?DL supports 128GB?
The descriptions regarding SDXC is in the datasheet or RM such as boot chapter, but card capacity descriptions regarding SDXC could not be found.
There is description for SDHC in datasheet Table 2. Fully compliant with SD command/response sets and Physical Layer as defined in the SD Memory Card
Specifications, v3.0 including high-capacity SDHC cards up to 32 GB.
Answer:
Please find attached spec, SDXC can support up to 2TB. And i.Mx6SDL doc show it support SDXC. So no problem using i.Mx6SDL to support SDXC. Please refer to attachd.