Porting KSZ9031on the imx7DPorting KSZ9031on the imx7D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting KSZ9031on the imx7DPorting KSZ9031on the imx7D

Porting KSZ9031on the imx7DPorting KSZ9031on the imx7D

This document simply introduce how to change uboot for porting new PHY on imx7D customized board

 

Background:

Current imx7D Sabresd board uses BCM54220B0KFBG PHY, the customized board wants to use KSZ9031 as PHY on the yocto 4.9.88 version, the customized board uses only one ethernet port on ENET2 port according to the imx7D Sabresd board

 

Requirement:

Refer to the yocto user guide of 4.9.88 version, built your own image, for simple, you can built core-image-minimal, and download the 4.9.88 mfgtool to program

  •        The document of 4.9.88:

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS

  •        mfgtool for downloading:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX6_L4.9.88_2.0.0_MFG_TOOL&appType=file...

  •        Design files:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=iMX7D-SABRE-DESIGNFILES&appType=file1&DO...

 

 

adding customized code in u-boot head file

refer to the customized board schematic as below:

 pastedImage_3.png

 

This board use eth2 as ethernet port, the code mx7dsabresd.h(path: yocto-L4.9.88_2.0/build-x11/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git/include/configs)

/* Network */

#ifdef CONFIG_DM_ETH

#define CONFIG_FEC_MXC

#define CONFIG_MII

#define CONFIG_FEC_XCV_TYPE             RGMII

#define CONFIG_FEC_ENET_DEV       0

 

#define CONFIG_PHYLIB

#define CONFIG_PHY_BROADCOM

/* ENET1 */

#if (CONFIG_FEC_ENET_DEV == 0)

#define IMX_FEC_BASE              ENET_IPS_BASE_ADDR

#define CONFIG_FEC_MXC_PHYADDR          0x0

#ifdef CONFIG_DM_ETH

#define CONFIG_ETHPRIME                 "eth0"

#else

#define CONFIG_ETHPRIME                 "FEC0"

#endif

#elif (CONFIG_FEC_ENET_DEV == 1)

#define IMX_FEC_BASE              ENET2_IPS_BASE_ADDR

#define CONFIG_FEC_MXC_PHYADDR          0x1

#ifdef CONFIG_DM_ETH

#define CONFIG_ETHPRIME                 "eth1"

#else

#define CONFIG_ETHPRIME                 "FEC1"

#endif

#endif

 

 

Change the source code as below, add two macro definition and change the PHY address according to the schematic:

/* Network */

#define CONFIG_PHY_MICREL

#define CONFIG_PHY_MICREL_KSZ9031

 

#ifdef CONFIG_DM_ETH

#define CONFIG_FEC_MXC

#define CONFIG_MII

#define CONFIG_FEC_XCV_TYPE             RGMII

 

#define CONFIG_FEC_ENET_DEV       0

 

 

#define CONFIG_PHYLIB

#define CONFIG_PHY_BROADCOM

/* ENET1 */

#if (CONFIG_FEC_ENET_DEV == 0)

#define IMX_FEC_BASE              ENET_IPS_BASE_ADDR

#define CONFIG_FEC_MXC_PHYADDR          0x1

#ifdef CONFIG_DM_ETH

#define CONFIG_ETHPRIME                 "eth0"

#else

#define CONFIG_ETHPRIME                 "FEC0"

#endif

#elif (CONFIG_FEC_ENET_DEV == 1)

#define IMX_FEC_BASE              ENET2_IPS_BASE_ADDR

#define CONFIG_FEC_MXC_PHYADDR          0x2

 

#ifdef CONFIG_DM_ETH

#define CONFIG_ETHPRIME                 "eth1"

#else

#define CONFIG_ETHPRIME                 "FEC1"

#endif

#endif

 

 

 

adding customized code in u-boot source file

the source code named mx7dsabresd.c (path: yocto-L4.9.88_2.0/build-x11/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git/board/freescale/mx7dsabresd)

 

  1.       Don’t forget include the micrel.h file
  2.        Focus on the setup_fec fuction

pastedImage_4.png 

Imx7d Sabresd board uses gpio_spi 5 as reset pin so the source code as below:

ret = gpio_lookup_name("gpio_spi@0_5", NULL, NULL, &gpio)

               if (ret) {

              printf("GPIO: 'gpio_spi@0_5' not found\n");

 

 pastedImage_5.png

The customized board uses GPIO1_IO03 as reset pin, so the source code was changed to :

imx_iomux_v3_setup_pad(MX7D_PAD_GPIO1_IO03__GPIO1_IO3 | MUX_PAD_CTRL(NO_PAD_CTRL));

ret = gpio_request(IMX_GPIO_NR(1, 3), "enet_phy_rst");

gpio_direction_output(IMX_GPIO_NR(1, 3), 0);

       mdelay(20);

       gpio_direction_output(IMX_GPIO_NR(1, 3), 1);

      udelay(100);

 

  1.       Focus on the function board_phy_config fuction

Use this function to set the phy rx, tx data pad skew and clock pad skew, for ksz9031, can refer to the UDOO board, then change the setting source code as below:

/* control data pad skew - devaddr = 0x02, register = 0x04 */

       ksz9031_phy_extended_write(phydev, 0x02,

                               MII_KSZ9031_EXT_RGMII_CTRL_SIG_SKEW,

                               MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x0000);

       /* rx data pad skew - devaddr = 0x02, register = 0x05 */

       ksz9031_phy_extended_write(phydev, 0x02,

                               MII_KSZ9031_EXT_RGMII_RX_DATA_SKEW,

                               MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x0000);

       /* tx data pad skew - devaddr = 0x02, register = 0x05 */

       ksz9031_phy_extended_write(phydev, 0x02,

                               MII_KSZ9031_EXT_RGMII_TX_DATA_SKEW,

                               MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x0000);

       /* gtx and rx clock pad skew - devaddr = 0x02, register = 0x08 */

       ksz9031_phy_extended_write(phydev, 0x02,

                               MII_KSZ9031_EXT_RGMII_CLOCK_SKEW,

                               MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x03FF);

  1.       Build the uboot source code then program to the customized board, the log file as below:

U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (Apr 20 2019 - 17:51:51 +0800)

 

CPU:   Freescale i.MX7D rev1.3 996 MHz (running at 792 MHz)

CPU:   Commercial temperature grade (0C to 95C) at 32C

Reset cause: POR

Model: Freescale i.MX7D SabreSD Board

Board: i.MX7D SABRESD RevC in secure mode

DRAM:  1 GiB

PMIC: PFUZE3000 DEV_ID=0x30 REV_ID=0x11

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

Display: TFT43AB (480x272)

Video: 480x272x24

In:    serial

Out:   serial

Err:   serial

switch to partitions #0, OK

mmc1(part 0) is current device

Net:  

Error: ethernet@30bf0000 address not set.

eth0: ethernet@30be0000

Error: ethernet@30bf0000 address not set.

 

Ending

Don’t worry about this error message, because you don’t set correct mac address, one has two option to set this,

For one, you can add mac address in the uboot manually, like

setenv ethaddr 00:11:22:33:44:55

    another option is add CONFIG_NET_RANDOM_ETHADDR=y in the configure file, then you don’t need to set mac address manually, would get a random mac address

 

this document just simply introduce how to change the source code in the u-boot, you also need to change the kernel dts file and kernel file to support the new PHY, the kernel has the same process, the phy address, the phy settings, and the gpio pins, hope this document give you some hints to port the new PHY

評価なし
バージョン履歴
最終更新日:
‎06-29-2019 11:45 PM
更新者: