The purpose of this article is to describe how to join together the Processor
Expert and ARM GCC toolchain under Eclipse environment.  
  Freescale provides the Processor Expert, which contains the Pin Settings Tool 
 to support an easy way to configure pin signals, from multiplexing to the electrical 
 properties of pins. With such Tool all the pins can be configured with a graphical 
 user interface, and then generate C code, in order to use it as an example in applications.
 Please refer to the following Web for more details.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PROCESSOR-EXPERT-IMX
 
  The Processor Expert Software for i.MX Processors (Version 1.0) does not include 
a compiler or linker. Customers should merge the generated code into a build system. 
  However, it is possible to use common Eclipse-based IDE for the Processor Expert (V 1.0) 
and GNU ARM “C” toolchains. In particular, the following sequence may be implemented for
both Linux and Windows hosts.
 
 1.
 Install Eclipse (Kepler release) IDE for C/C++ Developers.
 
 https://eclipse.org/downloads/packages/eclipse-ide-cc-developers/keplersr2
 
 2.
 Add Eclipse Processor Expert plug-in, as recommended in the documentation.
 
 http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PROCESSOR-EXPERT-IMX
 
 https://community.freescale.com/docs/DOC-101470
 
 3.  
 Add GNU ARM Eclipse, which contains configurations for different toolchains, 
including Linux ones.
 
 http://gnuarmeclipse.livius.net/blog/plugins-install/
 
4.
Install appropriate toolchain. For bare-metal applications Sourcery CodeBench Lite
for ARM is sutable one.
 
Sourcery CodeBench Lite Edition including ARM GCC IDE - Mentor Graphics
 
Please use Getting Started Guide document from the CodeBench Lite package,
that explains how to install and build applications with the CodeBench Lite.
    As an example, let’s consider minimal startup code for i.MX6Q (LED flickering 
project on i.MX6Q SDB / SDP). Assuming Eclipse IDE with the Processor Expert
and GNU ARM tools is installed, we should create new “C” project under Eclipse :
New -> C Project. Select “Empty Project” and “Cross ARM GCC”, enter “Project
 name”.  
 
 Then : select “Advanced settings” -> C/C++ Build -> Settings
 
 
 
  
Tab “Target Processor” :
 ARM Family : cortex – a9
 Architecture : armv7-a
 Instruction set : ARM (-marm)
 Endianness : Little endian (-mlittle-endian)
 FloatABI : Library with FP (softfp)
 FPU Type : neon
 Unaligned access : Disabled (-mno-unaligned-access)
 
 
“Cross ARM GNU Create Flash Image” :
 General : Raw binary.
 
 
 
 
 
 TAB “Toolchains” :
 Name : Sourcery CodeBench Lite for ARM EABI (arm-none-eabi-gcc)
 (If needed customers can select appropriate toolchain)
 Architecture : ARM (AArch32)
 Prefix : arm-none-eabi
 
 Check “Use global toolchain path” or select the required path directly.  
 
Source codes may added via Eclipse : File -> Import -> File System -> From directory
 
 Example source is enclosed.
 
 After sources as included in the project, let’s configure linker options via 
project properties,
 C/C++ Build -> Settings -> Tool Settings -> Cross ARM C Linker -> General.
 
Add script file “mx6dq.ld”, uncheck “Remove unused section”, check
“Do not use standard start files”.
 
  
 Note, the article of Miro Samek is very helpful in clarifying of startup code and linker
 script. Please refer to “Building Bare-Metal ARM Systems with GNU”. Article Published 
online at www.Embedded.com, July/August 2007.
So, now we can build the project : Project -> Build Project.
 Two executable file will be generated : test.elf (for JTAG debugger) and test.bin,
 which may be used to create bootable SD card, using cfimager-imx.exe utility :
 
CMD> cfimager-imx -o 0 -f test.bin -d g:
Please use readme files in the enclosed for more details.
 
 
 
 
 
 
 
 
 
 
 
 
Hi,
I have built the above program using GCC ARM GCC ARM Embedded in Launchpad . However given sample is compiled using Sourcery CodeBench Lite (which is available for evaluation period of 30 days only).
I get errors when compiled with GCC ARM. Check .jpg attached
Building target: Prog_from_Integrating.elf
Invoking: Cross ARM C Linker
arm-none-eabi-gcc --specs=rdimon.specs -lrdimon -mcpu=cortex-a9 -march=armv7-a -marm -mlittle-endian -mfloat-abi=softfp -mfpu=neon -mno-unaligned-access -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -T "E:\Kepler_Programs\Prog_from_Integrating\mx6dq.ld" -nostartfiles -Wl,-Map,"Prog_from_Integrating.map" -o "Prog_from_Integrating.elf" ./main.o
c:/program files (x86)/gnu tools arm embedded/4.9 2015q3/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: cannot find -lcs3arm
c:/program files (x86)/gnu tools arm embedded/4.9 2015q3/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: cannot find -lcs3
collect2.exe: error: ld returned 1 exit status
makefile:41: recipe for target 'Prog_from_Integrating.elf' failed
make: *** [Prog_from_Integrating.elf] Error 1
It shows cs3arm & cs3 cannot find. These are written in mx6dq.ld (linker Script) at GROUP(-lgcc -lc -lcs3arm -lcs3).
If I remove them from GROUP I get this 'Reset Handler' error.Check .jpg attached
Building target: Prog_from_Integrating.elf
Invoking: Cross ARM C Linker
arm-none-eabi-gcc --specs=rdimon.specs -lrdimon -mcpu=cortex-a9 -march=armv7-a -marm -mlittle-endian -mfloat-abi=softfp -mfpu=neon -mno-unaligned-access -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -T "E:\Kepler_Programs\Prog_from_Integrating\mx6dq.ld" -nostartfiles -Wl,-Map,"Prog_from_Integrating.map" -o "Prog_from_Integrating.elf" ./main.o
c:/program files (x86)/gnu tools arm embedded/4.9 2015q3/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: warning: cannot find entry symbol Reset_Handler; defaulting to 00900000
./main.o: In function `start_secondary_cpu':
E:\Kepler_Programs\Prog_from_Integrating\Debug/../main.c:124: undefined reference to `Reset_Handler'
E:\Kepler_Programs\Prog_from_Integrating\Debug/../main.c:124: undefined reference to `Reset_Handler'
collect2.exe: error: ld returned 1 exit status
makefile:41: recipe for target 'Prog_from_Integrating.elf' failed
make: *** [Prog_from_Integrating.elf] Error 1
Any help to solve this error would be appreciated? I want to build it using GCC ARM. (not Sourcery CodeBench)
Thanks and regards,
Sarang
The web links in the article beginning with www.freescale.com are not up to date. Where are they currently mapped to, please?
Hello,
It may be recommended to use the Pins Tool now
Pins Tool for i.MX Application Processors|NXP
Regards,
Yuri.
Hi Yuri,
thank you for your recommendation. I was able to generate the iomux_config files for my EVA board.
Could you please give me an additional advice where to get a simple bare-metal “HelloWorld”/ “Blinky” template project for MCIMX6UL-EVKB under ARM GCC with Eclipse?
I need just a quick start help. Maybe https://community.nxp.com/docs/DOC-94139 would be helpfull for me, but, the link to the “i.MX 6Series Platform SDK” files doesn’t work…
Thank you!
Best regards
Waldemar Rempel
Engineering Automation Systems Basis Firmware DC-IA/EAH2
Bosch Rexroth. The Drive & Control Company
Tel. +49 6062 78-1834
Fax +49 6062 78-771
Waldemar.Rempel@boschrexroth.de<mailto:Waldemar.Rempel@boschrexroth.de>
www.boschrexroth.com<http://www.boschrexroth.com>;
Bosch Rexroth AG
Berliner Straße 25
64711 Erbach
GERMANY
Firmensitz: Stuttgart, Registrierung: Amtsgericht Stuttgart HRB 23192
Vorstand: Rolf Najork (Vorsitzender) , Dr. Markus Forschner; Dr. Bertram Hoffmann; Dr. Marc Wucherer
Vorsitzender des Aufsichtsrats: Dr. Stefan Hartung
Von: Yuri
Gesendet: Dienstag, 23. Mai 2017 11:01
An: Rempel Waldemar (DC-IA/EAH2) <Waldemar.Rempel@boschrexroth.de>
Betreff: Re: - Integrating Processor Expert for i.MX and ARM GCC with Eclipse
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Integrating Processor Expert for i.MX and ARM GCC with Eclipse
new comment by Yuri Muhin<https://community.nxp.com/people/Yuri?et=watches.email.document_comment> View all comments on this document<https://community.nxp.com/docs/DOC-103736?commentID=43458&et=watches.email.document_comment#comment-43458>
Hello,
You may use the following regarding the Platform SDK :
swp-report/iMX6_Platform_SDK at master · backenklee/swp-report · GitHub
 Also, You may  look at the following :
Perhaps the following helps regarding i.MX6UL, since it may be considered as i.MX6SL derivative.
https://community.nxp.com/docs/DOC-331921
Regards,
Yuri.
I am compiling example given here but it giving following error.
Hello,
values of heap_start, top_of_stacks and __mmu_page_table_base__ are defined in linker file
mx6dq.ld. Verify if it is involved in Your case.
Regards,
Yuri.
Hello,
the mentioned lcs3 concerns with Sourcery CodeBench toolchain specifics.
Perhaps for Your toolchain linker file should be modified.
Regards,
Yuri.