Installing Japanese Language Pack for IMX Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing Japanese Language Pack for IMX Yocto

Installing Japanese Language Pack for IMX Yocto

Hello, this post describes how you can add Japanese Language to the Yocto BSP. There are just a few steps to achieve.

It was tested on the i.MX93-FRDM board, i.MX93-EVK and i.MX8M (Family). And Linux kernel 6.6.36.

 

The first step before to start your board building according to the Yocto Project User's Guide, is adding the below lines to the local.conf file:

GLIBC_GENERATE_LOCALES = "en_US.UTF-8 ja_JP.UTF-8"
IMAGE_LINGUAS = "en-us ja-jp"

IMAGE_INSTALL:append = " \
    glibc-gconv-euc-jp \
    glibc-gconv-sjis \
    glibc-gconv-utf-16 \
    glibc-utils \
    fontconfig \
    ttf-bitstream-vera \
    ttf-dejavu-sans \
"

 

Where: 

glibc-gconv-*: Adds Japanese encoding conversions.

 

After building, flash the Image to the board and boot it. You can check if the Japanese font was installed successfully with:

root@imx93frdm:~# locale -a
C
POSIX
en_US
en_US.utf8
ja_JP
ja_JP.utf8

 

We can see it was installed successfully:

ja_JP
ja_JP.utf8

 

Then, we can change the Language at Runtime with:

root@imx93frdm:~# export LANG=ja_JP.UTF-8
root@imx93frdm:~# export LC_ALL=ja_JP.UTF-8

 

Finally, probe with a command that supports Japanese outputs like "date":

root@imx93frdm:~# date
2024年  2月 27日 火曜日 17:29:11 UTC

 

 

I hope this information can helps to you.

 

Best regards,

Salas.

評価なし
バージョン履歴
最終更新日:
‎07-08-2025 01:23 PM
更新者: