I.MX6UL DDR3 Script Aid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6UL DDR3 Script Aid

I.MX6UL DDR3 Script Aid

Following docs(English or Chinese version) are also can be referred as a hand on guide.

Freescale i.MX6 DRAM Port Application Guide-DDR3

飞思卡尔i.MX6平台DRAM接口高阶应用指导-DDR3篇

Please find i.Mx6DQSDL LPDDR2 Script Aid through below link.

i.Mx6DQSDL LPDDR2 Script Aid

Please find i.Mx6DQSDL DDR3 Script Aid through below link.

i.Mx6DQSDL DDR3 Script Aid

Please find i.MX6SX DDR3 Script Aid through below link..

i.MX6SX DDR3 Script Aid

Any questions are welcome!

Change History:

0.02 - Add total 1Gbit density supporting.

Labels (1)
Attachments
Comments
hkr

Is there a newer version of the file? I saw a presentation with 5 tabs and also ARM DS-5 support... (https://community.nxp.com/docs/DOC-331528 )

Thanks! hkr

Hello LinWang,

   Greetings of the day...

       We have a customized imx6ul board which is having the two RAM chips(MT41K512M8DA-107P) connected parallel and using one CS pin DRAM_CS0. is this script support to test the 1GB DDR stress and calibration? where can i find the 1GB density script.

Thanks & Regards

Ganesh.K

No ratings
Version history
Last update:
‎02-24-2016 07:13 PM
Updated by: