I.MX27 PDK Board Flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX27 PDK Board Flashing

I.MX27 PDK Board Flashing

i.MX27 PDK Board Flashing

This tutorial teaches how to flash bootloader using ATK. To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot.

Using ATK

ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards.

This section will describe the procedure to erase the flash memory and program the bootloader.

1 - Connect a serial cable between PC and i.MX board.

2 - Some hardware configurations (switches) must be done to flash the board.

Set red and cream switches as below: 
Switch SW5 -> 00000 
Switch SW4 -> 10000001

Installing ATK on Linux

Download ATK:

Download. 

Extract ATK:

# unzip ATK_1_41_STD_installer.zip 

Execute the default install process:

# wine SETUP.EXE 

Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32)

Run ATK:

# wine ADSToolkit_std.exe 

Next Step

To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot.


400px-External_boot_imx27.jpg

PS: On SW5 and SW4, "1" means the keys selected towards the edge of the board.

3 - Run ATK by clicking Start -> Programs -> AdvancedToolKit -> AdvancedToolKit


Atk1_imx27.png

   
   Set the options:
   Device memory -> DDR; Custom Initial File -> (keep it unmarked)
   Communication Channel -> Serial Port (Usually COM1)

4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO.


Atk2_imx27.png

Flash Erasing

1 - To erase Flash memory, select the parameters as shown in the figure below:

Imx27_pdk_atk3.PNG

2 - Turn on the board and press Erase.

3 - ATK shows this message when flash is erased

Imx27_pdk_atk4.PNG

Flash Programming

The next step is to program the bootloader image into the board's Flash following the steps below.

1 - Select the parameters as shown in the figure below and press Program.

The bootloader binary image file can be found into your Board Support Package 
Set Program, NAND, Address: 0x00000000

Imx27_pdk_atk5.PNG

2 - Add it on Image File field and press Program.

3 - Close ATK, turn off the board and set switch back as shown in the picture below.

400px-Internal_boot_imx27.jpg

Installing ATK on Linux

Download ATK:

Download.

Extract ATK:

# unzip ATK_1_41_STD_installer.zip

Execute the default install process:

# wine SETUP.EXE

Get mfc42.dll and msvcp60.dll from a Windows Machine (C:\Windows\System32) and copy to wine system32 (/root/.wine/drive_c/windows/system32)

Run ATK:

# wine ADSToolkit_std.exe

Next Step

To flash kernel and root file system, follow the directions: IMX27 PDK NAND Flashing RedBoot.





标签 (1)
无评分
版本历史
最后更新:
‎09-10-2020 03:05 AM
更新人: