This article introduces how to connect a device via Bluetooth to the i.MX8M family of boards. The steps shown in this document were done using the i.MX8M Plus.
First, enable the BT service and start it. If systemctl refuses to start or enable these services, consider using the force option -f at the end of the following commands:
systemctl enable bluetooth.service
systemctl start bluetooth.service
Check status of BT. It should be active and running:
systemctl status bluetooth
You should see "Running" on Status:
● bluetooth.service - Bluetooth service
Loaded: loaded (/lib/systemd/system/bluetooth.service; enabled; vendor preset: enabled)
Active: active (running) since Mon 2021-11-29 19:41:18 UTC; 4s ago
Docs: man:bluetoothd(8)
Main PID: 710 (bluetoothd)
Status: "Running"
Tasks: 1
Memory: 1.9M
CGroup: /system.slice/bluetooth.service
└─710 /usr/libexec/bluetooth/bluetoothd
Nov 29 19:41:18 imx8mpevk systemd[1]: Starting Bluetooth service...
Nov 29 19:41:18 imx8mpevk systemd[1]: Started Bluetooth service.
To use the Bluetooth, it is necessary first to load the Wi-Fi, otherwise it won't be possible to load BT firmware. To do this, use the following steps:
modprobe moal mod_para=nxp/wifi_mod_para.conf
wpa_passphrase SSID SSID_PASSWD >> /etc/wpa_supplicant.conf
wpa_supplicant -d -B -i mlan0 -c /etc/wpa_supplicant.conf -Dnl80211
Up to this point, you should be able to use BT, however, if you want to continue connecting to a network using Wi-Fi, you can use the following steps. Otherwise, skip the following and go to the next section.
Run below command:
connmanctl
Connect to Wi-Fi:
connmanctl> enable wifi
connmanctl> scan wifi
#This should list the networks:
connmanctl> services
connmanctl> agent on
connmanctl> connect wifi_<some_numbers>_managed_psk
#Enter password of wifi network
Passphrase?
connmanctl> quit
Now that Wi-Fi is connected, BT can be used.
Show serial ports available on the system (each board has different devices):
dmesg | grep tty
i.MX8M Plus shows these results:
[ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk2p2 rootwait rw
[ 0.166330] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 29, base_baud = 5000000) is a IMX
[ 0.166815] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 30, base_baud = 5000000) is a IMX
[ 0.167185] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 31, base_baud = 1500000) is a IMX
[ 1.189285] printk: console [ttymxc1] enabled
[ 4.160356] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 7.171005] audit: type=1006 audit(1605328853.412:2): pid=665 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
For this article, the ttymxc0 port was selected. To attach the device port and set the baudrate (115200 for this case) run the following commands, where hciconfig is used to configure BT device and up opens and initializes HCI device:
hciattach ttymxc0 any 115200 flow
hciconfig hci0 up
hciconfig
After running the commands above, you should see this:
hci0: Type: Primary Bus: UART
BD Address: 00:E9:3A:0D:C7:80 ACL MTU: 1016:5 SCO MTU: 120:6
UP RUNNING
RX bytes:1424 acl:0 sco:0 events:82 errors:0
TX bytes:1218 acl:0 sco:0 commands:82 errors:0
Now you can manage BT with bluetoothctl.
To start bluetoothctl run the following command:
bluetoothctl
Scan for devices:
[bluetooth]# power on
[bluetooth]# default-agent
[bluetooth]# pairable on
#Start scanning for devices:
[bluetooth]# scan on
You should see the discovered devices:
[CHG] Controller 00:E9:3A:0D:C7:80 Discovering: yes
[NEW] Device E0:89:7E:86:47:47 E0-89-7E-86-47-47
[NEW] Device 59:80:27:7E:98:A2 59-80-27-7E-98-A2
[NEW] Device EC:81:93:51:FE:66 EC-81-93-51-FE-66
[NEW] Device 50:32:37:D0:A5:B8 50-32-37-D0-A5-B8
[NEW] Device 2C:DD:64:A1:B2:48 2C-DD-64-A1-B2-48
[NEW] Device 08:66:98:EF:B6:C5 08-66-98-EF-B6-C5
...
...
Wait for the system to find the device you want to pair and use the following command:
#Use the corresponding address from your device
[bluetooth]# pair 88:29:9C:59:BC:F6
Confirm the passkey both in the i.MX8M board and device. If all steps were done successfully you should see now the name of your connected device instead of [bluetooth]#. To stop scanning, the scan off command can be used. To see connected devices and information, use the following commands:
#A galaxy S10+ was connected to the i.MX8M Plus
[Galaxy S10+]# devices
[Galaxy S10+]# info