How to Enable LDO Bypass Based on i.MX6 Android ICS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Enable LDO Bypass Based on i.MX6 Android ICS

How to Enable LDO Bypass Based on i.MX6 Android ICS

Overview


i.MX6Dual/Quad supports using internal LDO or bypass internal LDO. LDO bypass is helpful to save power consumption and reduce thermal under high loading use cases because the power consumption on internal LDO can be saved. The purpose of this document is to introduce how to enable LDO bypass based on i.MX6 R13.4.1 release on i.MX6Dual/Quad SabreSD board.

Constraint


LDO Bypass solution currently can only be applied to i.MX6Dual/Quad 1GHz. LDO bypass function will force disabled on i.MX6Dual/Quad 1.2GHz, but customer can estimate this function through limit the max ARM frequency to 1GHz by command line 'arm_freq=1000' on i.MX6Dual/Quad 1.2GHz .

Hardware Voltage Settings


The following table lists the voltage settings in each working CPU frequency and VPU frequency with LDO bypass solution:


VPU FrequencyARM FrequencyVDDARM_IN (V)VDDSOC_IN (V)
0 to 352MHz996MHz1.251.25
264-> 352MHz702MHz1.151.25
0 to 264MHz792MHz1.151.175
264->352MHz396MHz0.951.25
<264MHz396MHz0.951.175


VDDARM_IN and VDDSOC_IN voltage setting should be within the voltage range, considering the ripple:

  • VDDARM_IN - ripple>VDDARM_INmin
  • VDDARM_IN + ripple<VDDARM_Inmax

For the Min/Max value, refer to the i.MX6Dual/Quad data sheet. The above list is based on SabreSD PFuse-100.

Software Changes

Please apply the patches into Android-13.4.1-LDO_BYPASS-pathes.tar.gz.gz based on R13.4.1. The change lists:

  • uboot-imx: move LDO bypass code and one PFUZE1.0 workaround code to kernel. Remove CONFIG_MX6_INTER_LDO_BYPASS in u-boot.
  • kernel: A set of patches are used to support LDO bypass enable/disable by command option.

How to Enable/Disable LDO Bypass

After applying for above patches, you can add command option into boot command line to enable or disable LDO:

  • Command option “ldo_active=off”: Enable LDO bypass mode
  • Command option “ldo_active=on”: Enable LDO active
ラベル(2)
添付
コメント

Anyone ever integrated the PF0100 into the imx6_cpufreq driver to take advantage of DVFS for LDO bypass mode?

--> e.g. 0.95V when running at 396MHz, 1.15 when running at 792MHz

Solution to use the PF0100 for DVFS: https://community.nxp.com/thread/462514#comment-954021 

評価なし
バージョン履歴
最終更新日:
‎01-31-2013 05:43 AM
更新者: