Enable PCIE driver on i.MX8MM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable PCIE driver on i.MX8MM

Enable PCIE driver on i.MX8MM

Platform: I.MX8MMEVK

uboot version:  uboot-imx_lf_v2023.04

BSP: 6.1.x

Add patch in uboot

git clone https://github.com/nxp-imx/uboot-imx.git
git checkout lf_v2023.04
git apply 0001-Enable-imx8mm-pcie-driver-v2023.04.patch

 

test log:

u-boot=> pci enum
pcie phy base: 0x32f00000, size 0x10000
pcie phy pll is locked after 0 us.
Link up, Gen1
u-boot=> pci
BusDevFun  VendorId   DeviceId   Device Class       Sub-Class
_____________________________________________________________
00.00.00   0x16c3     0xabcd     Bridge device           0x04
01.00.00   0x1131     0x3003     Network controller      0x00
01.00.01   0x1131     0x3004     Network controller      0x00

 

Attachments
No ratings
Version history
Last update:
‎05-23-2025 02:17 AM
Updated by: