Detailed Operations For Standalone On Linux BSP of I.MX Processors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Detailed Operations For Standalone On Linux BSP of I.MX Processors

Detailed Operations For Standalone On Linux BSP of I.MX Processors

Host Environment: ubuntu 16.04 LTS

Linux BSP For i.MX : version 4.9.88

The document has 5 main contents:

1. Compiling core-image-base in Yocto BSP

--Copy u-boot source code to a new directory

--Copy linux kernel source code to a new directory

2. Exporting 4.9.88 toolchain from Freescale Yocto BSP

(1) Using MACHINE=imx7dsabresd to export the toolchain

(2) Using MACHINE=imx6qsabresd to export the toolchain.

Actually above 2 are the same toolchain after exporting. Here , only show any one of boards(not ARM64) can be used for MACHINE. So users only need to export it for one time, select (1) or (2) to export toolchain.

(3) Using MACHINE=imx8mqevk to export ARM64 toolchain

3. Compling u-boot & linux kernel under Stanalone

  • iMX7DSabreSD

--Compiling  u-boot for imx7dsabresd

--Compiling kernel and dtb for imx7dsabresd

  • iMX8MQEVK

--Compiling u-boot for imx8mqevk

--Compiling kernel and dtb for imx8mqevk

4. Compiling OS Firmware for i.MX7DSabreSD board

--u-boot for mfg tools

--kernel and dtb for mfg tools

5. Copy OS Firmware to the related path of MFG tools

---------------------------------------------------------------------------------------------------------------------------

[Content of Document]

1. Compiling core-image-base in Yocto BSP

         After repo syn is done according to “i.MX_Yocto_Project_User's_Guide.pdf”, Use the command to compile linux BSP, u-boot & kernel source code will be released.

# DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source fsl-setup-release.sh -b build-fb

# bitbake core-image-base

         After compiling is done, u-boot & linux kernel source code is in the path below:

u-boot: ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git

linux: ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/git

         We can create a new directory for uboot and linux kernel source code. Here I created a directory named disk2.

# cd ~/

# mkdir disk2

# cd disk2

# mkdir u-boot-2017-03

# mkdir linux-imx-4.9.88

--Copy u-boot source code to a new directory

# cd ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git

# cp –r ./* ~/disk2/u-boot-2017-03

--Copy linux kernel source code to a new directory

# cd ~/imx-yocto-bsp/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/git

# cp –r ./* ~/disk2/ linux-imx-4.9.88

2. Exporting 4.9.88 toolchain from Freescale Yocto BSP

(1) Using MACHINE=imx7dsabresd to export the toolchain

Step1:

# cd ~/imx-yocto-bsp/

# DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source fsl-setup-release.sh -b build-minimal

… …

Do you accept the EULA you just read? (y/n)  y

EULA has been accepted.

Welcome to Freescale Community BSP

The Yocto Project has extensive documentation about OE including a

reference manual which can be found at:

    http://yoctoproject.org/documentation

For more information about OpenEmbedded see their website:

    http://www.openembedded.org/

You can now run 'bitbake <target>'

Common targets are:

    core-image-minimal

    meta-toolchain

    meta-toolchain-sdk

    adt-installer

    meta-ide-support

Your build environment has been configured with:

    MACHINE=imx7dsabresd

    SDKMACHINE=i686

    DISTRO=fsl-imx-fb

    EULA=

BSPDIR=

BUILD_DIR=.

meta-freescale directory found

Here “build-minimal” is a directory for compiling source code, users can also set it other name.

In ~/imx-yocto-bsp/build-minimal, Begin to export toolchain with the command.

Step2:

# DISTRO=fsl-imx-fb MACHINE=imx7dsabresd bitbake core-image-minimal -c populate_sdk

pastedImage_14.png

[Comment-1] About DISTRO and MACHINE on above 2 commands

  • MACHINE can be set the values below.
  • imx6qpsabreauto
  • imx6qpsabresd
  • imx6ulevk
  • imx6ull14x14evk
  • imx6ull9x9evk
  • imx6dlsabreauto
  • imx6dlsabresd
  • imx6qsabreauto
  • imx6qsabresd
  • imx6slevk
  • imx6solosabreauto
  • imx6solosabresd
  • imx6sxsabresd
  • imx6sxsabreauto
  • imx6sllevk
  • imx7dsabresd
  • imx7ulpevk
  • imx8mqevk

 

So MACHINE’s value is the name each Evaluation Borad.

DISTRO can be set the values below:

  • fsl-imx-x11 - X11 graphics are not supported on i.MX 8.
  • fsl-imx-wayland - Wayland weston graphics.
  • fsl-imx-xwayland - Wayland graphics and X11. X11 applications using EGL are not supported.
  • fsl-imx-fb - Frame Buffer graphics - no X11 or Wayland. Frame Buffer is not supported on i.MX 8

bitbake rootfs type

  •       core-image-minimal
  •       core-image-base
  •       core-image-sato
  •       fsl-image-machine-test
  •       fsl-image-validation-imx
  •       fsl-image-qt5-validation-imx

Below is the detailed description for above rootfs type:

pastedImage_16.png

[Comment-2] Descriptions on difference of toolchain between i.MX6/7 and i.MX8MQ

         i.MX6 and i.MX7 are both 32bit ARM processor, they use the same toolchain.

         i.MX8MQ is 64bit ARM processor, so it’s toolchain is different from that of i.MX6/7.

Setp 3:

         After above compiling is done, enter into ~/imx-yocto-bsp/build-minimal/tmp/deploy/sdk

# cd ~/imx-yocto-bsp/build-minimal/tmp/deploy/sdk

# ls

pastedImage_17.png

Run .sh file:

pastedImage_18.png

Then continue operations according to guidance:

pastedImage_19.png

pastedImage_20.png

Done:

pastedImage_21.png

OK, Let us check /opt/fsl-imx-fb/ directory:

# ls /opt/fsl-imx-fb/4.9.88-2.0.0/

pastedImage_22.png

         Because we used MACHINE=imx7dsabresd, environment was named “cortex-A7”, compiler’s version is still 4.9.88.

(2) Using MACHINE=imx6qsabresd to export the toolchain.

         We can change “MACHINE=imx6qsabresd” and repeat above 3 steps, environment will be named “cortex-A9”.

         Close the current terminal, and open a new one.

# cd ~/ imx-yocto-bsp

# DISTRO=fsl-imx-fb MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-A9-min

 pastedImage_24.png

         Then automatically enter “~/imx-yocto-bsp/build-A9-min”, run command below.

# DISTRO=fsl-imx-fb MACHINE=imx6qsabresd bitbake core-image-minimal -c populate_sdk

pastedImage_25.png

# ~/imx-yocto-bsp/build-A9-min/tmp/deploy/sdk

# ls

pastedImage_26.png

# ./ fsl-imx-fb-glibc-x86_64-core-image-minimal-cortexa9hf-neon-toolchain-4.9.88-2.0.0.sh

  Set it up in another directory: /opt/fsl-imx-fb/4.9.88

pastedImage_27.png

(3) Using MACHINE=imx8mqevk to export ARM64 toolchain

         Export Toolchain for i.MX8MQ, create a new terminal, then run these 2 commands below.

# ~/imx-yocto-bsp

# DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-xwayland

# DISTRO=fsl-imx-fb MACHINE=imx8mqevk bitbake core-image-minimal -c populate_sdk

pastedImage_29.png

Done.

         Copy the toolchain to /opt/fsl-imx-fb directory

# cd ~/imx-yocto-bsp/build-xwayland/tmp/deploy/sdk

# ls

pastedImage_30.png

#./fsl-imx-fb-glibc-x86_64-core-image-minimal-aarch64-toolchain-4.9.88-2.0.0.sh

         I installed it to a new directory: /opt/fsl-imx-fb/4.9.88-arm64

pastedImage_31.png

#ls ls /opt/fsl-imx-fb/4.9.88-arm64/

pastedImage_32.png

 OK, 64bit toolchain for i.MX8MQ has been exported to the directory.

3. Compling u-boot & linux kernel under Stanalone

  • iMX7DSabreSD

--Compiling  u-boot for imx7dsabresd

# cd ~/disk2/u-boot-2017-03

# source /opt/fsl-imx-fb/4.9.88-2.0.0/environment-setup-cortexa7hf-neon-poky-linux-gnueabi

# export ARCH=arm

# make clean

# make mx7dsabresd_defconfig

pastedImage_33.png

# make u-boot.imx

pastedImage_34.png

Done.

--Compiling kernel and dtb for imx7dsabresd

# cd ~/disk2/linux-imx-4.9.88/

[comment] If environment has been configured, that is, these 2 commands have been run on the current terminal, don’t need to run them again.

“source /opt/fsl-imx-fb/4.9.88-2.0.0/environment-setup-cortexa7hf-neon-poky-linux-gnueabi”

and

“export ARCH=arm”

# make clean

# make imx_v7_defconfig

# make

 

         zImage is in “~/disk2/linux-imx-4.9.88/arch/arm/boot”

         dtb is in “~/disk2/linux-imx-4.9.88/arch/arm/boot/dts”

 

         Probably users want to run “make menuconfig”, and meet the errors like below.

# sudo apt-get install libncurses*  (To solve the problem below)

pastedImage_37.png

# make menuconfig

pastedImage_38.png

[Comment-3]  Users can also use "environment-setup-cortexa9hf-neon-poky-linux-gnueabi" to compile u-boot and kernel.

  • iMX8MQEVK

--Compiling u-boot for imx8mqevk

# cd ~/disk2/u-boot-2017-03

# source /opt/fsl-imx-fb/4.9.88-arm64/environment-setup-aarch64-poky-linux

# export ARCH=arm64

# make clean

# make imx8mq_evk_defconfig

pastedImage_40.png

# make u-boot.imx

pastedImage_42.png

Done.

--Compiling kernel and dtb for imx8mqevk

# cd ~/disk2/linux-imx-4.9.88/

[comment] If environment has been configured, that is, these 2 commands have been run on the current terminal, don’t need to run them again.

“source /opt/fsl-imx-fb/4.9.88-arm64/environment-setup-aarch64-poky-linux”

and

“export ARCH=arm64”

# make clean

# make defconfig

pastedImage_43.png

# make

pastedImage_44.png

         Run the command to unset LDFLAGS:

# unset LDFLAGS

# make

pastedImage_45.png

Done.

4. Compiling OS Firmware for i.MX7DSabreSD board

--u-boot for mfg tools

# make mx7dsabresd_config

# make u-boot.imx

         Then rename u-boot.imx to be “u-boot-mx7dsabresd-mfg.imx”.

--kernel and dtb for mfg tools

         Copy imx_v7_mfg_defconfig file to “arch/arm/configs”, then run commands below.

# make imx_v7_mfg_defconfig

# make

         zImage will be generated at path arch/arm/boot.

         dtb file will be generated at path arch/arm/boot/dts

 

         Then rename zImage to be zImage-mx7dsabre-mfg,

         Rename imx7d-sdb.dtb to be zImage-imx7d-sdb-mfg.dtb

5. Copy OS Firmware to the related path of MFG tools

         Up to now, 3 files for OS Firmware has been generated, then copy these 3 files to mfgtools\Profiles\Linux\OS Firmware\firmware

 

         When MFG Tools begins to run, these 3 files and ramdisk will be downloaded to SDRAM on board, then run them, and download images(u-boot\kernel\rootfs\)  which have been ready in  “mfgtools\Profiles\Linux\OS Firmware\files”.

 

         Above steps and commands will be performed according to list in ucl2.xml. So customer will add a new list for her downloading or change an existing list according to image’s name.

NXP TIC team

Weidong Sun

04-25-2019

添付
コメント

Seems important, but what is this about?

0%が役に立ったと言っています (0/1)
バージョン履歴
最終更新日:
‎04-24-2019 08:25 PM
更新者: