We are pleased to announce that Config Tools for i.MX v16.0 are now available.
Full details on the release (features, known issues...)
The product is based on Eclipse 2023-12
Framework
– Enable the Peripherals tool in the Config Tools for i.MX
– Enable the Clocks tool in the Config Tools for i.MX
– A new command-line argument (- UpdateCode) has been added. It performs the same action as the Update
Code button in the user interface. It must be used with -HeadlessTool.
DDR tool
– CA bus driver strength and ODT configuration for the mScale processors are added.
– [MX 93/MX 91] The UART configuration from UI is added.
– MX 91 DDR tool update for Config tools
– MX 93 PF 09 DDR tool support is added.
SerDes tool
– MX 95 SerDes tool support is enabled.
Pins tool
– Simultaneous routing detection (routing of one signal may result in multiple signals being routed based
on the same register settings) is added. In that case, such signals are offered to be added into the
configuration.
– Support of internal pins that are not available in the package is added.