Prerequisites:
The build is verified on prebuilt rootfs(based on LTIB) which can be downloaded from freescale.com or built from Yocto fsl-image-gui
These steps are performed on the host:
1. Download the git respository for qt5:
$ git clone git://gitorious.org/qt/qt5.git qt5
cd qt5
Let us consider this as <QTDir>
2. Create a build directory to install for the qt5 packages. This directory can be in any loctation. For example,
$ mkdir /opt/qt5
sudo chown -R <username> /opt/qt5
Let us consider the the installdir as /opt/qt5
3. Enter the Qt5 directory and run the perl init-repository script to download all the source code for
Qt5. To download all the source code will take about an hour.
$ perl init-repository
4. Download the attached linux-imx5-g++.tar.gz and copy to qtbase/mkspecs/devices.
Will try to get updstreamed.
5. From the following path
$ gedit qtbase/mkspecs/devices/linux-imx5-g++/qmake.conf
6. At the top of the qmake.conf, there is a configure line. Copy and paste the configure line into a text file located
in your build build directory. Edit the configure line to find your toolchain and filesystem. Also make sure to
include the options -no-pch, -no-opengl, -opengl es2, Here is an example of
a configure line.
$ cd <QTDir>
$ cd qtbase
$ ./configure -v -opensource -confirm-license -no-pch -opengl es2 -make libs -device imx5 \
-nomake examples -nomake demos \
-device-option CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi- \
-sysroot <rootfs> -no-gcc-sysroot \
-prefix <installdir>
7. Make the textfile that has the configure line and executable and run it. When the configure summary is shown make sure the Qt5
has openGL ES 2.0 support. Do build
$make
$make install
When Qt5 has finished building, Qt5 will be installed in two places:
1. <location of rootfs>/<installdir>
2. <HOST Machine>/<install dir>
This is good because now all the libraries and binaries for Qt5 are installed on the host and the target filesystem. Therefore,
the target already has all the libraries and binaries needed to run Qt5.
8. Also need to build qtjsbackend and qtdeclarative.
$ cd <location to Qt5 git>
$ cd qtjsbackend
$ ../qtbase/bin/qmake -r
$ make && make install
$ $ cd <location to Qt5 git>
$ cd qtdeclarative
$ ../qtbase/bin/qmake -r
$ make && make install
9. Run Qt apps on target
- Boot the target either with NFS or SD Image
- Ensure that folder <installdir> is copied on target file system at “/usr/local”.
- Launch application using
$ cd /usr/local/qt5/examples/opengl/hellogl_es2
$ ./hellogl_es2 -platform eglfs
error:
hread -lgthread-2.0 -lrt -lglib-2.0
.obj/release-shared/qeventdispatcher_glib.o: In function `QEventDispatcherGlibPrivate::QEventDispatcherGlibPrivate(_GMainContext*)':
qeventdispatcher_glib.cpp:(.text+0x7f0): undefined reference to `g_main_context_push_thread_default'
.obj/release-shared/qeventdispatcher_glib.o: In function `QEventDispatcherGlib::~QEventDispatcherGlib()':
qeventdispatcher_glib.cpp:(.text+0xbf0): undefined reference to `g_main_context_pop_thread_default'
.obj/release-shared/qeventdispatcher_glib.o: In function `QEventDispatcherGlib::~QEventDispatcherGlib()':
qeventdispatcher_glib.cpp:(.text+0xdd4): undefined reference to `g_main_context_pop_thread_default'
.obj/release-shared/qeventdispatcher_glib.o: In function `QEventDispatcherGlib::~QEventDispatcherGlib()':
qeventdispatcher_glib.cpp:(.text+0xfb0): undefined reference to `g_main_context_pop_thread_default'
.obj/release-shared/qeventdispatcher_glib.o: In function `QEventDispatcherGlibPrivate::QEventDispatcherGlibPrivate(_GMainContext*)':
qeventdispatcher_glib.cpp:(.text+0x1114): undefined reference to `g_main_context_push_thread_default'
collect2: ld returned 1 exit status
make[2]: *** [../../lib/libQt5Core.so.5.1.0] Error 1
make[2]: Leaving directory `/home/mqy/qt5/qtbase/src/corelib'
need for help?
Had to add couple options to start compilation:
-no-xcb -no-c++11
but still got errors, first one:
make[2]: Entering directory `/home/user/git/qt5/qtbase/src/network'
/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-g++ -c -pipe -mfloat-abi=softfp -O2 -O2 -march=armv7-a -mfpu=neon -D_LINUX -fvisibility=hidden -fvisibility-inlines-hidden -fno-exceptions -Wall -W -D_REENTRANT -fPIC -DQT_NO_LIBUDEV -DQT_NO_XCB -DQT_NO_XKBCOMMON -DQT_NO_USING_NAMESPACE -DQT_BUILD_NETWORK_LIB -DQT_BUILDING_QT -DQT_NO_CAST_TO_ASCII -DQT_ASCII_CAST_WARNINGS -DQT_MOC_COMPAT -DQT_USE_QSTRINGBUILDER -DQT_DEPRECATED_WARNINGS -DQT_DISABLE_DEPRECATED_BEFORE=0x050000 -DQT_NO_EXCEPTIONS -D_LARGEFILE64_SOURCE -D_LARGEFILE_SOURCE -DQT_NO_DEBUG -DQT_CORE_LIB -I../../mkspecs/devices/linux-imx5-g++ -I. -I../../include -I../../include/QtNetwork -I../../include/QtNetwork/5.1.0 -I../../include/QtNetwork/5.1.0/QtNetwork -Ikernel -I../../include/QtCore -I../../include/QtCore/5.1.0 -I../../include/QtCore/5.1.0/QtCore -I.moc/release-shared -I/home/user/ltib/rootfs/usr/include -o .obj/release-shared/qsslsocket_openssl.o ssl/qsslsocket_openssl.cpp
ssl/qsslsocket_openssl.cpp: In member function 'virtual void QSslSocketBackendPrivate::continueHandshake()':
ssl/qsslsocket_openssl.cpp:1414: error: 'q_SSL_ctrl' was not declared in this scope
make[2]: *** [.obj/release-shared/qsslsocket_openssl.o] Error 1
make[2]: Leaving directory `/home/user/git/qt5/qtbase/src/network'
make[1]: *** [sub-network-make_first] Error 2
make[1]: Leaving directory `/home/user/git/qt5/qtbase/src'
make: *** [sub-src-make_first] Error 2
I got the same error and as a workaround I commented out the lines under #if GLIB_CHECK_VERSION (2, 22, 0) macro
======== ./src/corelib/kernel/qeventdispatcher_glib.cpp ===========
QEventDispatcherGlibPrivate::QEventDispatcherGlibPrivate(GMainContext *context)
: mainContext(context)
{
. . .
#if GLIB_CHECK_VERSION (2, 22, 0)
//g_main_context_push_thread_default (mainContext);
endif
. . .
}
QEventDispatcherGlib::~QEventDispatcherGlib()
{
. . .
#if GLIB_CHECK_VERSION (2, 22, 0)
//g_main_context_pop_thread_default (d->mainContext);
#endif
. . .
}
I use the option -no-openssl as a workaround to get rid off this error
./configure -v -opensource -confirm-license -no-pch -opengl es2 -make libs -device imx5 -no-openssl -no-xcb -no-c++11 -device-option CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi- -sysroot /home/juan/imx53/ltib/rootfs -no-gcc-sysroot -prefix /opt/qt5