Build bootloader without spl in Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build bootloader without spl in Yocto

Build bootloader without spl in Yocto

Software environment: L5.4.47_2.2.0

Hardware i.MX8QXPC0 EVK board

In the uuu script we can see the bootloader imx-boot-imx8qxpc0mek-sd.bin-flash is necessary.

The default BSP build generate in the yocto project is with the spl, some customers are confused about the how to build the imx-boot-imx8qxpc0mek-sd.bin-flash.

Here I give the manually compile way and generate it in yocto.

In the yocto generate it is more convenient than the manually compile way.

Hope this can do help for you.

Attachments
No ratings
Version history
Last update:
‎06-17-2021 02:30 AM
Updated by: