The i.MX Android N7.1.2_2.0.0 GA release is now available on IMX_SW page.
- Supported Hardware SoC/Boards:
- i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform
- i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform
- i.MX 6SoloLite EVK platform
- i.MX 6SoloX SABRE-SD board and platforms
- i.MX 6SoloX SABRE-AI board and platforms
- i.MX 7Dual SABRE-SD board and platform
Compared to the N7.1.1_1.0.0 release, this release has the following major changes:
- Upgraded the Android code base from android-7.1.1_r13 to android-7.1.2_r9.
- Upgraded U-Boot from v2015.04 to v2017.03.
- Upgraded the kernel from v4.1.15 to v4.9.17.
- Upgraded the GPU driver from 6.2.0.p2 to 6.2.2.p1.
- Upgraded the Wi-Fi BCMDHD release version to 1.141.100.6.
- Refine the Gralloc and HWC HAL.
- Enable the GPT partition to replace the MBR partition.
For features please consult the release notes.
For known issues and more details please consult the Release Notes.