All Boards PMIC Registers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

All Boards PMIC Registers

All Boards PMIC Registers

Atlas PMIC

i.MX Platforms uses Freescale Atlas chipset as power management IC (PMIC).

PMIC is connected with i.MX processor through SPI port.

Reading and Changing PMIC Registers

pmic_reg is a simple program that allows to read and change PMIC registers through SPI.

Click here to download the binary

Click here to download the source package

Click here to download the spec file


pmic_reg Installation

To use pmic_reg, you can simply download the binary file and move it to your system.

To build the source code, download and mv the source package (in this case "pmic_reg-1.0.tar.gz") to /opt/freescale/pkgs:

sudo mv pmic_reg-1.0.tar.gz /opt/freescale/pkgs

Download the spec file to spec directory:

mkdir <ltib directory>/dist/lfs-5.1/pmic_reg
cp pmic_reg.spec <ltib directory>/dist/lfs-5.1/pmic_reg

On <ltib directory>, extract, build and deploy pmic_reg:

./ltib -p pmic_reg.spec -m prep
./ltib -p pmic_reg.spec -m scbuild
./ltib -p pmic_reg.spec -m scdeploy

Source files will be located at <ltib directory>/rpm/BUILD/pmic_reg-1.0 and binary will be located at /usr/bin on your i.MX system rootfs.


pmic_reg Usage

To get pmic_reg help, just type pmic_reg:

PMIC_REG v1.0 (2009.12.15) Usage To read all PMIC registers: pmic_reg r To write to a specific register: pmic_reg w <register address> <register value>

标记 (1)
无评分
版本历史
最后更新:
‎09-10-2020 02:29 AM
更新人: