All Boards Deploy NFS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

All Boards Deploy NFS

All Boards Deploy NFS

NFS

After LTIB installation, follow the instructions below to configure and build Linux Image and Root File System.

TIP: Type: $./ltib --help to get more information on ltib

  • In the folder where LTIB were installed, execute the file:
$./ltib

It should take some minutes to complete the installation.

  • Configure the ltib to select the options and packages to be defined and installed in Linux Image and Root File System.
$./ltib -c     or     $./ltib -m config 

The menu configuration should appear:

400px-Ltib1.png

To configure for use the system with NFS, go to:

Target Image Generation -> Target Image -> NFS Only 

For basic compilation, exit LTIB. It will compile and add some pre-built packages to make the target file system.



标记 (1)
无评分
版本历史
最后更新:
‎09-10-2020 01:46 AM
更新人: