libnfc-nci supports PN7160 or not?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

libnfc-nci supports PN7160 or not?

ソリューションへジャンプ
1,423件の閲覧回数
NealZhang
Contributor III

Anybody could let me know if the PN7160 can be used with the libnfc-nci library? I read AN11697, which is a guide for using libnfc-nci with PN7120 and PN7150. However, I couldn't find any information indicating that this library supports the PN7160.

NealZhang_0-1724753744979.png

In addition, if the kernel driver nxp-pn5xx also supports PN7160 or not?

NealZhang_1-1724753744989.png

By the way, I'm going to integrate a NFC module into a linux board based on I.MX 8MPLUS, and we plan to use PN7160 for the advice from NXP official website

NealZhang_2-1724753744972.png

Thanks~~~

 

0 件の賞賛
返信
1 解決策
1,407件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @NealZhang 

I hope you are doing well.

It appears that the nxp-pn5xx only supports devices of the PN5xx Family. But there is other specific driver for the PN7160.

Also, it appears to be supported by libnfc-nci, as you can see on the AN11697 the libnfc-nci is running at user space with HAL:

Alejandro_Salas_0-1724772387741.png

But really I cannot to be sure if it is totally compatible.

 

I hope this can helps to you.

 

Best regards,

Salas.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,408件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @NealZhang 

I hope you are doing well.

It appears that the nxp-pn5xx only supports devices of the PN5xx Family. But there is other specific driver for the PN7160.

Also, it appears to be supported by libnfc-nci, as you can see on the AN11697 the libnfc-nci is running at user space with HAL:

Alejandro_Salas_0-1724772387741.png

But really I cannot to be sure if it is totally compatible.

 

I hope this can helps to you.

 

Best regards,

Salas.

0 件の賞賛
返信
1,397件の閲覧回数
NealZhang
Contributor III
Hi, Salas
Thanks very much for your kindly reply.
Actually, I have found the guide of PN7160
https://www.nxp.com.cn/docs/en/application-note/AN13287.pdf

Best regards,
Neal Zhang
0 件の賞賛
返信