[imx6qd] Increase graphic performance on sliced display?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx6qd] Increase graphic performance on sliced display?

2,057 Views
woutervh
Contributor IV

Hello,

on our product, we have panels which require full-hd timings (so 1920x1080). Only they are actually sliced to physically 1920x350. So 2/3 of the bandwidth is used for something not needed. Is there a way to reduce the framebuffer height, so reducing the needed bandwith, so increasing the refresh rate and performance? Only the IPU needs to output 1920x1080 towards the ldb. Everything before can be 1920x350.

Can this be done? I'm on kernel 5.4 with vivante drivers

0 Kudos
Reply
3 Replies

2,015 Views
woutervh
Contributor IV

Any additional input?

0 Kudos
Reply

2,041 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello woutervh,

The resolution of 1920x350 is not supported by current driver, you have to create this own driver.

 

Regards

 

 

0 Kudos
Reply

2,033 Views
woutervh
Contributor IV

Create an own driver for a resolution? How to do that? And will it indeed increase the performance compared to 1920x1080?

0 Kudos
Reply