iMX8MP - Vivante GPU and MSAA performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MP - Vivante GPU and MSAA performance

1,126 Views
vix
Contributor III

I've just built over the BSP i.MX, Linux, LF6.6.52_2.2.0 and in Chromium 117.0.5938.132 under chrome://gpu I see the following entry:

Problems Detected

  • On Vivante GPUs MSAA performance is not acceptable for GPU rasterization

Applied Workarounds: msaa_is_slow

What is the reason of this problem?

Is there some issue in the vivante drivers on iMX8MP?

Is this a hardware limit? But in this case I would not expect to see this under "Problems Detected" section.

 

Thanks

Tags (3)
0 Kudos
Reply
7 Replies

1,119 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

What is the reason of this problem?

... the reason is the vivante driver if 64 bits and chrome does not support this 64 bits in rasterization

 

Is there some issue in the vivante drivers on iMX8MP?

--- No, that is exclusively for Chrome

Is this a hardware limit? But in this case I would not expect to see this under "Problems Detected" section.

--- No.

regards

 
0 Kudos
Reply

1,116 Views
vix
Contributor III

Thanks @Bio_TICFSL 

... the reason is the vivante driver if 64 bits and chrome does not support this 64 bits in rasterization

Do you know if this is a topic under improvement in chrome/chromium?

Should I report this to chromium developers?

Is there an issue opened there?

0 Kudos
Reply

1,114 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Verisilicon is working on that.

Regards

0 Kudos
Reply

1,046 Views
vix
Contributor III

Hi @Bio_TICFSL 

 

do you mean Verisilicon has been working on a chromium patch?

Can you post here when the pach is available?

0 Kudos
Reply

1,043 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Sorry, So far there is no patch from NXP.

Regards

0 Kudos
Reply

1,015 Views
vix
Contributor III

I don't understand.

I mean: when (in the future) the patch from Verisilicon will be available, can you write here?

0 Kudos
Reply

1,013 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

I don;t know you can ask them.

https://www.verisilicon.com/en/ContactUs

Regards

 

0 Kudos
Reply