I've just built over the BSP i.MX, Linux, LF6.6.52_2.2.0 and in Chromium 117.0.5938.132 under chrome://gpu I see the following entry:
Problems Detected
Applied Workarounds: msaa_is_slow
What is the reason of this problem?
Is there some issue in the vivante drivers on iMX8MP?
Is this a hardware limit? But in this case I would not expect to see this under "Problems Detected" section.
Thanks
Hello,
What is the reason of this problem?
... the reason is the vivante driver if 64 bits and chrome does not support this 64 bits in rasterization
Is there some issue in the vivante drivers on iMX8MP?
--- No, that is exclusively for Chrome
Is this a hardware limit? But in this case I would not expect to see this under "Problems Detected" section.
--- No.
regards
Thanks @Bio_TICFSL
... the reason is the vivante driver if 64 bits and chrome does not support this 64 bits in rasterization
Do you know if this is a topic under improvement in chrome/chromium?
Should I report this to chromium developers?
Is there an issue opened there?
Hello,
Verisilicon is working on that.
Regards
Hi @Bio_TICFSL
do you mean Verisilicon has been working on a chromium patch?
Can you post here when the pach is available?
Hello,
Sorry, So far there is no patch from NXP.
Regards
I don't understand.
I mean: when (in the future) the patch from Verisilicon will be available, can you write here?