What is the state of iMX6 support regarding the imx-gst1.0-plugin and multimedia functionality. Is MX6 still supported and working for 5.10 kernel? I.e. MM_04.06.02_2108_L5.10.y
Regards,
Andreas
Ok, so after some digging I find that community projects almost exclusively use gstreamer-imx so I guess trying to build a yocto image using meta-imx would provide me with imx-gst1.0-plugins.
The reason I am asking is that I have an old application (3.10 kernel) using vpuenc/vpudec, this application enables the user to seek, fast forward, fast reverse and frame step backwards/forwards. I've tried this with the community gstreamer-imx but it seems it doesn't work at all.
Can you confirm if these use cases (reverse playback, frame stepping back/forward) works with imx-gst1.0-plugin for imx6q?
Best regards,
Andreas
>Can you confirm if these use cases (reverse playback, frame stepping back/forward) works with imx-gst1.0-plugin for imx6q?
yes. Known issues are described in sect.7.5 Known issues and limitations for multimedia
Best regards
igor
Hi Andreas
> Is MX6 still supported and working for 5.10 kernel? I.e. MM_04.06.02_2108_L5.10.y
right, supported as described in i.MX Linux Release Notes , Chapter 7 Multimedia i.MX Linux User’s Guide
https://source.codeaurora.org/external/imx/imx-gst1.0-plugin/?h=MM_04.06.02_2108_L5.10.y
Best regards
igor