Why IMX-MIPI-HDMI can only support up to 720p when use LCDIF on imx8MQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why IMX-MIPI-HDMI can only support up to 720p when use LCDIF on imx8MQ

Jump to solution
2,738 Views
xiaowei_zeng
Contributor III

In "i.MX8MQ EVK Display Selection Guide", it says when use IMX-MIPI-HDMI through LCDIF, it can only support up to 1280x720 60HZ

However, from the datasheet, LCDIF, MIPI and also the adv7535 on IMX-MIPI-HDMI all support 1920x1080 60HZ

So, I wonder the limitiation to 720p is cause by Linux driver or other factors? or some other factor in hardware?

 

Thanks.

Tags (1)
0 Kudos
Reply
1 Solution
2,719 Views
igorpadykov
NXP Employee
NXP Employee

>If the limition is the bandwidth, can I use a lower refresh frequency to avoid underflow?

 

yes

 

Best regards
igor

View solution in original post

0 Kudos
Reply
5 Replies
2,734 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xiaowei

 

limitation is internal bandwidth (hardware), so in general one can use more resolution

but underruns may occur, depending on use case.

 

Best regards
igor

0 Kudos
Reply
2,724 Views
xiaowei_zeng
Contributor III

Hi, igor

Thanks your quick response.

You mentioned the limitation is internal hardware bandwidth.

As is known, DCSS->MIPI->IMX-MIPI-HDMI can support 1920x1080 60HZ, but LCDIF->MIPI->IMX-MIPI-HDMI cannot suppot well. Does it means that the limitiation is in LCDIF's bandwidth?

If the limition is the bandwidth, can I use a lower refresh frequency to avoid underflow? e.g. reduce the pixel clock frequency to 1080p 50HZ or lower? or do have other workaround to run 1080p?

 

Thanks in advance.

BR

Xiaowei

 

Tags (1)
0 Kudos
Reply
2,720 Views
igorpadykov
NXP Employee
NXP Employee

>If the limition is the bandwidth, can I use a lower refresh frequency to avoid underflow?

 

yes

 

Best regards
igor

0 Kudos
Reply
1,035 Views
Few
Contributor I

Hi @igorpadykov 

I am currently having problems getting a MIPI-LVDS bridge to work on the i.MX8MM with kernel 5.10.

Is this a limitation of the i.MX or only in combination with the MIPI HDMI bridge?

 

Thanks!

0 Kudos
Reply
2,697 Views
xiaowei_zeng
Contributor III

Thanks igor.

When I set pixel clock to not higher than 120MHz , about 48Hz, the output works well.

 

BR

Xiaowei

Tags (1)
0 Kudos
Reply