Problem with Driving a 5" LVDS Raystar Screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with Driving a 5" LVDS Raystar Screen

Jump to solution
2,806 Views
ecitak
Contributor I

Hello,

We have a custom carrier board which utilizes a Variscite SoM that is running an iMX8MP processor. We are trying to drive a Raystar RFF500F-LNN-AWW, 5" LVDS screen with a Sitronix ST7262 IC. 

We tried with other screens and managed to get the display after the boot process. But for this case, we modified the device tree (I'm adding as an attachment) with no luck. There seems to be no driver for this specific model in the kernel. 

Are there any drivers we can use for this screen? Or what can be the problem? Any opinions are appreciated. 

Thanks.

0 Kudos
Reply
1 Solution
2,732 Views
ecitak
Contributor I

Hello, we solved the issue with the Variscite support, it seems they have fixed the LVDS clock of their SoM. The fix in the last part of https://variwiki.com/index.php?title=DART-MX8M-PLUS_Display&release=mx8mp-yocto-kirkstone-5.15-2.0.x... solved the issue after recompiling the kernel with the modifications.

View solution in original post

0 Kudos
Reply
2 Replies
2,733 Views
ecitak
Contributor I

Hello, we solved the issue with the Variscite support, it seems they have fixed the LVDS clock of their SoM. The fix in the last part of https://variwiki.com/index.php?title=DART-MX8M-PLUS_Display&release=mx8mp-yocto-kirkstone-5.15-2.0.x... solved the issue after recompiling the kernel with the modifications.

0 Kudos
Reply
2,741 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @ecitak 

You should get spec from Sitronix or Raystar , and modify the driver based on other Sitronix mainline driver.

0 Kudos
Reply