Is the OpenGL driver for the GPU available to RTOS vendors on any NXP atuomotive board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the OpenGL driver for the GPU available to RTOS vendors on any NXP atuomotive board?

3,867件の閲覧回数
willtang
Contributor I

I want to using OpenGL on RTOS (such as freeRTOS),  Is there any NXP automotive board support OpenGL on RTOS?

0 件の賞賛
返信
4 返答(返信)

3,851件の閲覧回数
smohsin
Contributor I

I'm not sure which NXP automotive board you're referring to, but most likely the answer is yes. OpenGL is a cross-platform graphics API that is widely used in embedded systems. Many RTOS vendors support OpenGL drivers for their products.

0 件の賞賛
返信

3,825件の閲覧回数
willtang
Contributor I

Thanks

 i.MX 6 and i.MX 8 serials board are ok for me。

I know some RTOS like QNX & Vxworks supports GPU。

But the  license cost are not acceptable for my project。

For my product , Opengl feature need to be implemented on FreeRTOS etc. RTOS ( free or lowcost)

Porting OpenGL needs source code in user space & kernel space .

I assume the GPU driver code is provided on on  i.MX 6 and i.MX 8 board.

But the user space driver is provided in binary。

So I want to know if  I could access  the user space  code by purchase some license,and the cost。

if  buying license is not an option,porting mesa3D to FreeRTOS (on  i.MX 6 and i.MX 8 board.)

is feasible or not?

Could you please give some advice?

Thanks in advance

 

 

 

0 件の賞賛
返信

3,862件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello willtang,

There is no opengl in rtos you can build GPU openGL stuff in linux.

Regards

 

0 件の賞賛
返信

3,858件の閲覧回数
willtang
Contributor I

 

Thanks.

my project need support opengl on RTOS.

Is it possible  porting  gpu user space & kernel driver on imx6/imx8  to RTOS?

gpu user space source on imx6/imx8 could be got ? and the cost.

Is it possible by porting mesa-3d to RTOS ?

 

 

0 件の賞賛
返信