IMX8MP,三屏显示时,运行qt程序时,无法将qt窗口指定到特定的屏幕

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP,三屏显示时,运行qt程序时,无法将qt窗口指定到特定的屏幕

1,967 Views
ygs
Contributor I

dear  NXP teams:

IMX8MP平台,我使用的是wayland构建weston桌面。在三屏显示时,屏幕分别为HDMI,LVDS,MIPI。运行qt程序,显示一个qt程序窗口到指定的屏幕,qt程序窗口无法显示在指定的屏幕,qt程序窗口始终显示在鼠标光标位置的屏幕。只有将鼠标光标移动到想要显示屏幕上,才能显示到那个屏幕上。同样的条件下在其他嵌入式平台不会出现这种情况。请问大家遇到过相似的这个问题吗?如何解决的?

thanks all 

@ NXP teams

0 Kudos
Reply
14 Replies

1,957 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

请提供BSP版本,一个简单的测试demo以及测试方法。

0 Kudos
Reply

1,913 Views
ygs
Contributor I

Dear Zhiming_Liu:

麻烦您看看我这个问题。

0 Kudos
Reply

1,900 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@ygs 需要全屏显示吗

0 Kudos
Reply

1,896 Views
ygs
Contributor I
不需要
0 Kudos
Reply

1,877 Views
ygs
Contributor I
Dear Zhiming_Liu :
麻烦问一下,您那边有解决办法吗?
0 Kudos
Reply

1,846 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@ygs 

还在和R&D 讨论这个问题。

0 Kudos
Reply

1,842 Views
ygs
Contributor I

@Zhiming_Liu  好的,麻烦你们了。如果有结果了,告知一下我,谢谢,我着急用这个功能。

0 Kudos
Reply

1,839 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

你们其他平台也是用的weston吗?

0 Kudos
Reply

1,837 Views
ygs
Contributor I

@Zhiming_Liu  是的,同样也是weston

0 Kudos
Reply

1,834 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

其他平台是用的哪个版本的weston?还有其他平台是?

0 Kudos
Reply

1,832 Views
ygs
Contributor I

@Zhiming_Liu  用的都是weston 10.0.1,其他平台是:RK3588

0 Kudos
Reply

1,868 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

目前还没有

0 Kudos
Reply

1,910 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

OK

0 Kudos
Reply

1,952 Views
ygs
Contributor I

Dear NXP Teams:

BSP版本为:L5.15.71_2.2.0

0 Kudos
Reply