How to port OpenGL ES2.0 to IMX6Q?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to port OpenGL ES2.0 to IMX6Q?

550 次查看
125672
Contributor I

I have an imx6Q chip, which has ported the Linux3.14.52 version and has the driver of the GPU kernel module. Now I need to use OpenGL ES2.0, but I still can't find a suitable library or pre-compiled library on the official NXP. Could you help provide it? Thank you

0 项奖励
回复
3 回复数

404 次查看
mattie236
Contributor I

Finding the correct graphics libraries for older embedded Linux systems like the i.MX 6Q with kernel 3.14.52 is challenging because the libraries are proprietary and tied to the specific Board Support Package (BSP). I cannot provide these files, as they are not publicly redistributable. The best approach is to search NXP's archives or community forums for the official BSP that matches your kernel version, as it will contain the necessary user-space libraries. Alternatively, you could explore the open-source Etnaviv driver, though its compatibility and features may vary for older kernels.

0 项奖励
回复

377 次查看
pengyong_zhang
NXP Employee
NXP Employee

hI @mattie236 

I will be on vacation for a week and may not reply during this period. If you are in a hurry, you can create a new ticket. My other colleagues will support you. Thanks for your understand.

0 项奖励
回复

504 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi @125672 

please refer the attachment file chapter 3.3

B.R

0 项奖励
回复