Gstreamer - glimagesink client-draw-callback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gstreamer - glimagesink client-draw-callback

2,690 Views
spear_kor
Contributor I

Dear All,

I was wondering if there is any available example for client-draw-callback implementation to draw frames using GLES2. 

I need to paint the decoded video frames on imx.8 using Yocto. 

 

0 Kudos
Reply
2 Replies

2,673 Views
spear_kor
Contributor I

Hello,

Thanks for the response.

However, I think I am misunderstood. I was asking for the client-draw-callback signal handler of GStreamer.

Thanks

0 Kudos
Reply

2,683 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Spear-kor,

 

In your yocto BSP you have the graphics examples, that include the triangle as example two, data in the
ESContext structure include information such as the window width and height, EGL context, and callback function pointers.

The rest of the main function is responsible for creating the window, initializing
the draw callback function, and entering the main loop:
esCreateWindow(&esContext, "Hello Triangle", 320, 240,
ES_WINDOW_RGB);
if(!Init(&esContext))
return 0;
esRegisterDrawFunc(&esContext, Draw);
esMainLoop(&esContext);

 

Regards

0 Kudos
Reply