GPU load on imx8mp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GPU load on imx8mp

跳至解决方案
1,199 次查看
jonashoeppner
Contributor II

When I dump the 'idle' information in the sysfs I get the following:

cat /sys/kernel/debug/gc/idle
On: 660,666,065,125 ns
Off: 12,594,477,978,125 ns
Idle: 0 ns
Suspend: 2,869,521,898,875 ns

Is there some documentation regarding the numbers?

I'm using a kernel based on the 5.10.52 from the NXP BSP.

0 项奖励
回复
1 解答
1,179 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

No documentation about it, but it is the time the graphics is in idle mode.

Regards

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,180 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

No documentation about it, but it is the time the graphics is in idle mode.

Regards

0 项奖励
回复
1,143 次查看
jonashoeppner
Contributor II

Thank you

0 项奖励
回复