Can i.MX8X drive a LVDS display with 1920x1200?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i.MX8X drive a LVDS display with 1920x1200?

1,692件の閲覧回数
alfonsomartin
Contributor I

In all the technical and marketing documentation about i.MX8X is shown that the maximum display resolution that you can drive is 1920x1080.

We had a request to connect a 1920x1200 LVDS display (http://www.ampire.com.tw/en/p1-product-detail.asp ) to the i.MX8X and just setting up properly the DT everything worked Ok.

Can you confirm that 1920x1200 displays are supported by i.MX8X?

In affirmative case; does it make sense to update the documentation?

thanks

0 件の賞賛
返信
1 返信

1,680件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for imx8qxp, The Display controller subsystem supports two Display Controllers (DC0 and DC1).

each DC can support up to:

Two LVDS interfaces supporting
- 1080p@60 on a single interface
- 4k@30 when aggregating the two interfaces

 

0 件の賞賛
返信