Buffer used for Gstreamer output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Buffer used for Gstreamer output

2,606 Views
Jack-Cha
Contributor V

Hi NXP

Please let me know which physical buffer is used in hardware when you output the display to the pipeline through the gstreamer.

A customer asked what buffers are physically used on the Gstremer pipeline when the camera is being inputted in BT656 format and output to LVDS Dual Display. Can you explain whether the physical device used as a buffer is DRAM, DMA, mmap, etc., including Data Path?

 

Thanks.

Regards, 

Arrow

0 Kudos
Reply
6 Replies

2,583 Views
Jack-Cha
Contributor V

Hi. 

i.MX 8 QuadXPlus (auto grade) is used for my customer's platform. 

Thanks.

 

0 Kudos
Reply

2,562 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,556 Views
Jack-Cha
Contributor V

Hi Joanxie

Thanks for your kind reply.

Can you tell me how that reserved memory works in conjunction with Gstremaer?

We don't know which memory areas were engaged with GStremaer?

 

reserved-memory {
 #address-cells = <2>;
 #size-cells = <2>;
 ranges;
  
 gpu_reserved: gpu_reserved@880000000 {
 no-map;
 reg = <0x8 0x80000000 0 0x10000000>;
 };
  
 decoder_boot: decoder-boot@84000000 {
 reg = <0 0x84000000 0 0x2000000>;
 no-map;
 };
  
 encoder_boot: encoder-boot@86000000 {
 reg = <0 0x86000000 0 0x200000>;
 no-map;
 };
  
 decoder_rpc: decoder-rpc@92000000 {
 reg = <0 0x92000000 0 0x100000>;
 no-map;
 };
  
 dsp_reserved: dsp@92400000 {
 reg = <0 0x92400000 0 0x1000000>;
 no-map;
 };
 dsp_reserved_heap: dsp_reserved_heap {
 reg = <0 0x93400000 0 0xef0000>;
 no-map;
 };
 dsp_vdev0vring0: vdev0vring0@942f0000 {
 reg = <0 0x942f0000 0 0x8000>;
 no-map;
 };
  
 dsp_vdev0vring1: vdev0vring1@942f8000 {
 reg = <0 0x942f8000 0 0x8000>;
 no-map;
 };
  
 dsp_vdev0buffer: vdev0buffer@94300000 {
 compatible = "shared-dma-pool";
 reg = <0 0x94300000 0 0x100000>;
 no-map;
 };
  
 encoder_rpc: encoder-rpc@94400000 {
 reg = <0 0x94400000 0 0x700000>;
 no-map;
 };
 /* global autoconfigured region for contiguous allocations */
 linux,cma {
 compatible = "shared-dma-pool";
 reusable;
 size = <0 0x3c000000>;
 alloc-ranges = <0 0xc0000000 0 0x3c000000>;
 linux,cma-default;
 };
 

};

 

0 Kudos
Reply

2,469 Views
joanxie
NXP TechSupport
NXP TechSupport

gstreamer is just a framework, depends on what you need, you can add vpu or gpu plugin in the gstreamer, then you can find related gpu or vpu(encoder/decoder) from the memory map

0 Kudos
Reply

2,536 Views
Jack-Cha
Contributor V

Hi

Customer need to write project report for this. Hence they would like to understand IMX8X' internal data path when using Gstreamer for dual lvds display output in addition to MIPI Camera Input,

It would be appreciate if you are able to provide us with more details about data path regarding Gstreamer Test Use case.

 

Thanks.

Regards, 

Jack

0 Kudos
Reply

2,594 Views
joanxie
NXP TechSupport
NXP TechSupport

what processor are you talking about?

0 Kudos
Reply