Buffer used for Gstreamer output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Buffer used for Gstreamer output

2,609件の閲覧回数
Jack-Cha
Contributor V

Hi NXP

Please let me know which physical buffer is used in hardware when you output the display to the pipeline through the gstreamer.

A customer asked what buffers are physically used on the Gstremer pipeline when the camera is being inputted in BT656 format and output to LVDS Dual Display. Can you explain whether the physical device used as a buffer is DRAM, DMA, mmap, etc., including Data Path?

 

Thanks.

Regards, 

Arrow

0 件の賞賛
返信
6 返答(返信)

2,586件の閲覧回数
Jack-Cha
Contributor V

Hi. 

i.MX 8 QuadXPlus (auto grade) is used for my customer's platform. 

Thanks.

 

0 件の賞賛
返信

2,565件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

2,559件の閲覧回数
Jack-Cha
Contributor V

Hi Joanxie

Thanks for your kind reply.

Can you tell me how that reserved memory works in conjunction with Gstremaer?

We don't know which memory areas were engaged with GStremaer?

 

reserved-memory {
 #address-cells = <2>;
 #size-cells = <2>;
 ranges;
  
 gpu_reserved: gpu_reserved@880000000 {
 no-map;
 reg = <0x8 0x80000000 0 0x10000000>;
 };
  
 decoder_boot: decoder-boot@84000000 {
 reg = <0 0x84000000 0 0x2000000>;
 no-map;
 };
  
 encoder_boot: encoder-boot@86000000 {
 reg = <0 0x86000000 0 0x200000>;
 no-map;
 };
  
 decoder_rpc: decoder-rpc@92000000 {
 reg = <0 0x92000000 0 0x100000>;
 no-map;
 };
  
 dsp_reserved: dsp@92400000 {
 reg = <0 0x92400000 0 0x1000000>;
 no-map;
 };
 dsp_reserved_heap: dsp_reserved_heap {
 reg = <0 0x93400000 0 0xef0000>;
 no-map;
 };
 dsp_vdev0vring0: vdev0vring0@942f0000 {
 reg = <0 0x942f0000 0 0x8000>;
 no-map;
 };
  
 dsp_vdev0vring1: vdev0vring1@942f8000 {
 reg = <0 0x942f8000 0 0x8000>;
 no-map;
 };
  
 dsp_vdev0buffer: vdev0buffer@94300000 {
 compatible = "shared-dma-pool";
 reg = <0 0x94300000 0 0x100000>;
 no-map;
 };
  
 encoder_rpc: encoder-rpc@94400000 {
 reg = <0 0x94400000 0 0x700000>;
 no-map;
 };
 /* global autoconfigured region for contiguous allocations */
 linux,cma {
 compatible = "shared-dma-pool";
 reusable;
 size = <0 0x3c000000>;
 alloc-ranges = <0 0xc0000000 0 0x3c000000>;
 linux,cma-default;
 };
 

};

 

タグ(1)
0 件の賞賛
返信

2,472件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

gstreamer is just a framework, depends on what you need, you can add vpu or gpu plugin in the gstreamer, then you can find related gpu or vpu(encoder/decoder) from the memory map

0 件の賞賛
返信

2,539件の閲覧回数
Jack-Cha
Contributor V

Hi

Customer need to write project report for this. Hence they would like to understand IMX8X' internal data path when using Gstreamer for dual lvds display output in addition to MIPI Camera Input,

It would be appreciate if you are able to provide us with more details about data path regarding Gstreamer Test Use case.

 

Thanks.

Regards, 

Jack

0 件の賞賛
返信

2,597件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what processor are you talking about?

0 件の賞賛
返信